camera module for MIMXRT1160-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

camera module for MIMXRT1160-EVK

ソリューションへジャンプ
2,208件の閲覧回数
kenthesis
Contributor I

Hi,

I am currently evaluating MIMXRT1160-EVK, which has a MIPI-CSI camera interface. The user guide said it could be used with MT9M114, a SOC image sensor chip. Is there a particular evaluation board for MT9M114 that I can purchase, so it plugs directly into MIMXRT1160-EVK?

 

Thank you!

Ken

タグ(3)
0 件の賞賛
返信
1 解決策
2,191件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Yes, you can use MT9M114 or OV5640 as a camera. The MT9M114 is included in the RT1064-EVK. And OV5640 is on RT1170-EVK. Unfortunately, we do not sell these camera modules separately.

The camera compatible out of the box with the MIMXRT1160-EVK is the same as the one included in the MIMXRT1170-EVK. The manufacturer for this module is Suzhou Real Electronics Technology Co., LTD, with the manufacturing part number R5640AA.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,174件の閲覧回数
kenthesis
Contributor I

Hi Omar,

Thank you for sharing. Great to hear that RT1170-EVK has a camera module. I will purchase this evk to test then. 

Kenneth

0 件の賞賛
返信
2,192件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Yes, you can use MT9M114 or OV5640 as a camera. The MT9M114 is included in the RT1064-EVK. And OV5640 is on RT1170-EVK. Unfortunately, we do not sell these camera modules separately.

The camera compatible out of the box with the MIMXRT1160-EVK is the same as the one included in the MIMXRT1170-EVK. The manufacturer for this module is Suzhou Real Electronics Technology Co., LTD, with the manufacturing part number R5640AA.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信