camera interface performance?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

camera interface performance?

1,376 Views
kangmw086
Contributor III

I want to know the performance difference between IMX6 parallel camera interface and MIPI interface.

Is there any comparison data such as parallel maximum operation speed and mipi maximum operation speed?

Is there a difference in gstreamer processing speed between when the camera input is parallel and when it is mipi?

camera input ~ HDMI output.

or

camera input ~ streaming output.

regards!

Labels (3)
0 Kudos
Reply
1 Reply

1,302 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello k,

One can use parallel CSI Interface,you can connect up to 4 cameras to the MIPI. for this you have to either use a MIPI CSI-2 hub or multiplexed the four streams in and FPGA.

The Parallel camera is limited to 10bits per camera.

Regards

0 Kudos
Reply