building Android OS from SD card for imx8m mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

building Android OS from SD card for imx8m mini

7,966 Views
Ruban1
Contributor II
I need full process.8MMINILPD4-EVKB
0 Kudos
Reply
21 Replies

7,868 Views
Ruban1
Contributor II

.

0 Kudos
Reply

7,874 Views
joanxie
NXP TechSupport
NXP TechSupport

download the android user guide from the link as below, then follow the step as user guide mentions

"https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications..."

 

0 Kudos
Reply

7,859 Views
Ruban1
Contributor II

All procedure is completed and it was build completely.

There was no error while building.

When SD card is inserted to IMX8M MINI the boot is getting completed .Kernel starts and in some point in Kernel its rebooting and jump to the starting .

Error is attached below

[ 14.352680] imx-sdma 302b0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 14.369747] ci_hdrc ci_hdrc.0: remove, state 1
[ 14.374210] usb usb1: USB disconnect, device number 1
[ 14.379268] usb 1-1: USB disconnect, device number 2
[ 14.545952] ci_hdrc ci_hdrc.0: USB bus 1 deregistered
[ 14.572483] reboot: Restarting system with command 'bootloader'

U-Boot SPL 2020.04-dirty (Mar 22 2021 - 09:56:56 +0530)
power_bd71837_init
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.2(release):android-11.0.0_1.0.0-rc3-0-g1555e5d00
NOTICE: BL31: Built : 09:57:44, Mar 22 2021


U-Boot 2020.04-dirty (Mar 22 2021 - 09:56:56 +0530)

CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 45C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (1920 x 1080)
[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 1555e5d
- U-Boot 2020.04-dirty

flash target is MMC:1
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Writing A/B metadata to disk.
verify OK, boot 'boot_b'
Kernel load addr 0x40480000 size 43143 KiB
kernel @ 40480000 (44177920)
ramdisk @ 44680000 (8503659)
fdt @ 44480000 (47651)
## Flattened Device Tree blob at 44480000
Booting using the fdt blob at 0x44480000
Using Device Tree in place at 0000000044480000, end 000000004448ea22

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.4.47 (ruban@ruban-OptiPlex-5070) (Android (6573524 based on r383902b) clang version 11.0.2 (https://android.goog1
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[ 0.000000] printk: bootconsole [ec_imx6q0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 800 MiB at 0x0000000084000000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbfbcd500-0xbfbcefff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000b84fffff]
[ 0.000000] node 0: [mem 0x00000000b8510000-0x00000000bfffffff]
[ 0.000000] Zeroed struct page in unavailable ranges: 16 pages
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 33 pages/cpu s96280 r8192 d30696 u135168
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515056
[ 0.000000] Policy zone: DMA32
[ 0.000000] Kernel command line: console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init androidboot.console=ttymxc1 androidboo
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1179992K/2092992K available (21564K kernel code, 2310K rwdata, 13652K rodata, 5312K init, 576K bss, 93800K reserved, 819)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x208/0x41c with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000003] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008487] Console: colour dummy device 80x25
[ 0.012617] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.022845] pid_max: default: 32768 minimum: 301
[ 0.027550] LSM: Security Framework initializing
[ 0.032144] SELinux: Initializing.
[ 0.035674] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.043063] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.075028] ASID allocator initialised with 32768 entries
[ 0.083027] rcu: Hierarchical SRCU implementation.
[ 0.091949] EFI services will not be available.
[ 0.099067] smp: Bringing up secondary CPUs ...
[ 0.131235] Detected VIPT I-cache on CPU1
[ 0.131263] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.131297] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.163283] Detected VIPT I-cache on CPU2
[ 0.163300] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.163322] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.195340] Detected VIPT I-cache on CPU3
[ 0.195357] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.195376] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.195443] smp: Brought up 1 node, 4 CPUs
[ 0.249202] SMP: Total of 4 processors activated.
[ 0.253920] CPU features: detected: 32-bit EL0 Support
[ 0.259098] CPU features: detected: CRC32 instructions
[ 0.280588] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.286126] CPU: All CPU(s) started at EL2
[ 0.290254] alternatives: patching kernel code
[ 0.295715] CPU3: update max cpu_capacity 1024
[ 0.296784] devtmpfs: initialized
[ 0.307593] CPU1: update max cpu_capacity 1024
[ 0.310381] Initilizing CustomIPI irq domain
[ 0.316296] Registered cp15_barrier emulation handler
[ 0.321352] Registered setend emulation handler
[ 0.326221] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.335709] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.365231] pinctrl core: initialized pinctrl subsystem
[ 0.368344] DMI not present or invalid.
[ 0.371893] NET: Registered protocol family 16
[ 0.376680] schedtune: configured to support 5 boost groups
[ 0.391922] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.395224] audit: initializing netlink subsys (disabled)
[ 0.400914] audit: type=2000 audit(0.344:1): state=initialized audit_enabled=0 res=1
[ 0.408440] cpuidle: using governor menu
[ 0.413099] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.420089] Serial: AMBA PL011 UART driver
[ 0.423346] imx mu driver is registered.
[ 0.427226] imx rpmsg driver is registered.
[ 0.432485] printk: console [pstore-1] enabled
[ 0.436048] pstore: Registered ramoops as persistent store backend
[ 0.442096] ramoops: using 0x100000@0xb7f00000, ecc: 0
[ 0.473508] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.493857] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.497762] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.504474] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.511214] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.519089] cryptd: max_cpu_qlen set to 1000
[ 0.525672] ACPI: Interpreter disabled.
[ 0.527715] iommu: Default domain type: Translated
[ 0.531909] vgaarb: loaded
[ 0.534846] SCSI subsystem initialized
[ 0.538387] usbcore: registered new interface driver usbfs
[ 0.543598] usbcore: registered new interface driver hub
[ 0.548954] usbcore: registered new device driver usb
[ 0.554890] mc: Linux media interface: v0.10
[ 0.558279] videodev: Linux video capture interface: v2.00
[ 0.563825] pps_core: LinuxPPS API ver. 1 registered
[ 0.568751] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.577949] PTP clock support registered
[ 0.582147] trusty trusty: failed to get version: -1
[ 0.586868] trusty trusty: selected api version: 0 (requested 3)
[ 0.593868] EDAC MC: Ver: 3.0.0
[ 0.597043] FPGA manager framework
[ 0.599561] Advanced Linux Sound Architecture Driver Initialized.
[ 0.606018] Bluetooth: Core ver 2.22
[ 0.609185] NET: Registered protocol family 31
[ 0.613641] Bluetooth: HCI device and connection manager initialized
[ 0.620033] Bluetooth: HCI socket layer initialized
[ 0.624930] Bluetooth: L2CAP socket layer initialized
[ 0.630006] Bluetooth: SCO socket layer initialized
[ 0.636262] clocksource: Switched to clocksource arch_sys_counter
[ 0.720222] VFS: Disk quotas dquot_6.6.0
[ 0.721361] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.728412] pnp: PnP ACPI: disabled
[ 0.738257] thermal_sys: Registered thermal governor 'step_wise'
[ 0.738262] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.741802] NET: Registered protocol family 2
[ 0.752832] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.760998] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.769026] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.776490] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.782925] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.789613] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.796884] NET: Registered protocol family 1
[ 0.801553] PCI: CLS 0 bytes, default 64
[ 0.805266] Trying to unpack rootfs image as initramfs...
[ 1.149071] Freeing initrd memory: 8304K
[ 1.151228] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.158381] kvm [1]: IPA Size Limit: 40bits
[ 1.163585] kvm [1]: GICv3: no GICV resource entry
[ 1.166954] kvm [1]: disabling GICv2 emulation
[ 1.171431] kvm [1]: GIC system register CPU interface enabled
[ 1.177363] kvm [1]: vgic interrupt IRQ1
[ 1.181350] kvm [1]: Hyp mode initialized successfully
[ 1.189846] Initialise system trusted keyrings
[ 1.191545] workingset: timestamp_bits=44 max_order=19 bucket_order=0
[ 1.204668] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.207802] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 1.214225] fuse: init (API version 7.31)
[ 1.218160] 9p: Installing v9fs 9p2000 file system support
[ 1.238063] Key type asymmetric registered
[ 1.239313] Asymmetric key parser 'x509' registered
[ 1.244260] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 239)
[ 1.251655] io scheduler mq-deadline registered
[ 1.256205] io scheduler kyber registered
[ 1.276602] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 1.284271] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 1.302250] mxs-dma 33000000.dma-controller: initialized
[ 1.306036] Bus freq driver module loaded
[ 1.312546] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.318291] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 5000000) is a IMX
[ 1.325389] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX
[ 1.334093] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX
[ 1.342548] printk: console [ttymxc1] enabled
[ 1.342548] printk: console [ttymxc1] enabled
[ 1.351204] printk: bootconsole [ec_imx6q0] disabled
[ 1.351204] printk: bootconsole [ec_imx6q0] disabled
[ 1.367060] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.373706] [drm] No driver support for vblank timestamp query.
[ 1.379720] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 1.389676] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 1.397234] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 1.405513] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -517
[ 1.423315] brd: module loaded
[ 1.433685] loop: module loaded
[ 1.437319] zram: Added device: zram0
[ 1.442437] nd_pmem namespace0.0: unable to guarantee persistence of writes
[ 1.443862] imx ahci driver is registered.
[ 1.450155] pmem0: detected capacity change from 0 to 65536
[ 1.457084] spi-nor spi3.0: n25q256ax1 (32768 Kbytes)
[ 1.470368] libphy: Fixed MDIO Bus: probed
[ 1.475393] tun: Universal TUN/TAP device driver, 1.6
[ 1.481368] thunder_xcv, ver 1.0
[ 1.484658] thunder_bgx, ver 1.0
[ 1.487921] nicpf, ver 1.0
[ 1.491564] pps pps0: new PPS source ptp0
[ 1.501847] libphy: fec_enet_mii_bus: probed
[ 1.508981] fec 30be0000.ethernet eth0: registered PHC device 0
[ 1.516354] hclge is initializing
[ 1.519677] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.526912] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.532322] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.539381] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.545176] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.551020] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.556983] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.563953] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.569568] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.577408] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.583522] sky2: driver version 1.30
[ 1.587941] PPP generic driver version 2.4.2
[ 1.592396] PPP BSD Compression module registered
[ 1.597118] PPP Deflate Compression module registered
[ 1.602197] PPP MPPE Compression module registered
[ 1.607000] NET: Registered protocol family 24
[ 1.611453] PPTP driver version 0.8.5
[ 1.615357] usbcore: registered new interface driver r8152
[ 1.620889] usbcore: registered new interface driver asix
[ 1.626352] usbcore: registered new interface driver ax88179_178a
[ 1.632487] usbcore: registered new interface driver cdc_ether
[ 1.638397] usbcore: registered new interface driver net1080
[ 1.644105] usbcore: registered new interface driver cdc_subset
[ 1.650071] usbcore: registered new interface driver zaurus
[ 1.655698] usbcore: registered new interface driver cdc_ncm
[ 1.661571] VFIO - User Level meta-driver version: 0.3
[ 1.668810] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.675359] ehci-pci: EHCI PCI platform driver
[ 1.679850] ehci-platform: EHCI generic platform driver
[ 1.685292] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.691484] ohci-pci: OHCI PCI platform driver
[ 1.695974] ohci-platform: OHCI generic platform driver
[ 1.701994] usbcore: registered new interface driver uas
[ 1.707368] usbcore: registered new interface driver usb-storage
[ 1.713466] usbcore: registered new interface driver usbserial_generic
[ 1.720023] usbserial: USB Serial support registered for generic
[ 1.726065] usbcore: registered new interface driver ftdi_sio
[ 1.731842] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.739194] usbcore: registered new interface driver usb_serial_simple
[ 1.745754] usbserial: USB Serial support registered for carelink
[ 1.751874] usbserial: USB Serial support registered for zio
[ 1.757563] usbserial: USB Serial support registered for funsoft
[ 1.763599] usbserial: USB Serial support registered for flashloader
[ 1.769982] usbserial: USB Serial support registered for google
[ 1.775931] usbserial: USB Serial support registered for libtransistor
[ 1.782486] usbserial: USB Serial support registered for vivopay
[ 1.788520] usbserial: USB Serial support registered for moto_modem
[ 1.794818] usbserial: USB Serial support registered for motorola_tetra
[ 1.801459] usbserial: USB Serial support registered for novatel_gps
[ 1.807840] usbserial: USB Serial support registered for hp4x
[ 1.813614] usbserial: USB Serial support registered for suunto
[ 1.819561] usbserial: USB Serial support registered for siemens_mpi
[ 1.825956] usbcore: registered new interface driver usb_ehset_test
[ 1.833937] imx_usb 32e40000.usb: No over current polarity defined
[ 1.841676] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/soc@0:bus@30000000/30370000.snvs/30370000.snvs:snvs-powerkey/input0
[ 1.855502] usbcore: registered new interface driver xpad
[ 1.860967] usbcore: registered new interface driver usb_acecad
[ 1.866928] usbcore: registered new interface driver aiptek
[ 1.872542] usbcore: registered new interface driver gtco
[ 1.877983] usbcore: registered new interface driver hanwang
[ 1.883683] usbcore: registered new interface driver kbtab
[ 1.890944] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.897206] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:09:00 UTC (540)
[ 1.906559] i2c /dev entries driver
[ 1.910987] mx6s-csi 32e20000.csi1_bridge: initialising
[ 1.916840] mxc_mipi-csi 32e30000.mipi_csi: 32e30000.mipi_csi supply mipi-phy not found, using dummy regulator
[ 1.927081] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[ 1.934065] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[ 1.939751] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[ 1.949735] uvcvideo: Unable to create debugfs directory
[ 1.955112] usbcore: registered new interface driver uvcvideo
[ 1.960868] USB Video Class driver (1.1.1)
[ 1.965709] __power_supply_register: Expected proper parent device for 'battery'
[ 1.973475] __power_supply_register: Expected proper parent device for 'usb'
[ 1.983993] trusty-log not supported on secure side.
[ 1.989151] trusty-virtio trusty:trusty-virtio: initializing
[ 1.994864] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
[ 2.004363] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr
[ 2.011859] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices
[ 2.019724] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0)
[ 2.026428] device-mapper: uevent: version 1.0.3
[ 2.031304] device-mapper: ioctl: 4.41.0-ioctl (2019-09-16) initialised: dm-devel@redhat.com
[ 2.040036] Bluetooth: HCI UART driver ver 2.3
[ 2.044507] Bluetooth: HCI UART protocol H4 registered
[ 2.049660] Bluetooth: HCI UART protocol BCSP registered
[ 2.055010] Bluetooth: HCI UART protocol LL registered
[ 2.060162] Bluetooth: HCI UART protocol ATH3K registered
[ 2.065592] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.072046] Bluetooth: HCI UART protocol Broadcom registered
[ 2.077736] Bluetooth: HCI UART protocol QCA registered
[ 2.085274] sdhci: Secure Digital Host Controller Interface driver
[ 2.091474] sdhci: Copyright(c) Pierre Ossman
[ 2.096086] Synopsys Designware Multimedia Card Interface Driver
[ 2.102753] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.141848] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 2.152030] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.158653] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.166867] usbcore: registered new interface driver usbhid
[ 2.172465] usbhid: USB HID core driver
[ 2.178858] ashmem: initialized
[ 2.186537] galcore: clk_get vg clock failed, disable vg!
[ 2.192307] Galcore version 6.4.3.p0.286725
[ 2.254715] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 2.266010] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 2.269456] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0
[ 2.270770] mmcblk2boot0: mmc2:0001 DG4016 partition 1 4.00 MiB
[ 2.279545] hantrodec 0 : module inserted. Major = 506
[ 2.284120] mmcblk2boot1: mmc2:0001 DG4016 partition 2 4.00 MiB
[ 2.289644] hantrodec 1 : module inserted. Major = 506
[ 2.295740] mmcblk2rpmb: mmc2:0001 DG4016 partition 3 4.00 MiB, chardev (510:0)
[ 2.301060] hx280enc: module inserted. Major <505>
[ 2.314611] usbcore: registered new interface driver snd-usb-audio
[ 2.325997] Alternate GPT is invalid, using primary GPT.
[ 2.331400] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 2.366912] fsl-micfil-dai 30080000.micfil: GET IRQ: 16
[ 2.372188] fsl-micfil-dai 30080000.micfil: GET IRQ: 17
[ 2.377435] fsl-micfil-dai 30080000.micfil: GET IRQ: 18
[ 2.382684] fsl-micfil-dai 30080000.micfil: GET IRQ: 19
[ 2.394361] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 30090000.spdif mapping ok
[ 2.402022] imx-spdif sound-spdif: ASoC: no DMI vendor name!
[ 2.411659] imx-micfil sound-micfil: snd-soc-dummy-dai <-> 30080000.micfil mapping ok
[ 2.419541] imx-micfil sound-micfil: ASoC: no DMI vendor name!
[ 2.427634] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 2.439345] drop_monitor: Initializing network drop monitor service
[ 2.445717] NET: Registered protocol family 26
[ 2.450181] netem: version 1.3
[ 2.453253] u32 classifier
[ 2.455963] input device check on
[ 2.459635] Actions configured
[ 2.463747] xt_time: kernel timezone is -0000
[ 2.468246] gre: GRE over IPv4 demultiplexor driver
[ 2.473144] IPv4 over IPsec tunneling driver
[ 2.478041] Initializing XFRM netlink socket
[ 2.482353] IPsec XFRM device driver
[ 2.486421] NET: Registered protocol family 10
[ 2.492174] Segment Routing with IPv6
[ 2.495962] mip6: Mobile IPv6
[ 2.499926] NET: Registered protocol family 17
[ 2.504412] NET: Registered protocol family 15
[ 2.509633] Bluetooth: RFCOMM TTY layer initialized
[ 2.514539] Bluetooth: RFCOMM socket layer initialized
[ 2.519701] Bluetooth: RFCOMM ver 1.11
[ 2.523464] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.528787] Bluetooth: BNEP filters: protocol multicast
[ 2.534026] Bluetooth: BNEP socket layer initialized
[ 2.539002] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.544955] Bluetooth: HIDP socket layer initialized
[ 2.549962] l2tp_core: L2TP core driver, V2.0
[ 2.554338] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.559138] 8021q: 802.1Q VLAN Support v1.8
[ 2.563351] lib80211: common routines for IEEE802.11 drivers
[ 2.569439] 9pnet: Installing 9P2000 support
[ 2.573748] tsn generic netlink module v1 init...
[ 2.579618] registered taskstats version 1
[ 2.583740] Loading compiled-in X.509 certificates
[ 2.588679] Key type ._fscrypt registered
[ 2.592701] Key type .fscrypt registered
[ 2.596634] Key type fscrypt-provisioning registered
[ 2.602547] pstore: Using crash dump compression: deflate
[ 2.616152] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 2.624994] usb_phy_generic usbphynop2: usbphynop2 supply vcc not found, using dummy regulator
[ 2.648013] ldo6: supplied by regulator-dummy
[ 2.653204] i2c i2c-0: IMX I2C adapter registered
[ 2.659308] adv7511 1-003d: 1-003d supply avdd not found, using dummy regulator
[ 2.666731] adv7511 1-003d: 1-003d supply dvdd not found, using dummy regulator
[ 2.674071] adv7511 1-003d: 1-003d supply pvdd not found, using dummy regulator
[ 2.681409] adv7511 1-003d: 1-003d supply a2vdd not found, using dummy regulator
[ 2.688832] adv7511 1-003d: 1-003d supply v3p3 not found, using dummy regulator
[ 2.696168] adv7511 1-003d: 1-003d supply v1p2 not found, using dummy regulator
[ 2.712098] random: fast init done
[ 2.719232] i2c i2c-1: IMX I2C adapter registered
[ 2.728782] ov5640_mipi 2-003c: No sensor reset pin available
[ 2.734592] ov5640_mipi 2-003c: 2-003c supply DOVDD not found, using dummy regulator
[ 2.742422] ov5640_mipi 2-003c: 2-003c supply DVDD not found, using dummy regulator
[ 2.750108] ov5640_mipi 2-003c: 2-003c supply AVDD not found, using dummy regulator
[ 2.768589] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 2.773921] ov5640_mipi 2-003c: Camera is not found
[ 2.778955] i2c i2c-2: IMX I2C adapter registered
[ 2.785520] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator
[ 2.794962] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.816643] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.828364] imx6q-pcie 33800000.pcie: PCIe PLL locked after 20 us.
[ 2.834615] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 2.841877] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 2.849297] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 2.857356] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.865658] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.872314] [drm] No driver support for vblank timestamp query.
[ 2.878326] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 2.888290] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.897371] imx-drm soc@0:bus@32c00000:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.907279] mmc0: queuing unknown CIS tuple 0x01 (3 bytes)
[ 2.912910] [drm] Initialized imx-drm 1.0.0 20120507 for soc@0:bus@32c00000:display-subsystem on minor 1
[ 2.933281] mmc0: queuing unknown CIS tuple 0x1a (5 bytes)
[ 2.942554] mmc0: queuing unknown CIS tuple 0x1b (8 bytes)
[ 2.948753] mmc0: queuing unknown CIS tuple 0x14 (0 bytes)
[ 2.970499] mmc0: queuing unknown CIS tuple 0x80 (1 bytes)
[ 2.976146] mmc0: queuing unknown CIS tuple 0x81 (1 bytes)
[ 2.981704] mmc0: queuing unknown CIS tuple 0x82 (1 bytes)
[ 2.987235] mmc0: new ultra high speed SDR104 SDIO card at address 0001
[ 3.435795] Console: switching to colour frame buffer device 240x67
[ 3.474131] imx-drm soc@0:bus@32c00000:display-subsystem: fb0: imx-drmdrmfb frame buffer device
[ 3.483670] imx_usb 32e40000.usb: No over current polarity defined
[ 3.489959] imx_usb 32e40000.usb: 32e40000.usb supply vbus not found, using dummy regulator
[ 3.504001] bt power gpio is:38
[ 3.507291] mxc_bt_rfkill driver success loaded
[ 3.512102] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 3.521563] rfkill: BT RF going to : on
[ 3.525439] mxc_bt_rfkill_reset
[ 3.530810] Hot alarm is canceled. GPU3D clock will return to 64/64
[ 3.539029] asoc-simple-card sound-bt-sco: bt-sco-pcm <-> 30020000.sai mapping ok
[ 3.546550] asoc-simple-card sound-bt-sco: ASoC: no DMI vendor name!
[ 3.554928] asoc-simple-card sound-wm8524: wm8524-hifi <-> 30030000.sai mapping ok
[ 3.562548] asoc-simple-card sound-wm8524: ASoC: no DMI vendor name!
[ 3.577318] imx-ak4458 sound-ak4458: ASoC: failed to init link ak4458: -517
[ 3.584318] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-517)
[ 3.593987] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 3.602730] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 3.860419] imx6q-pcie 33800000.pcie: Phy link never came up
[ 3.945278] imx6q-pcie 33800000.pcie: failed to initialize host
[ 3.951228] imx6q-pcie 33800000.pcie: unable to add pcie port.
[ 3.956318] ak4458 2-0010: ASoC: failed to probe component -6
[ 3.962831] imx-ak4458 sound-ak4458: ASoC: failed to instantiate card -6
[ 3.969586] imx-ak4458 sound-ak4458: snd_soc_register_card failed (-6) //Ruban
[ 3.978566] input: bd718xx-pwrkey as /devices/platform/soc@0/soc@0:bus@30800000/30a20000.i2c/i2c-0/0-004b/gpio-keys.1.auto/input/input1
[ 3.991552] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 4.003322] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 4.010004] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 4.018347] ALSA device list:
[ 4.018672] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db //Ruban
[ 4.021627] #0: imx-spdif
[ 4.032156] #1: imx-audio-micfil
[ 4.035812] #2: bt-sco-audio
[ 4.038875] #3: wm8524-audio
[ 4.043808] Freeing unused kernel memory: 5312K
[ 4.068602] Run /init as init process
[ 4.101418] init: init first stage started!
[ 4.105766] init: Unable to open /lib/modules, skipping module loading.
[ 4.112703] init: Switching root to '/first_stage_ramdisk'
[ 4.120558] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 4.216912] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found in /sys, waiting for tb
[ 4.317618] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 4.322545] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 4.344288] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 4.349868] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[ 4.358144] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.365371] usb usb1: Product: EHCI Host Controller
[ 4.370271] usb usb1: Manufacturer: Linux 5.4.47 ehci_hcd
[ 4.375674] usb usb1: SerialNumber: ci_hdrc.0
[ 4.381043] hub 1-0:1.0: USB hub found
[ 4.384825] hub 1-0:1.0: 1 port detected
[ 4.724934] usb 1-1: new full-speed USB device number 2 using ci_hdrc
[ 4.899356] usb 1-1: New USB device found, idVendor=413c, idProduct=301b, bcdDevice=11.23
[ 4.907556] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.914703] usb 1-1: Product: Dell Universal Receiver
[ 4.919764] usb 1-1: Manufacturer: Dell
[ 4.928863] input: Dell Dell Universal Receiver as /devices/platform/soc@0/soc@0:bus@32c00000/32e40000.usb/ci_hdrc.0/usb1/1-1/1-1:1.0/0003:42
[ 5.002473] hid-generic 0003:413C:301B.0001: input,hidraw0: USB HID v1.11 Keyboard [Dell Dell Universal Receiver] on usb-ci_hdrc.0-1/input0
[ 5.020145] input: Dell Dell Universal Receiver Mouse as /devices/platform/soc@0/soc@0:bus@32c00000/32e40000.usb/ci_hdrc.0/usb1/1-1/1-1:1.1/3
[ 5.036132] input: Dell Dell Universal Receiver Consumer Control as /devices/platform/soc@0/soc@0:bus@32c00000/32e40000.usb/ci_hdrc.0/usb1/14
[ 5.113407] input: Dell Dell Universal Receiver System Control as /devices/platform/soc@0/soc@0:bus@32c00000/32e40000.usb/ci_hdrc.0/usb1/1-15
[ 5.130670] hid-generic 0003:413C:301B.0002: input,hidraw1: USB HID v1.11 Mouse [Dell Dell Universal Receiver] on usb-ci_hdrc.0-1/input1
[ 5.148174] hid-generic 0003:413C:301B.0003: hiddev96,hidraw2: USB HID v1.11 Device [Dell Dell Universal Receiver] on usb-ci_hdrc.0-1/input2
[ 14.239841] init: Wait for partitions returned after 10005ms
[ 14.245666] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout:b
[ 14.262191] init: Failed to mount required partitions early ...
[ 14.269358] init: InitFatalReboot: signal 6
[ 14.277395] init: #00 pc 00000000000afe30 /system/bin/init
[ 14.283068] init: #01 pc 000000000004cd90 /system/bin/init
[ 14.288671] init: #02 pc 0000000000013ab0 /system/lib64/libbase.so
[ 14.295011] init: #03 pc 0000000000013090 /system/lib64/libbase.so
[ 14.301297] init: #04 pc 0000000000075b1c /system/bin/init
[ 14.306902] init: #05 pc 000000000002e0ec /system/bin/init
[ 14.312542] kvm: exiting hardware virtualization
[ 14.312875] imx-sdma 302b0000.dma-controller: external firmware not found, using ROM firmware
[ 14.312929] cfg80211: failed to load regulatory.db
[ 14.313004] imx-sdma 302c0000.dma-controller: external firmware not found, using ROM firmware
[ 14.313071] imx-sdma 30bd0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 14.313076] imx-sdma 30bd0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 19.269982] init: Reboot ending, jumping to kernel
[ 35.880671] VSD_3V3: disabling
[ 47.488649] random: crng init done

 

 

 

 

 

 

0 Kudos
Reply

7,853 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mind using demo images to test first? could you get the same issue?

 

0 Kudos
Reply

7,847 Views
Ruban1
Contributor II

Yes , i was facing same issue even flashing with Demo image provided by NXP for IMX8M MINI

0 Kudos
Reply

7,830 Views
joanxie
NXP TechSupport
NXP TechSupport

I have downloaded android 11.0.0_1.0.0 as your demands, download to the board and boot up successfully, I used the command:

\Android\android-11.0.0_1.0.0_image_8mmevk.tar\android-11.0.0_1.0.0_image_8mmevk> .\uuu_imx_android_flash.bat -f imx8mm -a -e
This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic partition is supported
vendor_boot is supported
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- lib1.3.124-0-gee3f09a

Success 1 Failure 0

then set the boot mode to emmc booting up without any issue

 

0 Kudos
Reply

7,826 Views
Ruban1
Contributor II

I am using Ubuntu 20.04 OS . .\uuu_imx_android_flash.bat -f imx8mm -a -e this command is for Windos OS

For Ubuntu 20.04 OS .\uuu_imx_android_flash.sh -f imx8mm -a -e with .sh shell script

0 Kudos
Reply

7,817 Views
joanxie
NXP TechSupport
NXP TechSupport

I don't have ubuntu 20.04 to test for you, but I think this should be same, did you download the images to the board successfully? since I have already verified it on win10 OS, if you could, you can reproduce this steps, if you still failed booting up the board, try to contact the owner who offered your board, to confirm if your board is broken or not

 

0 Kudos
Reply

7,812 Views
Ruban1
Contributor II

Sir in board Android is already present in emmc. But i am working to build boot-able SD card with Android OS . Just like plug and play. I want to run Android only through SD card.

Later planning Yocto OS in SD card .. i dont want to change anything on the board emmc. Is that possible only run through SD without Downloading the OS to the board EMMC 

Tags (1)
0 Kudos
Reply

7,796 Views
joanxie
NXP TechSupport
NXP TechSupport

besides, the emmc boot mode is different from sd boot mode, obviously you test the emmc always, I was confused with your question, you need boot up from sd card, but you download the image to the emmc and boot up failed? anyway, I tested emmc on board successfully, you can use the new command to download demo images to the sd card and try again, don't forget set the correct boot mode

 

0 Kudos
Reply

7,716 Views
Ruban1
Contributor II

what is the new command to download

 

0 Kudos
Reply

7,702 Views
joanxie
NXP TechSupport
NXP TechSupport

I don't know what you mean, you can find all of download command in the android user guide

 

0 Kudos
Reply

7,698 Views
Ruban1
Contributor II

Still there is error

 

0 Kudos
Reply

7,668 Views
joanxie
NXP TechSupport
NXP TechSupport

what do you mean? give specific informaiton

0 Kudos
Reply

7,797 Views
joanxie
NXP TechSupport
NXP TechSupport

since you want to download to the sd card only, you use the wrong command like " .\uuu_imx_android_flash.bat -f imx8mm -a -e" which is for emmc, if you want to download to the sd card, try to use the command like " .\uuu_imx_android_flash.bat -f imx8mm -a -e -t sd"

 If "-t"option is not used, images will be flashed to eMMC.

 

0 Kudos
Reply

7,775 Views
Ruban1
Contributor II

one more doubt .Should i run this commands connected to imx8m mini evk board and insert SD in this evk board.

This process i am doing is I am using ubuntu 20.04 OS PC and connecting SD card using  card reader and trying to flash SD card then if it got flashed successfully .I am then inserting in imx8m mini evk board  and turning it ON.

0 Kudos
Reply

7,775 Views
Ruban1
Contributor II

i tried but still facing error

./uuu_imx_android_flash.sh -f imx8mm -a -e -t sd
This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic parttition is supported
vendor_boot parttition is supported
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-14-g519c261

Wait for Known USB Device Appear...
Error: fail open file: >/tmp/uuu.lst

 

0 Kudos
Reply

7,772 Views
joanxie
NXP TechSupport
NXP TechSupport

what uuu version do you use? try to download 1.3.124 and try again

 

0 Kudos
Reply

7,769 Views
Ruban1
Contributor II

UUU version 1.4.107  i am working on Ubuntu 20.04 . its unable to downgrade the version of UUU . i tried even with git .its only able to download but the version it the same. i tried to remove the upgrade version and use downloaded uuu .then its not running. Its telling to install.

 

Its not able only UUU version.


Wait for Known USB Device Appear...
Error: fail open file: >/tmp/uuu.lst

This is the main error. its not able to open the file

0 Kudos
Reply

7,753 Views
joanxie
NXP TechSupport
NXP TechSupport

I downloaded it on my lpddr4 board successfully with WIN10 OS:

This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic partition is supported
vendor_boot is supported
generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- lib1.3.124-0-gee3f09a

Success 1 Failure 0

but I found android 11 has reboot issue with sd card, I double checked release note and dts file, I found imx8mm lpddr4 use WI-FI slot, which uses usdhc2, so on imx8mm lpddr4 board, try to use emmc

 

0 Kudos
Reply