build fsl-image-qt5 on imx6ull developerment problem!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

build fsl-image-qt5 on imx6ull developerment problem!

2,057件の閲覧回数
lilleli
Contributor I

Hi i.MX Community,

 I build yocto image ,below erro!

bitbake core-image-minimal
Loading cache: 100% |############################################| Time: 0:00:02
Loaded 3049 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull14x14evk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.9.11-1.0.0"
TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:78890ea22750804e3e9113e76f7ca3d7234c8342"
meta-oe
meta-multimedia = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-freescale = "HEAD:a398b50b7fc084a9e68cc3000c218d5028522a25"
meta-freescale-3rdparty = "HEAD:68314612e236cab1da82d72a0da62635a3523f84"
meta-freescale-distro = "HEAD:cd5c7a2539f40004f74126e9fdf08254fd9a6390"
meta-bsp
meta-sdk = "HEAD:daba3340ecd8b358e0c6c415baeee0fcae95c525"
meta-browser = "HEAD:10f6e3778d823ee1be106c126216c6f941088fbf"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-qt5 = "HEAD:ff073f04109900fc07bf81e2f1df63c626caf342"

Initialising tasks: 100% |#######################################| Time: 0:00:04
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: util-linux-native-2.28.1-r0 do_compile: oe_runmake failed
ERROR: util-linux-native-2.28.1-r0 do_compile: Function failed: do_compile (log file is located at /home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/temp/log.do_compile.7660)
ERROR: Logfile of failure stored in: /home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/temp/log.do_compile.7660
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 1 ARCH=x86_64 CPU= CPUOPT= OPT=-isystem/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe
| ERROR: oe_runmake failed
| make all-recursive
| make[1]: Entering directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build'
| Making all in po
| make[2]: Entering directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build/po'
| make[2]: Nothing to be done for `all'.
| make[2]: Leaving directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build/po'
| make[2]: Entering directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build'
| gcc -std=gnu99 -DHAVE_CONFIG_H -I. -I../util-linux-2.28.1 -include config.h -I../util-linux-2.28.1/include -DLOCALEDIR=\"/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/sysroots/x86_64-linux/usr/share/locale\" -D_PATH_LOCALSTATEDIR=\"/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/sysroots/x86_64-linux/var\" -isystem/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/sysroots/x86_64-linux/usr/include -fsigned-char -fno-common -Wall -Werror=sequence-point -Wextra -Wmissing-declarations -Wmissing-parameter-type -Wmissing-prototypes -Wno-missing-field-initializers -Wredundant-decls -Wsign-compare -Wtype-limits -Wuninitialized -Wunused-but-set-parameter -Wunused-but-set-variable -Wunused-parameter -Wunused-result -Wunused-variable -Wnested-externs -Wpointer-arith -Wstrict-prototypes -Wformat-security -Wimplicit-function-declaration -isystem/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/sysroots/x86_64-linux/usr/include -O2 -pipe -c -o schedutils/chrt.o ../util-linux-2.28.1/schedutils/chrt.c
| In file included from /usr/include/x86_64-linux-gnu/sys/syscall.h:31:0,
| from ../util-linux-2.28.1/schedutils/chrt.c:63:
| ../util-linux-2.28.1/schedutils/chrt.c: In function ‘sched_setattr’:
| ../util-linux-2.28.1/schedutils/chrt.c:88:17: error: ‘__NR_sched_setattr’ undeclared (first use in this function)
| return syscall(SYS_sched_setattr, pid, attr, flags);
| ^
| ../util-linux-2.28.1/schedutils/chrt.c:88:17: note: each undeclared identifier is reported only once for each function it appears in
| ../util-linux-2.28.1/schedutils/chrt.c: In function ‘sched_getattr’:
| ../util-linux-2.28.1/schedutils/chrt.c:93:17: error: ‘__NR_sched_getattr’ undeclared (first use in this function)
| return syscall(SYS_sched_getattr, pid, attr, size, flags);
| ^
| ../util-linux-2.28.1/schedutils/chrt.c: In function ‘sched_setattr’:
| ../util-linux-2.28.1/schedutils/chrt.c:89:1: warning: control reaches end of non-void function [-Wreturn-type]
| }
| ^
| ../util-linux-2.28.1/schedutils/chrt.c: In function ‘sched_getattr’:
| ../util-linux-2.28.1/schedutils/chrt.c:94:1: warning: control reaches end of non-void function [-Wreturn-type]
| }
| ^
| make[2]: *** [schedutils/chrt.o] Error 1
| make[2]: Leaving directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build'
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory `/home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/build'
| make: *** [all] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/fsl/fsl-release-bsp/fsl-release-bsp/build-gateway/tmp/work/x86_64-linux/util-linux-native/2.28.1-r0/temp/log.do_compile.7660)
ERROR: Task (virtual:native:/home/fsl/fsl-release-bsp/fsl-release-bsp/sources/poky/meta/recipes-core/util-linux/util-linux_2.28.1.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 621 tasks of which 606 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
virtual:native:/home/fsl/fsl-release-bsp/fsl-release-bsp/sources/poky/meta/recipes-core/util-linux/util-linux_2.28.1.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,512件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Lille Li,

This error looks like the one on the following link, where the problem was some of the packages required by the host, maybe that will help:

https://community.nxp.com/thread/472545

Regards,

0 件の賞賛
返信

1,512件の閲覧回数
lilleli
Contributor I

Thank fsl community,now  have other problem,

CanI build imx6ull image in the win10+vmware +unbuntu 14.4 platform?

we meet a seriour problem ,offen stop in virtul machine worker!

0 件の賞賛
返信

1,512件の閲覧回数
lilleli
Contributor I

hello community,

     I single compile kernel ,use below command,but have some prolbem:

bitbake -c menuconfig -v linux-imx 

pastedImage_1.png

0 件の賞賛
返信