build Yocto imx-3.10.53-1.1.2_patch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build Yocto imx-3.10.53-1.1.2_patch

1,288 次查看
panmin
Contributor I

when i build yocto project of imx-3.10.53-1.1.2_patch,i cannot finished it ,here are same information,how can i fix it ,thanks

my command:

MACHINE=imx6qsabreauto source fsl-setup-release.sh -b build-fb -e fb

bitbake core-image-minimal

Loading cache: 100% |#################################################################################################| ETA:  00:00:00

Loaded 2182 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.6.2"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):30b8d9378b8260e452552b806610dc9b6fe0b69f"

meta-oe           = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-fsl-arm      = "(nobranch):9bc540eec9a7e280af13371ea70650fcc47ea627"

meta-fsl-arm-extra = "(nobranch):e1085deb3d915d2a95a65cceadc77c6de0dadfb6"

meta-fsl-demos    = "(nobranch):f141c7d1158b8addbd6f1ed047a1b47c2ed85f8f"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):4608ca9b90b4f5c37c318a3eada4d760d016cfa5"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome       

meta-networking  

meta-ruby         = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-qt5          = "(nobranch):c29c317e0f22202bfaa85329a580564bbc179089"

meta-fsl-qt5     

meta-fsl-bluez    = "(nobranch):4608ca9b90b4f5c37c318a3eada4d760d016cfa5"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: Unpack failure for URL: 'http://www.python.org/ftp/python/2.7.3/Python-2.7.3.tar.bz2'. Unpack command PATH="/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/python-native:/home/pm/fsl-arm-yocto-bsp/sources/poky/scripts:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/bin/crossscripts:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/pm/fsl-arm-yocto-bsp/sources/poky/scripts:/home/pm/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games" bzip2 -dc /home/pm/fsl-arm-yocto-bsp/downloads/Python-2.7.3.tar.bz2 | tar x --no-same-owner -f - failed with return value 2

ERROR: Logfile of failure stored in: /home/pm/fsl-arm-yocto-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/python/2.7.3-r0.3/temp/log.do_unpack.31762

Log data follows:

| DEBUG: Executing python function do_unpack

| DEBUG: Executing python function base_do_unpack

| NOTE: Unpacking /home/pm/fsl-arm-yocto-bsp/downloads/Python-2.7.3.tar.bz2 to /home/pm/fsl-arm-yocto-bsp/build-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/python/2.7.3-r0.3/

|

| bzip2: Compressed file ends unexpectedly;

|     perhaps it is corrupted?  *Possible* reason follows.

| bzip2: Success

|     Input file = /home/pm/fsl-arm-yocto-bsp/downloads/Python-2.7.3.tar.bz2, output file = (stdout)

|

| It is possible that the compressed file(s) have become corrupted.

| You can use the -tvv option to test integrity of such files.

|

| You can use the `bzip2recover' program to attempt to recover

| data from undamaged sections of corrupted files.

|

| tar: Unexpected EOF in archive

| tar: Unexpected EOF in archive

| tar: Error is not recoverable: exiting now

| DEBUG: Python function base_do_unpack finished

| DEBUG: Python function do_unpack finished

| ERROR: Function failed: Unpack failure for URL: 'http://www.python.org/ftp/python/2.7.3/Python-2.7.3.tar.bz2'. Unpack command PATH="/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/python-native:/home/pm/fsl-arm-yocto-bsp/sources/poky/scripts:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/bin/crossscripts:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/pm/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/pm/fsl-arm-yocto-bsp/sources/poky/scripts:/home/pm/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games" bzip2 -dc /home/pm/fsl-arm-yocto-bsp/downloads/Python-2.7.3.tar.bz2 | tar x --no-same-owner -f - failed with return value 2

ERROR: Task 873 (/home/pm/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/python/python_2.7.3.bb, do_unpack) failed with exit code '1'

NOTE: Tasks Summary: Attempted 572 tasks of which 569 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/pm/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/python/python_2.7.3.bb, do_unpack

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

0 项奖励
回复
1 回复

967 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Are you still having problems baking this image?

I would review that all necessary packages are included; did you install all packages required by the Yocto User Guide?

0 项奖励
回复