broad com wifi bcm4329 cross compiling issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

broad com wifi bcm4329 cross compiling issue

1,015 次查看
veeranjaneyulug
Contributor III

Hi

Good day every one .

How to compile the broad com wifi driver in linux kernel 3.14.28 version .Is it supported? where its located in driver file and make menuconfig.Can you explain how to cross compile and how to insert the modules on to the target board.

And how to bootup the wifi on imx6 target board.

And then how to boot from emmc on imx6 target board.send me emmc default bootargs .

Thanks & Regards

veera

0 项奖励
回复
1 回复

894 次查看
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

seems bcm4329 is used on wandboard, so one can look at its sources

http://wandboard.org/70-20140519-wandboard-rev-c1 

https://github.com/wandboard-org/linux/tree/wandboard_imx_3.14.28_1.0.0_ga

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复