boot up from SPI-NOR flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

boot up from SPI-NOR flash

跳至解决方案
7,727 次查看
carmilili
Contributor III

Have a custom device based on the i.MX6Q processor and have some problem with booting up from SPI-NOR flash.

Using the same file of u-boot.bin burn to SD card,eMMC and SPI-NOR flash.

It can booting up from SD card and eMMC successfully.

But boot up from SPI-NOR flash, when I use the command of "print".

There is no environment variable.


CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 189

Temperature:   31 C, calibration data 0x5a95097d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]

Boot Device: SPI NOR

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Card did not respond to voltage select!

MMC init failed

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=11

Net:   got MAC address from IIM: 00:04:9f:02:b1:af

FEC0

MX6Q SABRESD U-Boot > print

stdin=serial

stdout=serial

stderr=serial

ethact=FEC0

Environment size: 53/8188 bytes

MX6Q SABRESD U-Boot >

SPI-NOR flash connect to SPI3.The chip select is cs0.

I burn the u-boot image to SPI-NOR flash by MfgTool.

Does someone know  what is the problem may be?

Do I need to config the pin of SPI3 no the code of u-boot?

What can I have a try?

标签 (3)
0 项奖励
回复
1 解答
5,540 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

For SPI NOR flash support, you can reference to the uboot head file "include/configs/mx6q_sabrelite.h", this board was designed for SPI NOR boot.

You should make sure there is the followed setting in your uboot config file:

#define CONFIG_CMD_SPI

#define CONFIG_CMD_SF

#ifdef CONFIG_CMD_SF

#define CONFIG_FSL_SF  1

#define CONFIG_SPI_FLASH_IMX_SST 1

#define CONFIG_SPI_FLASH_CS 0

#define CONFIG_IMX_ECSPI

#define IMX_CSPI_VER_2_3 1

#define MAX_SPI_BYTES  (64 * 4)

#endif

#elif defined(CONFIG_FSL_ENV_IN_SF)

#define CONFIG_ENV_IS_IN_SPI_FLASH 1

#define CONFIG_ENV_SPI_CS  0

#define CONFIG_ENV_OFFSET       (768 * 1024)

#else

在原帖中查看解决方案

0 项奖励
回复
5 回复数
5,541 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

For SPI NOR flash support, you can reference to the uboot head file "include/configs/mx6q_sabrelite.h", this board was designed for SPI NOR boot.

You should make sure there is the followed setting in your uboot config file:

#define CONFIG_CMD_SPI

#define CONFIG_CMD_SF

#ifdef CONFIG_CMD_SF

#define CONFIG_FSL_SF  1

#define CONFIG_SPI_FLASH_IMX_SST 1

#define CONFIG_SPI_FLASH_CS 0

#define CONFIG_IMX_ECSPI

#define IMX_CSPI_VER_2_3 1

#define MAX_SPI_BYTES  (64 * 4)

#endif

#elif defined(CONFIG_FSL_ENV_IN_SF)

#define CONFIG_ENV_IS_IN_SPI_FLASH 1

#define CONFIG_ENV_SPI_CS  0

#define CONFIG_ENV_OFFSET       (768 * 1024)

#else

0 项奖励
回复
5,540 次查看
乐乐季
Contributor I

HI Qiang:

I want to update uboot2013.

my step:

1.MX6QSABRELITE U-Boot > tftp u-boot.imx    //Load address: 0x12000000

2.MX6QSABRELITE U-Boot > sf probe

3.MX6QSABRELITE U-Boot > sf erase 0 50000

4.MX6QSABRELITE U-Boot > sf write 12000000 0 4ed14 // uboot2013 size is 4ed14

But I reboot,my board without serial print information.

If I update uboot2009,it is Success.

please help me ! thank you!

0 项奖励
回复
5,540 次查看
乐乐季
Contributor I

I solved the problem:

  sf probe

  sf erase 0 +0x50000

  sf write 0x10800000 0x400 0x50000

but I don't understand why 0x400 as the starting address?

please!

0 项奖励
回复
5,540 次查看
AnsonHuang
NXP Employee
NXP Employee

maybe you used uboot 2014, right, as we did NOT add 0x400 offset on uboot image from uboot 2014, so you need to program from offset 0x400 on spi flash. you can compare the uboot binary content between uboot 2009 and uboot 2014.

0 项奖励
回复
5,540 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Carmili

     As far as I know, we did NOT have spi nor uboot enabled for i.MX6Q SabreSD board, only have it in SabreAuto board. So can you let me know which config you used to build spi -nor u-boot you flashed into the board? We can see that in include/configs/mx6q_sabreauto_spi-nor.h, there is definition about CONFIG_FSL_ENV_IN_SF and the offset of ENV, you may need to check them.