boot up by tftpboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot up by tftpboot

1,497 次查看
mm2021
Contributor III

I'm debugging the i.MX 8M Mini board.

Now I can compile the kernel and get Image file. I put the Image file to SD card to replace the old one, the board can boot up to linux smoothly.
Now I'd like to get Image in ubbot by tftpboot.

As far as I know, in uboot, I can use the following command to load Image to ram:
tftp <addr in ram> Image

But how to set the address in ddr?

Thanks!

 

0 项奖励
回复
2 回复数

1,468 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi @mm2021,

 

Please read the Linux user guide, chapter 4.4.1.2 Downloading an image to MMC/SD, there you will find how to do the configuration and the steps to follow.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 

For the loadaddr I think it is 0x40480000, also you could see this address if you, on U-boot write printenv and look for that address.

 

Hope this helps you.

Regards,

Israel.

0 项奖励
回复

1,488 次查看
mm2021
Contributor III

anybody can give some ideas?

0 项奖励
回复