boot time optimisation reg(kernel side)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot time optimisation reg(kernel side)

1,883件の閲覧回数
sachusanal
Contributor III

Dear Sir ,

 

i have mx6qsabresd  board with me,when i flashing the image after the boot loader loading for the kernel booting so mant time is taken,and also i need to set a spalsh screen in kernel but  the splash screen is loading after 6or 7 seconds, a blank screen is loading i need to avoid that blank screen also please help me to solve this issue

I here by attch my .config  file for your reference.

Original Attachment has been moved to: .config.zip

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,614件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sachu

suggest to look at below link

Linux Fast Boot on i.MX6 Sabresd Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,614件の閲覧回数
sachusanal
Contributor III

In my kernel i set one splash screen but the splash screen is loading at last of the kernel section.

after the starting kernel print on terminal get along time to load splash  screen what should i do

0 件の賞賛
返信