boot time optimisation reg(kernel side)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot time optimisation reg(kernel side)

1,897 Views
sachusanal
Contributor III

Dear Sir ,

 

i have mx6qsabresd  board with me,when i flashing the image after the boot loader loading for the kernel booting so mant time is taken,and also i need to set a spalsh screen in kernel but  the splash screen is loading after 6or 7 seconds, a blank screen is loading i need to avoid that blank screen also please help me to solve this issue

I here by attch my .config  file for your reference.

Original Attachment has been moved to: .config.zip

Labels (1)
0 Kudos
Reply
2 Replies

1,628 Views
igorpadykov
NXP Employee
NXP Employee

Hi sachu

suggest to look at below link

Linux Fast Boot on i.MX6 Sabresd Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,628 Views
sachusanal
Contributor III

In my kernel i set one splash screen but the splash screen is loading at last of the kernel section.

after the starting kernel print on terminal get along time to load splash  screen what should i do

0 Kudos
Reply