boot.scr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot.scr

10,519 Views
Afeefah
Contributor I

The boot process failed to load boot.scr. Getting a print "Failed to load 'boot.scr'" while booting device.

0 Kudos
Reply
10 Replies

10,502 Views
Afeefah
Contributor I

I'm using imx6ull and BSP version is 5.15.52

 

0 Kudos
Reply

10,505 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Can you tell us which board and which version BSP are you using?

0 Kudos
Reply

10,486 Views
Afeefah
Contributor I

Hi Nxp community,

I'm using 5.15.52 BSP version and iMx6ull board. The booting gets completed but failure prints are observed. Could you please let me know what is causing this? Also please let me know how I can solve this.

Thank you,

Afeefah Fathima

0 Kudos
Reply

10,480 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

can you share the boot log file to us?

0 Kudos
Reply

10,474 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP reference board or the board you designed yourself? Here ignore this information, your kernel can not boot up success and the boot.scr can not cause your kernel can not boot.

Can you share us your boot command for the kernel boot? When u-boot boot up, press print and share us your boot command for the kernel boot.

0 Kudos
Reply

10,461 Views
Afeefah
Contributor I

We have our own board in which we are using NXP's iMx6ull processor. I have shared details about kernel boot.

0 Kudos
Reply

10,450 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

you can try to add the earlycon=ec_imx6q,uart baseaddress,115200 in your boot command mmcargs.

For the uart baseaddress you need to confirm your use.

0 Kudos
Reply

10,443 Views
Afeefah
Contributor I

Hi @Rita_Wang 

The value for earlycon is already set as 

bootargs = "console=ttymxc2,115200 earlycon=ec_imx6q,0x30880000,115200";

what could be the other possibilities? Is there any other suggestion.

 

0 Kudos
Reply

10,469 Views
Afeefah
Contributor I

Below is the screenshot attached of boot log.

0 Kudos
Reply

8,370 Views
chillinwithscb
Contributor III
Since the kernel loads, I wonder whether the message about boot.scr is important or not.
0 Kudos
Reply