boot problem for IMX6 SABRE_SD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot problem for IMX6 SABRE_SD board

Jump to solution
10,341 Views
vjwan
Contributor I

Hi everyone,

I start to use IMX6 SABRE_SD board recently. The original boot is eMMC for android. The DIP switch (SW6) configuration is 1101 0110 (1 is on). The screen (LG LP101WH1) is connected to LVDS1.

Now I want to change to boot linux from a 32G SD card. Command 

     sudo dd if=fsl-image-gui-imx6qsabresd-20140118115633.rootfs.sdcard of=/dev/sdb bs=1M && sync

is used to deploy SD image (reference document "Freescale Yocto User’s Guide"). The DIP switch configuration is changed to 0110 0010. LVDS is changed to connect LVDS0. "video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666" is set by command
     setenv bootargs_mmc 'setenv bootargs video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666'

After booting, there is no display in the screen.

Another question is when I use mmcblk0p2, the system can boot. If using mmcblk0p1 or mmcblk1p2 (In the document “i.MX 6Dual/6Quad SABRE-SD Linux Release Notes”,root=/dev/mmcblk1p2 for "boot from SD"), the boot fails. It seems like that mmcblk0p2 is booting from eMMC.

Anyone know how to solove the problem? Thanks a lot!

Here is the u-boot config :
-------------------------------------------------
U-Boot > printenv
baudrate=115200
boot_fdt=try
bootargs_mmc=setenv bootargs video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666
bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run

mmcboot; else run netboot; fi; fi; else run netboot; fi
bootdelay=1
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
ethact=FEC
ethaddr=00:04:9f:02:6a:57
ethprime=FEC
fdt_addr=0x18000000
fdt_file=imx6q-sabresd.dtb
fdt_high=0xffffffff
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt;

then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi;

fi; else bootm; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk0p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd

tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr}

${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load

the DT; fi; fi; else bootm; fi;
script=boot.scr
uimage=uImage
update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev};

then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc

write ${loadaddr} 0x2 ${fw_sz}; fi; fi


The  kernel log :
-------------------------------------------------
U-Boot 2013.10 (Jan 18 2014 - 03:13:56)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: MX6-SabreSD
DRAM:  1 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to HDMI
Display: HDMI (1024x768)
In:    serial
Out:   serial
Err:   serial
Net:   FEC [PRIME]
Hit any key to stop autoboot:  0
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading uImage
4042504 bytes read in 186 ms (20.7 MiB/s)
Booting from mmc ...
reading imx6q-sabresd.dtb
** Unable to read file imx6q-sabresd.dtb **
## Booting kernel from Legacy Image at 12000000 ...
   Image Name:   Linux-3.0.35-4.1.0+yocto+gbdde70
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4042440 Bytes = 3.9 MiB
   Load Address: 10008000
   Entry Point:  10008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 3.0.35-4.1.0+yocto+gbdde708 (liuxi@liuxi-laptop) (gcc version 4.8.1 (GCC) ) #1 SMP PREEMPT Sat Jan 18 02:31:20 CST 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @8c008000 s5792 r8192 d14688 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 194560
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 512MB 256MB = 768MB total
Memory: 765064k/765064k available, 283512k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)
    vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)
    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .init : 0x80008000 - 0x8003e000   ( 216 kB)
      .text : 0x8003e000 - 0x80b0e5b8   (11074 kB)
      .data : 0x80b10000 - 0x80b7c1f0   ( 433 kB)
       .bss : 0x80b7c214 - 0x80bf0690   ( 466 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
devtmpfs: initialized
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: SPKVDD: 4200 mV
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2500 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
max17135 2-0048: PMIC MAX17135 for eInk display
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = c0880000 suspend_iram_base=c091c000
PM driver module loaded
IMX usb wakeup probe
add wake up source irq 75
IMX usb wakeup probe
cpu regulator mode:ldo_bypass
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 1494
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.3: ipu1-di0 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
No sata disk.
m25p80 spi0.0: unrecognized JEDEC id ffffff
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1
egalax_ts 1-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -22
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
mag3110 2-000e: check mag3110 chip ID
input: mag3110 as /devices/virtual/input/input2
mag3110 2-000e: mag3110 is probed
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
input: mma845x as /devices/virtual/input/input3
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
Galcore version 4.6.9.6622
Thermal calibration data is 0x56c4b17d
Thermal sensor with ratio = 179
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SU32G 29.7 GiB
mmcblk0: p1 p2
wm8962 0-001a: customer id 0 revision D
input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input4
asoc: wm8962 <-> imx-ssi.1 mapping ok
input: wm8962-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input5
input: wm8962-audio Ext Spk as /devices/platform/soc-audio.5/sound/card0/input6
imx_3stack asoc driver
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
  #0: wm8962-audio
NET: Registered protocol family 26
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 2014-01-18 23:00:10 UTC (1390086010)
EXT3-fs: barriers not enabled
kjournald starting.  Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 216K
mmc1: new high speed DDR MMC card at address 0001
mmcblk1: mmc1:0001 SEM08G 7.39 GiB
mmcblk1boot0: mmc1:0001 SEM08G partition 1 2.00 MiB
mmcblk1boot1: mmc1:0001 SEM08G partition 2 2.00 MiB
mmcblk1: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk1boot1: unknown partition table
mmcblk1boot0: unknown partition table
INIT: version 2.88 booting
Starting udev
udevd[105]: starting version 182
Starting Bootlog daemon: ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
ov5640_read_reg:write reg error:reg=300a
bootlogd.
camera ov5640_mipi is not found
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
ALSA: Restoring mixer settings...
Configuring network interfaces... EXT4-fs (mmcblk1p7): warning: checktime reached, running e2fsck is recommended
EXT4-fs (mmcblk1p4): warning: checktime reached, running e2fsck is recommended
EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk1p6): warning: checktime reached, running e2fsck is recommended
eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)
EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: (null)
udhcpc (v1.21.1) started
Sending discover...
PHY: 1:01 - Link is Up - 100/Full
Sending discover...
Sending select for 192.168.0.17...
Lease of 192.168.0.17 obtained, lease time 86400
/etc/udhcpc.d/50default: Adding DNS 192.168.0.1
done.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
INIT: Entering runlevel: 5
Starting Xserver
Starting system message bus: dbus.
Starting Connection Manager
Starting Dropbear SSH server: dropbear.
Starting advanced power management daemon: apmd.
apmd[578]: apmd 3.2.1 interfacing with apm driver 1.13 and APM BIOS 1.2
creating NFS state directory: eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)
done
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
   ...fail!
Starting Telephony daemon
Starting Linux NFC daemon
Starting OProfileUI server
Running local boot scripts (/etc/rc.local).

** (oprofile-server:642): WARNING **: Failed to create avahi client: Daemon not running
Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.5.1 imx6qsabresd /dev/ttymxc0

imx6qsabresd login:

Regards,

VJ

Labels (3)
1 Solution
3,280 Views
vjwan
Contributor I

Hi Weidong,

Thanks for your reply. It turns out that we need to change ldb_modedb in ldb.c. For LG LP101WH1 TLB!,

     "LDB-LXGA", 60, 1360, 768, 13825,

      80, 48,

      14, 3,

      32, 5,

      0,

      FB_VMODE_NONINTERLACED,

      FB_MODE_IS_DETAILED

Also we need add ldb=dul0 at the end of video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666'


Regards,

VJ

View solution in original post

0 Kudos
Reply
3 Replies
3,280 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello, VJ,

     From booting log you provided on above, partitions of your SD card is android, Why did you use Yocto images to boot android system ? Linux BSP was released in Yocto ! Not android BSP.

...

mmc1: new high speed DDR MMC card at address 0001

mmcblk1: mmc1:0001 SEM08G 7.39 GiB

mmcblk1boot0: mmc1:0001 SEM08G partition 1 2.00 MiB

mmcblk1boot1: mmc1:0001 SEM08G partition 2 2.00 MiB

mmcblk1: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

mmcblk1boot1: unknown partition table

mmcblk1boot0: unknown partition table

...

   Please use fdisk command to re-partition SD card for linux system! Then use dd command to copy images to SD !

----------- I tested booting from SD card , it's no problem, following is what I did ,just an example for you -------

sudo dd if= fsl-image-x11-imx6qsabresd-20140103025526.rootfs.sdcard of=/dev/sdb bs=512

Regards,

Weidong

0 Kudos
Reply
3,281 Views
vjwan
Contributor I

Hi Weidong,

Thanks for your reply. It turns out that we need to change ldb_modedb in ldb.c. For LG LP101WH1 TLB!,

     "LDB-LXGA", 60, 1360, 768, 13825,

      80, 48,

      14, 3,

      32, 5,

      0,

      FB_VMODE_NONINTERLACED,

      FB_MODE_IS_DETAILED

Also we need add ldb=dul0 at the end of video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666'


Regards,

VJ

0 Kudos
Reply
3,280 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi VJ,

Have you solved your problem? If yes, Please click Correct Answer/Helpful Answer. Thanks a lot~~

Best Regards

Dan

0 Kudos
Reply