boot mode pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,789件の閲覧回数
sapirbuz
Contributor IV

Hi,

 

MIMXRT1051CVL5B.

We would like to use 2 boot options on our design: boot from fuse and boot from serial downloader.

Must we keep the boot_mode[1,0] pins to define the boot mode on the fly? Or can we define it by SW and use the boot_mode[1,0] as GPIO for another purpose?

0 件の賞賛
返信
1 解決策
2,773件の閲覧回数
jay_heng
NXP Employee
NXP Employee

We must place external PU/PD. as IOMUXC cfg register will be reset when power-on

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,781件の閲覧回数
jay_heng
NXP Employee
NXP Employee

boot mode pins status is sampled once power-on, when chip is booted, you can use boot mode pins as GPIOs. we cannot switch boot mode by SW.

2,775件の閲覧回数
sapirbuz
Contributor IV

can the boot mode pins be sampled according to the defined internal pull-up pull-down? or must we place external PU/PD?

sapirbuz_0-1655709082274.png

 

0 件の賞賛
返信
2,774件の閲覧回数
jay_heng
NXP Employee
NXP Employee

We must place external PU/PD. as IOMUXC cfg register will be reset when power-on

0 件の賞賛
返信