boot mode pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

boot mode pins

跳至解决方案
2,796 次查看
sapirbuz
Contributor IV

Hi,

 

MIMXRT1051CVL5B.

We would like to use 2 boot options on our design: boot from fuse and boot from serial downloader.

Must we keep the boot_mode[1,0] pins to define the boot mode on the fly? Or can we define it by SW and use the boot_mode[1,0] as GPIO for another purpose?

0 项奖励
回复
1 解答
2,780 次查看
jay_heng
NXP Employee
NXP Employee

We must place external PU/PD. as IOMUXC cfg register will be reset when power-on

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,788 次查看
jay_heng
NXP Employee
NXP Employee

boot mode pins status is sampled once power-on, when chip is booted, you can use boot mode pins as GPIOs. we cannot switch boot mode by SW.

2,782 次查看
sapirbuz
Contributor IV

can the boot mode pins be sampled according to the defined internal pull-up pull-down? or must we place external PU/PD?

sapirbuz_0-1655709082274.png

 

0 项奖励
回复
2,781 次查看
jay_heng
NXP Employee
NXP Employee

We must place external PU/PD. as IOMUXC cfg register will be reset when power-on

0 项奖励
回复