boot config pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot config pins

2,176 Views
sapirbuz
Contributor IV

Hi,

We are using MCU PN MIMXRT1051CVL5B.

The Boot will be through an external 8Mb serial NOR Flash using the NXP 3.3V FlexSPI port A secondary pins.

In our design, the only available config pins (that are used as configuration pins) are boot_mode[0] and boot_mode[1].

boot_cfc2[2:0] are GPIOs pins and can't be used as the boot configuration pins in our design because we planned to be in the boot from fuses mode and not the internal boot mode.

When we try to program the fuses by serial downloader, an error occurs saying that the external memory wasn't found.

How can we program the fuses without reading the boot_cfc2[2:0] and connecting to the external memory?

0 Kudos
Reply
4 Replies

2,159 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sapirbuz 

Could you please describe your question more detail and correct.

boot_cfc2[2:0] 

->> Do you meaning boot_cfg2[2:0]  ? And this is not pin, it is Fuse.

oot_mode[0] and boot_mode[1] are the boot pins.

 

BR

Alice

0 Kudos
Reply

2,151 Views
sapirbuz
Contributor IV

yes, boot_cfg[2:0]

0 Kudos
Reply

2,146 Views
sapirbuz
Contributor IV

We want to burn the fuses to define the secondary flash as a boot device, but we can't do it because we can't connect to the flashloader, and we can't connect to the flashloader because we can't burn the fuses.

please see the pictures below:

sapirbuz_0-1679412369368.png

 

sapirbuz_1-1679413107913.png

 

 

0 Kudos
Reply

2,156 Views
sapirbuz
Contributor IV

what data is missing? please elaborate

0 Kudos
Reply