bluetoothheadset can not work when using skype

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bluetoothheadset can not work when using skype

1,123件の閲覧回数
zhoubo699
Contributor I

HI all:

      I connected my bluetooth headset to I.MX6Q_SABRESD, and my BSP is linux-3.0.35, the buletooth headset can listen music ,but when I using the skype to call, the bluetooth headset can not work, I tried to connected the pcm pin of buletooth chip to esai interface on I.MX6Q_SABRESD, but it seems like the codec driver can not support the bluetooth headset communicate with the I.MX6Q_SABRESD,I referenced the i.MX_6_linux_reference_Manual,Unfortunately,I  did not find an answer ,what should I do in the driver so that the bluetooth headset can work when I using skype to call another one? thanks a lot,

0 件の賞賛
返信
1 返信

1,048件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bo

it may be recommended to try latest 4.x kernels which

may support it better

https://boundarydevices.com/mx6-kernel-4-1-0/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信