block app

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

block app

1,456 Views
marekbil
Contributor I

Hi, I have rs port in my device witch android. Port in device is local socket. How can I blocked install externall app from this socket ?

Labels (1)
0 Kudos
Reply
1 Reply

1,327 Views
b36401
NXP Employee
NXP Employee

Do you mean that you have wired network interface and you need to disable applications installation over this port?
You can disable http and https from this interface with firewall settings.
Or you can disable not whole http(s) but only the addresses like play.google.com.
This way you stop Google Play to work.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply