bitburner not recognized imx233

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitburner not recognized imx233

1,781 次查看
cesarpantoja
Contributor I

Hi

I have a custom board with imx233, the design has been tested before; but in this, when I prepare to blow fuses with bitburner simply does not recognize it and in the box where it should appear HID ... nothing comes, and I need configure for Boot from SD.

I tried all options in the boot pins and nothing, connectivity also was tested and everything seems in order.

The Bitburner Version and windows version is the same used in other cards equals.

other try to boot from usb with mxsldr but neither recognizes the imx233.

I appreciate any suggestion

标签 (1)
0 项奖励
回复
3 回复数

1,369 次查看
Yuri
NXP Employee
NXP Employee

  1. Is it possible to try using BitInit from the OTP TOOLs?

First the otp_burner.py script should be used to generate OtpInit.sb file that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

< https://www.freescale.com/webapp/Download?colCode=IMX_OPT_TOOLS&appType=license&location=null >

2.
As for USB HID detection, please check board USB OTG design :
- if all power voltages meet (i.Mx23) specifications ;
- if USB-5V is present ;
- if the (USB) recovery mode is selected correctly.   

0 项奖励
回复

1,369 次查看
cesarpantoja
Contributor I

Hi Yuri thanks for reply

I found that the voltages are not correct, I checked the decoupling capacitors, but I'm still looking for the cause

0 项奖励
回复

1,369 次查看
Yuri
NXP Employee
NXP Employee

"I found that the voltages are not correct" - so it makes sense to analyze power supply system.

0 项奖励
回复