bitbake yocto question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake yocto question

1,761件の閲覧回数
hnxylhb
Contributor I

WARNING: Failed to fetch URL http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 8, output:

http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:

2015-07-13 09:22:58 ERROR 404: Not Found.

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/jishuxing/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/imx-test-hdcp/3.10.17-1.0.0-r0/temp/log.do_fetch.3692

ERROR: Task 1667 (/home/jishuxing/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/imx-test/imx-test-hdcp_3.10.17-1.0.0.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2351 tasks of which 2350 didn't need to be rerun and 1 failed.

No currently running tasks (2350 of 4013)

ラベル(2)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello roc li,

Would you please provide more information on this error? Which BSP are you using and which images or packages are you baking? I’m curious because the binaries are not being downloaded from the gits but from Freescale.com

0 件の賞賛
返信