bitbake targets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake targets

2,236件の閲覧回数
slouchez
Contributor I

General question in 2 parts

(so general I know the information is somewhere but can't find what I need in the way I'm asking...)

{1] building for the imx28evk, I'm prompted by bitbake to choose between different 'levels' of functionality:

    core-image-minimal

    meta-toolchain

    meta-toolchain-sdk

    adt-installer

    meta-ide-support

Is there a description somewhere of these pre-defined options?

I'm after a 'development build" i.e. where I can compile on the target - console only no UI needed

This is while I learn to run with NFS to my Ubuntu host.

[2] eventually I will need to choose the contents of the file system. Is there a "How to" for that?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,867件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Most images would (and should) have some information on the actual .bb file as comments or in a separate readme file.

That being said the core-image-minimal option is as the name implies a minimal image for the i.MX28EVK that does not have graphics support so perhaps it will indeed suit your needs.

Some of the recipes you mentioned are actually not from images but from other kind of packages like meta-toolchain which serves to extract the toolchain in order to manually compile the kernel or other source code. You may find information on this feature in the following community document:

https://community.freescale.com/docs/DOC-95122

I would recommend looking at the Yocto Reference Manual of the poky version you’re using (1.7 for dizzy, link below) as you would need to create an image recipe in order to add the desired existing packages and the new packages that you would write.

http://www.yoctoproject.org/docs/1.7.1/mega-manual/mega-manual.html

I hope this information helps!

0 件の賞賛
返信