bitbake imx-image-core failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake imx-image-core failed

Jump to solution
3,681 Views
sheltonHe
Contributor I

Hello, nxp engineer, I am using nxp's yocto project (imx-yocto-LF5.10.9_1.0.0), I followed the "i.MX_Yocto_Project_Users_Guide.pdf" manual to build, and exited when compiling imx-boot, please ask this what is the problem? Is there a problem with the latest Yocto project? My compilation command and error message are as follows:

bitbake imx-image-core

 企业微信截图_16185668898073.png

 

ps:  imx8mplus evk 、 imx-yocto-LF5.10.9_1.0.0

 

Tags (1)
0 Kudos
Reply
1 Solution
3,659 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello SheltonHe,

 

You need to erase everything with bitbake -c cleanall and reinstall yocto in your system, for project image I recommned to start with the imx-image-full.

 

Regards

 

View solution in original post

0 Kudos
Reply
5 Replies
3,660 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello SheltonHe,

 

You need to erase everything with bitbake -c cleanall and reinstall yocto in your system, for project image I recommned to start with the imx-image-full.

 

Regards

 

0 Kudos
Reply
3,646 Views
sheltonHe
Contributor I

Okay thank you! I would like to ask where can I download the documentation for unit_test?

0 Kudos
Reply
3,637 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

This should be in the ref. manual of linux BSP, you can download the proper documentation of your BSP on:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...

 

0 Kudos
Reply
3,628 Views
sheltonHe
Contributor I

Thank you,i find it.

0 Kudos
Reply
3,668 Views
sheltonHe
Contributor I

Hello?Asking for help

0 Kudos
Reply