bitbake image stucks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,660件の閲覧回数
572038173
Contributor I

when i tried Yocto downloading using command "bitbake imx-image-multimedia",it always stuck in blow task:

     Currently 1 running tasks (1817 of 7206) 25% |######### |
      0: opencv-4.2.0.imx-r0 do_fetch (pid 2525)

I have checked disk usage,it;s about 43GB and stops growing.I try to restart bitbake ,but it still stuck in the same place. 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
4,575件の閲覧回数
iris_wen
NXP Employee
NXP Employee

Hi Jingjie,

Usually "do_fetch" error or stuck is caused by network issue. Please check your network or change a new network and try in different time.

If you have used yocto to compile successfully before, you can directly copy the relevant files downloaded before to the current project. This way you can skip the "do_fetch" step.

元の投稿で解決策を見る

2 返答(返信)
4,576件の閲覧回数
iris_wen
NXP Employee
NXP Employee

Hi Jingjie,

Usually "do_fetch" error or stuck is caused by network issue. Please check your network or change a new network and try in different time.

If you have used yocto to compile successfully before, you can directly copy the relevant files downloaded before to the current project. This way you can skip the "do_fetch" step.

4,575件の閲覧回数
572038173
Contributor I

I have solve this problem by restart Ubuntu,thank you.

0 件の賞賛
返信