bitbake image stucks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake image stucks

Jump to solution
4,649 Views
572038173
Contributor I

when i tried Yocto downloading using command "bitbake imx-image-multimedia",it always stuck in blow task:

     Currently 1 running tasks (1817 of 7206) 25% |######### |
      0: opencv-4.2.0.imx-r0 do_fetch (pid 2525)

I have checked disk usage,it;s about 43GB and stops growing.I try to restart bitbake ,but it still stuck in the same place. 

Tags (2)
0 Kudos
Reply
1 Solution
4,564 Views
iris_wen
NXP Employee
NXP Employee

Hi Jingjie,

Usually "do_fetch" error or stuck is caused by network issue. Please check your network or change a new network and try in different time.

If you have used yocto to compile successfully before, you can directly copy the relevant files downloaded before to the current project. This way you can skip the "do_fetch" step.

View solution in original post

2 Replies
4,565 Views
iris_wen
NXP Employee
NXP Employee

Hi Jingjie,

Usually "do_fetch" error or stuck is caused by network issue. Please check your network or change a new network and try in different time.

If you have used yocto to compile successfully before, you can directly copy the relevant files downloaded before to the current project. This way you can skip the "do_fetch" step.

4,564 Views
572038173
Contributor I

I have solve this problem by restart Ubuntu,thank you.

0 Kudos
Reply