bitbake image-qt5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake image-qt5

623 次查看
fanyazhou
Contributor I

hello

 

WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###############################################################################################################################################################################| ETA: 00:00:00
Loaded 2843 entries from dependency cache.
Parsing recipes: 100% |#############################################################################################################################################################################| Time: 00:00:00
Parsing of 2258 .bb files complete (2256 cached, 2 parsed). 2842 targets, 441 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabresd"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-3.0.0"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"
meta-mie = "<unknown>:<unknown>"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
$<50>WARNING: u-boot-imx-2016.03-r0 do_fetch: Failed to fetch URL git://git.freescale.com/imx/uboot-imx.git;protocol=git;branch=imx_v2016.03_4.1.15_2.0.0_ga, attempting MIRRORS if available
$<50>ERROR: u-boot-imx-2016.03-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/dev/project/common/Yocto/Krogoth/fsl-release-bsp/downloads//git2/git.freescale.com.imx.uboot-imx.git'...
fatal: unable to connect to git.freescale.com:
git.freescale.com: Name or service not known


$<50>ERROR: u-boot-imx-2016.03-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/uboot-imx.git;protocol=git;branch=imx_v2016.03_4.1.15_2.0.0_ga'. Unable to fetch URL from any source.
$<50>ERROR: Logfile of failure stored in: /home/dev/project/common/Yocto/Krogoth/fsl-release-bsp/build_mie/tmp/work/imx6qsabresd-poky-linux-gnueabi/u-boot-imx/2016.03-r0/temp/log.do_fetch.77695
$<50>ERROR: Task 171 (/home/dev/project/common/Yocto/Krogoth/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2016.03.bb, do_fetch) failed with exit code '1'
$<50>NOTE: Tasks Summary: Attempted 3590 tasks of which 3589 didn't need to be rerun and 1 failed.
No currently running tasks (2262 of 3610)

Summary: 1 task failed:
/home/dev/project/common/Yocto/Krogoth/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2016.03.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 项奖励
回复
1 回复

609 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @fanyazhou 

I hope you are doing well.

->Please make sure to stick to the host ubuntu version the doc is verified for.
->Please make sure while building the image, that ISP is restricting some URLs that are required to fetch.

Please follow section 8.1 as mentioned in the doc.
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

Thanks & Regards.

Sanket Parekh

0 项奖励
回复