bitbake fsl-image-qt5-validation-imx error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake fsl-image-qt5-validation-imx error

5,731 次查看
lingguan
Contributor II

Hi,

I have recently purchased imx8mqevk board.

I have installed ubuntu16.04 in the vmware

I have download the yocto project by using "repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml".

Then I run the commond:

->"DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-xwayland"

->"bitbake fsl-image-qt5-validation-imx"

but there are some errors:

"ERROR: Task (/home/ling/bin/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qt3d_git.bb:do_compile) failed with exit code '1'

"

error log:

"

/usr/src/debug/qt3d/5.9.4+gitAUTOINC+02d01a6897-r0/git/src/3rdparty/assimp/code/IFCLoader.cpp:255: undefined reference to `Assimp::IFC::GetSchema(Assimp::STEP::EXPRESS::ConversionSchema&)'
| collect2: error: ld returned 1 exit status
| Makefile:875: recipe for target '../../bin/qgltf' failed
| make[2]: *** [../../bin/qgltf] Error 1
| make[2]: Leaving directory '/home/ling/bin/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/qt3d/5.9.4+gitAUTOINC+02d01a6897-r0/build/tools/qgltf'
| Makefile:44: recipe for target 'sub-qgltf-make_first' failed
| make[1]: *** [sub-qgltf-make_first] Error 2
| make[1]: Leaving directory '/home/ling/bin/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/qt3d/5.9.4+gitAUTOINC+02d01a6897-r0/build/tools'
| Makefile:72: recipe for target 'sub-tools-make_first' failed
| make: *** [sub-tools-make_first] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/ling/bin/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/qt3d/5.9.4+gitAUTOINC+02d01a6897-r0/temp/log.do_compile.7295)

"

Can anyone help me?

Sincerely.

标签 (1)
0 项奖励
回复
7 回复数

3,671 次查看
zhaoem82
Contributor I

I have installed all of package listed in the yocto user guide,I have the same issue,How can I do?

0 项奖励
回复

3,671 次查看
lingguan
Contributor II

May be you can use imx-4.9.51

0 项奖励
回复

3,671 次查看
zhenyongliu
Contributor I

I have the same issue, have you solve it? The only different from yours is that I am trying to use "repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-morty -m imx-4.9.51-8mq_ga.xml".  Is there any progress in your site?

0 项奖励
回复

3,671 次查看
lingguan
Contributor II

Hi, 643651564 QQ and wechat. 讨论讨论。

0 项奖励
回复

3,671 次查看
joanxie
NXP TechSupport
NXP TechSupport

have you installed all of package listed in the yocto user guide? if not, pls refer to the chapter 3.1 Host packages of user guide, and install all of them

0 项奖励
回复

3,671 次查看
joanxie
NXP TechSupport
NXP TechSupport

try to clean and build again

https://community.nxp.com/thread/353311 

0 项奖励
回复

3,671 次查看
lingguan
Contributor II

Thank you for your reply. I have already try to clean the project by

" bitbake -c clean fsl-image-qt5-validation-imx ", but can not solve my error.

The error log :

"

make[5]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtextlist'
cd qinputcontrol/ && ( test -e Makefile || /home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/git/tests/auto/gui/text/qinputcontrol/qinputcontrol.pro -qtconf /home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/bin/qt.conf ) && make -f Makefile
make[5]: Entering directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtexttable'
make[5]: Nothing to be done for `first'.
make[5]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtexttable'
make[5]: Entering directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtextscriptengine'
make[5]: Nothing to be done for `first'.
make[5]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtextscriptengine'
make[5]: Entering directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtextobject'
make[5]: Nothing to be done for `first'.
make[5]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qtextobject'
make[5]: Entering directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qinputcontrol'
make[5]: Nothing to be done for `first'.
make[5]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text/qinputcontrol'
make[4]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui/text'
make[3]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto/gui'
make[2]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests/auto'
make[1]: *** [sub-auto-make_first] Error 2
make[1]: Leaving directory `/home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/build/tests'
make: *** [sub-tests-make_first] Error 2
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_compile (log file is located at /home/ling/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-mx8mq-poky-linux/qtbase/5.9.4+gitAUTOINC+0d9208cecb-r0/temp/log.do_compile.11936)

"

0 项奖励
回复