bitbake fsl-image-qt5 error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake fsl-image-qt5 error

1,181 Views
ahljzdh
Contributor I

imx6ull  yocto项目构建

出错信息如下:

WARNING: linuxptp-1.6-r0 do_fetch: Failed to fetch URL http://sourceforge.net/projects/linuxptp/files/v1.6/linuxptp-1.6.tgz, attempting MIRRORS if available
WARNING: cpuburn-neon-20140626-r0 do_fetch: Failed to fetch URL https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..., attempting MIRRORS if available
WARNING: ntp-4.2.8p7-r0 do_fetch: Failed to fetch URL http://www.eecis.udel.edu/~ntp/ntp_spool/ntp4/ntp-4.2/ntp-4.2.8p7.tar.gz, attempting MIRRORS if available
WARNING: vlan-1.9-r0 do_fetch: Failed to fetch URL http://vlan.sourcearchive.com/downloads/1.9-3ubuntu9/vlan_1.9.orig.tar.gz, attempting MIRRORS if available
WARNING: ptpd-2.3.1-r0 do_fetch: Failed to fetch URL http://downloads.sourceforge.net/project/ptpd/ptpd/2.3.1/ptpd-2.3.1.tar.gz, attempting MIRRORS if available
WARNING: nano-2.2.5-r3.0 do_fetch: Failed to fetch URL ftp://nano-editor.org/pub/nano/v2.2/nano-2.2.5.tar.gz, attempting MIRRORS if available
ERROR: ntp-4.2.8p7-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: ntp-4.2.8p7-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://www.eecis.udel.edu/~ntp/ntp_spool/ntp4/ntp-4.2/ntp-4.2.8p7.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/ntp/4.2.8p7-r0/temp/log.do_fetch.6920
ERROR: Task 2579 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-support/ntp/ntp_4.2.8p7.bb, do_fetch) failed with exit code '1'
ERROR: linuxptp-1.6-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: linuxptp-1.6-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://sourceforge.net/projects/linuxptp/files/v1.6/linuxptp-1.6.tgz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/linuxptp/1.6-r0/temp/log.do_fetch.6922
ERROR: Task 2527 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-connectivity/linuxptp/linuxptp_1.6.bb, do_fetch) failed with exit code '1'
ERROR: cpuburn-neon-20140626-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: cpuburn-neon-20140626-r0 do_fetch: Function failed: Fetcher failure for URL: 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-a8.S;name=ssvb'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.6919
ERROR: Task 2748 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch) failed with exit code '1'
ERROR: vlan-1.9-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: vlan-1.9-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://vlan.sourcearchive.com/downloads/1.9-3ubuntu9/vlan_1.9.orig.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/vlan/1.9-r0/temp/log.do_fetch.6924
ERROR: Task 2474 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-connectivity/vlan/vlan_1.9.bb, do_fetch) failed with exit code '1'
ERROR: ptpd-2.3.1-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: ptpd-2.3.1-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://downloads.sourceforge.net/project/ptpd/ptpd/2.3.1/ptpd-2.3.1.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/ptpd/2.3.1-r0/temp/log.do_fetch.6923
ERROR: Task 2514 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-daemons/ptpd/ptpd_2.3.1.bb, do_fetch) failed with exit code '1'
ERROR: nano-2.2.5-r3.0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: nano-2.2.5-r3.0 do_fetch: Function failed: Fetcher failure for URL: 'ftp://nano-editor.org/pub/nano/v2.2/nano-2.2.5.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/nano/2.2.5-r3.0/temp/log.do_fetch.6921
ERROR: Task 2566 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-support/nano/nano_2.2.5.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3876 tasks of which 3870 didn't need to be rerun and 6 failed.
Waiting for 0 running tasks to finish:
请问怎么解决,谢谢!
0 Kudos
Reply
1 Reply

1,051 Views
joanxie
NXP TechSupport
NXP TechSupport

this is network issue, pls check if your ubuntu network, then use the command like :

"bitbake -c ntp cleanll

bitbake -c ntp"

if it works now, try other packages which have error message like this again

0 Kudos
Reply