bitbake fsl-image-qt5 error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake fsl-image-qt5 error

1,951 次查看
ahljzdh
Contributor I

imx6ull   yocto项目

出错信息如下:

WARNING: linuxptp-1.6-r0 do_fetch: Failed to fetch URL http://sourceforge.net/projects/linuxptp/files/v1.6/linuxptp-1.6.tgz, attempting MIRRORS if available
WARNING: cpuburn-neon-20140626-r0 do_fetch: Failed to fetch URL https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..., attempting MIRRORS if available
WARNING: ntp-4.2.8p7-r0 do_fetch: Failed to fetch URL http://www.eecis.udel.edu/~ntp/ntp_spool/ntp4/ntp-4.2/ntp-4.2.8p7.tar.gz, attempting MIRRORS if available
WARNING: vlan-1.9-r0 do_fetch: Failed to fetch URL http://vlan.sourcearchive.com/downloads/1.9-3ubuntu9/vlan_1.9.orig.tar.gz, attempting MIRRORS if available
WARNING: ptpd-2.3.1-r0 do_fetch: Failed to fetch URL http://downloads.sourceforge.net/project/ptpd/ptpd/2.3.1/ptpd-2.3.1.tar.gz, attempting MIRRORS if available
WARNING: nano-2.2.5-r3.0 do_fetch: Failed to fetch URL ftp://nano-editor.org/pub/nano/v2.2/nano-2.2.5.tar.gz, attempting MIRRORS if available
ERROR: ntp-4.2.8p7-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: ntp-4.2.8p7-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://www.eecis.udel.edu/~ntp/ntp_spool/ntp4/ntp-4.2/ntp-4.2.8p7.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/ntp/4.2.8p7-r0/temp/log.do_fetch.6920
ERROR: Task 2579 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-support/ntp/ntp_4.2.8p7.bb, do_fetch) failed with exit code '1'
ERROR: linuxptp-1.6-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: linuxptp-1.6-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://sourceforge.net/projects/linuxptp/files/v1.6/linuxptp-1.6.tgz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/linuxptp/1.6-r0/temp/log.do_fetch.6922
ERROR: Task 2527 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-connectivity/linuxptp/linuxptp_1.6.bb, do_fetch) failed with exit code '1'
ERROR: cpuburn-neon-20140626-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 4, output:
Proxy tunneling failed: Bad RequestUnable to establish SSL connection.
ERROR: cpuburn-neon-20140626-r0 do_fetch: Function failed: Fetcher failure for URL: 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-a8.S;name=ssvb'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.6919
ERROR: Task 2748 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch) failed with exit code '1'
ERROR: vlan-1.9-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: vlan-1.9-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://vlan.sourcearchive.com/downloads/1.9-3ubuntu9/vlan_1.9.orig.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/vlan/1.9-r0/temp/log.do_fetch.6924
ERROR: Task 2474 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-connectivity/vlan/vlan_1.9.bb, do_fetch) failed with exit code '1'
ERROR: ptpd-2.3.1-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: ptpd-2.3.1-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://downloads.sourceforge.net/project/ptpd/ptpd/2.3.1/ptpd-2.3.1.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/ptpd/2.3.1-r0/temp/log.do_fetch.6923
ERROR: Task 2514 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-networking/recipes-daemons/ptpd/ptpd_2.3.1.bb, do_fetch) failed with exit code '1'
ERROR: nano-2.2.5-r3.0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
20 redirections exceeded.
ERROR: nano-2.2.5-r3.0 do_fetch: Function failed: Fetcher failure for URL: 'ftp://nano-editor.org/pub/nano/v2.2/nano-2.2.5.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/ssx/fsl-relase-bsp/build/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/nano/2.2.5-r3.0/temp/log.do_fetch.6921
ERROR: Task 2566 (/home/ssx/fsl-relase-bsp/sources/meta-openembedded/meta-oe/recipes-support/nano/nano_2.2.5.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3876 tasks of which 3870 didn't need to be rerun and 6 failed.
Waiting for 0 running tasks to finish:
Ubuntu虚拟机下构建,下载不成功,请问如何解决,是否有其他的镜像地址可以下载。
0 项奖励
回复
2 回复数

1,884 次查看
Sun1z
Contributor III

Don't imagine to develop yocto / android ... without VPN

1,884 次查看
joanxie
NXP TechSupport
NXP TechSupport

what bsp version and ubuntu version do you use? pls double check your network, can your ubuntu connect website? it seems that your network issue.

0 项奖励
回复