bitbake compilation error with imx-gst1.0-plugin_4.4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake compilation error with imx-gst1.0-plugin_4.4.2

1,254件の閲覧回数
vincentbodin
Contributor II

Dear all,

I have a compilation error when I bitbake the package imx-gst1.0-plugin:

../../git/libs/device-2d/imx_2d_device_g2d.c: In function 'imx_g2d_config_input':
| ../../git/libs/device-2d/imx_2d_device_g2d.c:302:23: error: 'G2D_AMPHION_TILED' undeclared (first use in this function); did you mean 'G2D_SUPERTILED'?
| g2d->src.tiling = G2D_AMPHION_TILED;
| ^~~~~~~~~~~~~~~~~
| G2D_SUPERTILED
| ../../git/libs/device-2d/imx_2d_device_g2d.c:302:23: note: each undeclared identifier is reported only once for each function it appears in
| ../../git/libs/device-2d/imx_2d_device_g2d.c: In function 'imx_g2d_blit':
| ../../git/libs/device-2d/imx_2d_device_g2d.c:421:23: warning: assignment makes pointer from integer without a cast [-Wint-conversion]
| src->mem->paddr = paddr;
| ^
| ../../git/libs/device-2d/imx_2d_device_g2d.c:430:23: warning: assignment makes pointer from integer without a cast [-Wint-conversion]
| dst->mem->paddr = paddr;
| ^
| ../../git/libs/device-2d/imx_2d_device_g2d.c:466:26: error: 'G2D_AMPHION_TILED' undeclared (first use in this function); did you mean 'G2D_SUPERTILED'?
| if (g2d->src.tiling == G2D_AMPHION_TILED && src->fd[1] >= 0)
| ^~~~~~~~~~~~~~~~~
| G2D_SUPERTILED
| ../../git/libs/device-2d/imx_2d_device_g2d.c:471:26: error: 'G2D_AMPHION_INTERLACED' undeclared (first use in this function); did you mean 'G2D_AMPHION_TILED'?
| g2d->src.tiling |= G2D_AMPHION_INTERLACED;
| ^~~~~~~~~~~~~~~~~~~~~~
| G2D_AMPHION_TILED

This is my local.conf:

IMAGE_INSTALL_append = " libstdc++ chkconfig glib-networking glibmm \
pkgconfig \
zlib glib-2.0 evtest \
cpufrequtils \
openssh-sftp-server \
imx-vpu \
firmware-imx \
qtbase \
qtmultimedia \
qtmultimedia-plugins \
dbus \
i2c-tools \
gstreamer1.0-plugins-imx \
imx-gst1.0-plugin \
gstreamer1.0-plugins-base \
gstreamer1.0-plugins-good \
gstreamer1.0-plugins-bad \
gstreamer1.0 \
psplash \
u-boot-toradex-fsl-fw-utils \
ntfs-3g-ntfsprogs \
"

Could you please advice ?

Many thanks, Vincent

0 件の賞賛
返信
1 返信

1,085件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

Are you using Ubuntu to build the BSP? which version of Ubuntu are you using?

could you show me the steps? so I can try it on my side.

0 件の賞賛
返信