bitbake过程中,电脑异常关机

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake过程中,电脑异常关机

1,355 Views
2046880190
Contributor III

大家好:

   今天遇上一件尴尬的事情,bitbake过程中,电脑蓝屏。

   再次开机执行Bitbake就一直报错。

   之前报错我都可以通过重新执行下列代码恢复

DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh -b jun_build/

bitbake fsl-image-qt5-validation-imx

但是这次用这个方式好像恢复不了了,请教怎么处理这个问题,下面是报错信息:

jun@ubuntu:~/i.mx8/imx-yocto-bsp/jun_build$ bitbake fsl-image-qt5-validation-imxNOTE: Your conf/bblayers.conf has been automatically updated.
Loading cache: 100% |############################################| Time: 0:00:06
Loaded 3287 entries from dependency cache.
Parsing recipes: 100% |##########################################| Time: 0:00:04
Parsing of 2440 .bb files complete (2438 cached, 2 parsed). 3289 targets, 406 skipped, 9 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mqevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "4.9.88-2.1.0_8mm_alpha"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "my_imx_bsp:fdeecc901196bbccd7c5b1ea4268a2cf56764a62"
meta-oe
meta-multimedia = "my_imx_bsp:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-freescale = "my_imx_bsp:49ac225a38f6d84519798e3264f2e4d19b84f70a"
meta-freescale-3rdparty = "my_imx_bsp:62de01743c9233ea718de22991c47b73a78b4857"
meta-freescale-distro = "my_imx_bsp:0ec6d7e206705702b5b534611754de0787f92b72"
meta-bsp
meta-sdk = "my_imx_bsp:8898f51c96e0e79dd56690d797d309f013ec9f76"
meta-browser = "my_imx_bsp:d6f9aed41c73b75a97d71bff060b03a66ee087b1"
meta-gnome
meta-networking
meta-python
meta-filesystems = "my_imx_bsp:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-qt5 = "my_imx_bsp:cfe02f26de53e5c20e6f9555059cbaaf5ab9b22f"

Initialising tasks: 100% |#######################################| Time: 0:00:33
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: qtdeclarative-5.9.5+gitAUTOINC+f23d1d54a0-r0 do_compile_ptest_base: oe_runmake failed
ERROR: qtdeclarative-5.9.5+gitAUTOINC+f23d1d54a0-r0 do_compile_ptest_base: Function failed: do_compile_ptest_base (log file is located at /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/temp/log.do_compile_ptest_base.10069)
ERROR: Logfile of failure stored in: /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/temp/log.do_compile_ptest_base.10069
Log data follows:
| DEBUG: Executing shell function do_compile_ptest_base
| NOTE: make MAKEFLAGS=-j 1 OE_QMAKE_COMPILER=aarch64-poky-linux-gcc --sysroot=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot OE_QMAKE_CC=aarch64-poky-linux-gcc --sysroot=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot OE_QMAKE_CXX=aarch64-poky-linux-g++ --sysroot=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot OE_QMAKE_CFLAGS= -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0=/usr/src/debug/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0 -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot= OE_QMAKE_CXXFLAGS= -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0=/usr/src/debug/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0 -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native= -fdebug-prefix-map=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot= -fvisibility-inlines-hidden OE_QMAKE_LINK=aarch64-poky-linux-g++ --sysroot=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot OE_QMAKE_LDFLAGS=-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed OE_QMAKE_AR=aarch64-poky-linux-ar OE_QMAKE_STRIP=echo OE_QMAKE_WAYLAND_SCANNER=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/wayland-scanner OE_QMAKE_INCDIR_QT=/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot//usr/include/qt5
| cd auto/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/auto.pro ) && make -f Makefile
| make[1]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto'
| cd qml/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qml.pro ) && make -f Makefile
| make[2]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml'
| cd parserstress/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/parserstress/parserstress.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/parserstress'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/parserstress'
| cd qjsvalueiterator/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsvalueiterator/qjsvalueiterator.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsvalueiterator'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsvalueiterator'
| cd qjsonbinding/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsonbinding/qjsonbinding.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsonbinding'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qjsonbinding'
| cd qqmlfile/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfile/qqmlfile.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfile'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfile'
| cd qqmlfileselector/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfileselector/qqmlfileselector.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfileselector'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlfileselector'
| cd qmlmin/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qmlmin/qmlmin.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qmlmin'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qmlmin'
| cd qqmlcomponent/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlcomponent/qqmlcomponent.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlcomponent'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlcomponent'
| cd qqmlconsole/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlconsole/qqmlconsole.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlconsole'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlconsole'
| cd qqmlengine/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlengine/qqmlengine.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlengine'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlengine'
| cd qqmlerror/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlerror/qqmlerror.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlerror'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlerror'
| cd qqmlincubator/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlincubator/qqmlincubator.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlincubator'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlincubator'
| cd qqmlinfo/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlinfo/qqmlinfo.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlinfo'
| make[3]: Nothing to be done for 'first'.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmlinfo'
| cd qqmllistreference/ && ( test -e Makefile || /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/recipe-sysroot-native/usr/bin/qt5/qmake -o Makefile /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmllistreference/qqmllistreference.pro ) && make -f Makefile
| make[3]: Entering directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmllistreference'
| make[3]: *** No targets. Stop.
| make[3]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml/qqmllistreference'
| ERROR: oe_runmake failed
| Makefile:374: recipe for target 'sub-qqmllistreference-make_first' failed
| make[2]: *** [sub-qqmllistreference-make_first] Error 2
| make[2]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto/qml'
| Makefile:53: recipe for target 'sub-qml-make_first' failed
| make[1]: *** [sub-qml-make_first] Error 2
| make[1]: Leaving directory '/home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/git/tests/auto'
| Makefile:45: recipe for target 'sub-auto-make_first' failed
| make: *** [sub-auto-make_first] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile_ptest_base (log file is located at /home/jun/i.mx8/imx-yocto-bsp/jun_build/tmp/work/aarch64-poky-linux/qtdeclarative/5.9.5+gitAUTOINC+f23d1d54a0-r0/temp/log.do_compile_ptest_base.10069)
ERROR: Task (/home/jun/i.mx8/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_compile_ptest_base) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1923 tasks of which 1922 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/jun/i.mx8/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_compile_ptest_base
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Labels (1)
0 Kudos
Reply
2 Replies

1,148 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jun,

    I just compiled Linux BSP v4.9.88 for i.MX8MQ, no problem.

    For issues on PC blue screen, we don't have share experience with you.

    For errors during compiling linux BSP,  you can firstly run bitbak clean command to remove some temperary files, then re-compile it again.

Have a nice day!

BR,

Weidong

0 Kudos
Reply

1,148 Views
2046880190
Contributor III

您好:

   我按照您提供的办法,clean了一次,仍旧是报错 的,现在打算把这个目录复制一份,然后重新来一次。

   电脑蓝屏不是编译的问题,是我在操作一些USB外设,把电脑搞出问题了

   谢谢!

0 Kudos
Reply