ata1: softreset failed (device not ready)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ata1: softreset failed (device not ready)

2,411件の閲覧回数
Danial
Contributor II

debug imformation:

ahci: SSS flag set, parallel bus scan disabled
ahci ahci.0: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc
scsi0 : ahci
ata1: SATA max UDMA/133 irq_stat 0x00000040, connection status changed irq 28

ata1: link is slow to respond, please be patient (ready=0)

ata1: softreset failed (device not ready)
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: limiting SATA link speed to 1.5 Gbps
ata1: softreset failed (device not ready)
ata1: reset failed, giving up

I attach a sata disk to the QSB board, and enable the sata driver. The sata disk use the 

computer's sata power. 

Who can help me?

Regards.

ラベル(1)
0 件の賞賛
返信
1 返信

1,722件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

please configure like the following :

CONFIG_SATA_PMP=n

CONFIG_ATA=y
CONFIG_ATA_VERBOSE_ERROR=y
CONFIG_SATA_AHCI_PLATFORM=y
CONFIG_ATA_SFF=y

0 件の賞賛
返信