asoc-simple-card driver not loading on imx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

asoc-simple-card driver not loading on imx8mq

500 次查看
synaption
Contributor I

Alsa does not recognize my i2s pins or dummy card. I am on imx-linux 6.1

+ sudo cat /sys/kernel/debug/devices_deferred
sound-header asoc-simple-card: parse error
+ sudo ls /sys/kernel/debug/asoc/
components dais
++ uname -r
+ sudo ls ls /lib/modules/6.1.36/kernel/sound/
ls: cannot access 'ls': No such file or directory
/lib/modules/6.1.36/kernel/sound/:
core drivers soc usb
+ ls /proc/device-tree/
'#address-cells' clock-osc-25m name
'#size-cells' clock-osc-27m opp-table
aliases clock-pmic pmu
busfreq compatible pps
chosen cpus psci
clock-ckil dummy-dai regulator-usdhc2-vmmc
clock-ext1 gpio-fan soc@0
clock-ext2 gpu3d@38000000 sound-header
clock-ext3 interrupt-parent thermal-zones
clock-ext4 memory@40000000 timer
clock-hdmi-phy-27m model
+ ls /sys/bus/platform/devices/
100000.caam-sm 33000000.dma-apbh
30000000.bus 38100000.usb
30000000.bus:caam_secvio 381f0040.usb-phy
30010000.sai 38200000.usb
30200000.gpio 382f0040.usb-phy
30210000.gpio 3d800000.ddr-pmu
30220000.gpio 'Fixed MDIO bus.0'
30230000.gpio alarmtimer.0.auto
30240000.gpio bd71837-clk.2.auto
30260000.tmu bd71837-pmic.3.auto
30280000.watchdog busfreq
302c0000.dma-controller caam-dma
30330000.pinctrl caam_sm
30340000.syscon cpufreq-dt
30340000.syscon:mux-controller dummy-dai
30350000.efuse gpio-fan
30350000.efuse:imx8mq-soc gpio-keys.1.auto
30360000.syscon imx-cpufreq-dt
30370000.caam-snvs imx-pgc-domain.0
30370000.snvs imx-pgc-domain.1
30370000.snvs:snvs-rtc-lp imx-pgc-domain.10
30380000.clock-controller imx-pgc-domain.2
30390000.reset-controller imx-pgc-domain.3
303a0000.gpc imx-pgc-domain.4
30400000.bus imx-pgc-domain.5
30660000.pwm imx-pgc-domain.6
30670000.pwm imx-pgc-domain.7
30680000.pwm imx-pgc-domain.8
30690000.pwm imx-pgc-domain.9
306a0000.timer platform-framebuffer.0
30800000.bus pmu
30820000.spi pps
30860000.serial psci
30880000.serial psci-cpuidle
30900000.crypto reg-dummy
30902000.jr regulator-usdhc2-vmmc
30903000.jr regulatory.0
30a20000.i2c serial8250
30aa0000.mailbox snd-soc-dummy
30b40000.mmc soc@0
30b50000.mmc sound-header
30bd0000.dma-controller timer
30be0000.ethernet xhci-hcd.4.auto
32c00000.bus xhci-hcd.5.auto
32e2d000.interrupt-controller
+ ls /dev/snd/
timer
+ ls /proc/asound/
cards devices pcm timers version
+ ls /sys/class/sound/
timer
+ dmesg
+ grep -iE 'alsa|audio|sai|snd|sound|deferred'
[ 0.063840] Advanced Linux Sound Architecture Driver Initialized.
[ 2.197728] ALSA device list:
[ 2.200699] No soundcards found.
[ 16.094656] platform sound-header: deferred probe pending
+ zcat /proc/config.gz


These are the relevant portions of my linux config.

+ grep -iE 'snd|sound'
CONFIG_REGMAP_SOUNDWIRE=m
CONFIG_SOUND=y
CONFIG_SND=y
CONFIG_SND_TIMER=y
CONFIG_SND_PCM=y
CONFIG_SND_PCM_ELD=y
CONFIG_SND_PCM_IEC958=y
CONFIG_SND_DMAENGINE_PCM=y
CONFIG_SND_HWDEP=m
CONFIG_SND_RAWMIDI=y
CONFIG_SND_COMPRESS_OFFLOAD=y
CONFIG_SND_JACK=y
CONFIG_SND_JACK_INPUT_DEV=y
# CONFIG_SND_OSSEMUL is not set
CONFIG_SND_PCM_TIMER=y
# CONFIG_SND_HRTIMER is not set
CONFIG_SND_DYNAMIC_MINORS=y
CONFIG_SND_MAX_CARDS=32
CONFIG_SND_SUPPORT_OLD_API=y
CONFIG_SND_PROC_FS=y
CONFIG_SND_VERBOSE_PROCFS=y
# CONFIG_SND_VERBOSE_PRINTK is not set
CONFIG_SND_CTL_FAST_LOOKUP=y
CONFIG_SND_DEBUG=y
CONFIG_SND_DEBUG_VERBOSE=y
# CONFIG_SND_PCM_XRUN_DEBUG is not set
# CONFIG_SND_CTL_INPUT_VALIDATION is not set
# CONFIG_SND_CTL_DEBUG is not set
# CONFIG_SND_JACK_INJECTION_DEBUG is not set
# CONFIG_SND_SEQUENCER is not set
CONFIG_SND_DRIVERS=y
# CONFIG_SND_DUMMY is not set
CONFIG_SND_ALOOP=m
# CONFIG_SND_MTPAV is not set
# CONFIG_SND_SERIAL_U16550 is not set
# CONFIG_SND_SERIAL_GENERIC is not set
# CONFIG_SND_MPU401 is not set
CONFIG_SND_PCI=y
# CONFIG_SND_AD1889 is not set
# CONFIG_SND_ALS300 is not set
# CONFIG_SND_ALI5451 is not set
# CONFIG_SND_ATIIXP is not set
# CONFIG_SND_ATIIXP_MODEM is not set
# CONFIG_SND_AU8810 is not set
# CONFIG_SND_AU8820 is not set
# CONFIG_SND_AU8830 is not set
# CONFIG_SND_AW2 is not set
# CONFIG_SND_AZT3328 is not set
# CONFIG_SND_BT87X is not set
# CONFIG_SND_CA0106 is not set
# CONFIG_SND_CMIPCI is not set
# CONFIG_SND_OXYGEN is not set
# CONFIG_SND_CS4281 is not set
# CONFIG_SND_CS46XX is not set
# CONFIG_SND_CTXFI is not set
# CONFIG_SND_DARLA20 is not set
# CONFIG_SND_GINA20 is not set
# CONFIG_SND_LAYLA20 is not set
# CONFIG_SND_DARLA24 is not set
# CONFIG_SND_GINA24 is not set
# CONFIG_SND_LAYLA24 is not set
# CONFIG_SND_MONA is not set
# CONFIG_SND_MIA is not set
# CONFIG_SND_ECHO3G is not set
# CONFIG_SND_INDIGO is not set
# CONFIG_SND_INDIGOIO is not set
# CONFIG_SND_INDIGODJ is not set
# CONFIG_SND_INDIGOIOX is not set
# CONFIG_SND_INDIGODJX is not set
# CONFIG_SND_EMU10K1 is not set
# CONFIG_SND_EMU10K1X is not set
# CONFIG_SND_ENS1370 is not set
# CONFIG_SND_ENS1371 is not set
# CONFIG_SND_ES1938 is not set
# CONFIG_SND_ES1968 is not set
# CONFIG_SND_FM801 is not set
# CONFIG_SND_HDSP is not set
# CONFIG_SND_HDSPM is not set
# CONFIG_SND_ICE1712 is not set
# CONFIG_SND_ICE1724 is not set
# CONFIG_SND_INTEL8X0 is not set
# CONFIG_SND_INTEL8X0M is not set
# CONFIG_SND_KORG1212 is not set
# CONFIG_SND_LOLA is not set
# CONFIG_SND_LX6464ES is not set
# CONFIG_SND_MAESTRO3 is not set
# CONFIG_SND_MIXART is not set
# CONFIG_SND_NM256 is not set
# CONFIG_SND_PCXHR is not set
# CONFIG_SND_RIPTIDE is not set
# CONFIG_SND_RME32 is not set
# CONFIG_SND_RME96 is not set
# CONFIG_SND_RME9652 is not set
# CONFIG_SND_SE6X is not set
# CONFIG_SND_SONICVIBES is not set
# CONFIG_SND_TRIDENT is not set
# CONFIG_SND_VIA82XX is not set
# CONFIG_SND_VIA82XX_MODEM is not set
# CONFIG_SND_VIRTUOSO is not set
# CONFIG_SND_VX222 is not set
# CONFIG_SND_YMFPCI is not set
# CONFIG_SND_HDA_INTEL is not set
CONFIG_SND_HDA_PREALLOC_SIZE=64
CONFIG_SND_SPI=y
CONFIG_SND_USB=y
CONFIG_SND_USB_AUDIO=m
CONFIG_SND_USB_AUDIO_USE_MEDIA_CONTROLLER=y
# CONFIG_SND_USB_UA101 is not set
# CONFIG_SND_USB_CAIAQ is not set
# CONFIG_SND_USB_6FIRE is not set
# CONFIG_SND_USB_HIFACE is not set
# CONFIG_SND_BCD2000 is not set
# CONFIG_SND_USB_POD is not set
# CONFIG_SND_USB_PODHD is not set
# CONFIG_SND_USB_TONEPORT is not set
# CONFIG_SND_USB_VARIAX is not set
CONFIG_SND_SOC=y
CONFIG_SND_SOC_GENERIC_DMAENGINE_PCM=y
CONFIG_SND_SOC_COMPRESS=y
CONFIG_SND_SOC_TOPOLOGY=y
# CONFIG_SND_SOC_ADI is not set
# CONFIG_SND_SOC_AMD_ACP is not set
# CONFIG_SND_AMD_ACP_CONFIG is not set
# CONFIG_SND_ATMEL_SOC is not set
# CONFIG_SND_BCM63XX_I2S_WHISTLER is not set
# CONFIG_SND_DESIGNWARE_I2S is not set
CONFIG_SND_SOC_FSL_Asrc=m
CONFIG_SND_SOC_FSL_SAI=y
CONFIG_SND_SOC_FSL_MQS=m
CONFIG_SND_SOC_FSL_AUDMIX=m
CONFIG_SND_SOC_FSL_SSI=m
CONFIG_SND_SOC_FSL_SPDIF=m
CONFIG_SND_SOC_FSL_ESAI=m
CONFIG_SND_SOC_FSL_MICFIL=m
CONFIG_SND_SOC_FSL_EAsrc=m
CONFIG_SND_SOC_FSL_XCVR=m
CONFIG_SND_SOC_FSL_AUD2HTX=m
CONFIG_SND_SOC_FSL_ESAI_CLIENT=y
CONFIG_SND_SOC_FSL_UTILS=y
CONFIG_SND_SOC_FSL_RPMSG=m
CONFIG_SND_SOC_IMX_PCM_DMA=y
CONFIG_SND_SOC_IMX_AUDIO_RPMSG=m
CONFIG_SND_SOC_IMX_PCM_RPMSG=m
CONFIG_SND_SOC_IMX_AUDMUX=m
CONFIG_SND_IMX_SOC=m
# CONFIG_SND_SOC_IMX_ES8328 is not set
CONFIG_SND_SOC_IMX_SGTL5000=m
CONFIG_SND_SOC_IMX_SPDIF=m
CONFIG_SND_SOC_FSL_ASOC_CARD=m
CONFIG_SND_SOC_IMX_AUDMIX=m
CONFIG_SND_SOC_IMX_HDMI=m
CONFIG_SND_SOC_IMX_RPMSG=m
CONFIG_SND_SOC_IMX_CARD=m
CONFIG_SND_SOC_IMX_PCM512X=m
# CONFIG_SND_I2S_HI6210_I2S is not set
# CONFIG_SND_SOC_IMG is not set
# CONFIG_SND_SOC_INTEL_KEEMBAY is not set
# CONFIG_SND_SOC_MTK_BTCVSD is not set
CONFIG_SND_SOC_SOF_TOPLEVEL=y
# CONFIG_SND_SOC_SOF_PCI is not set
# CONFIG_SND_SOC_SOF_ACPI is not set
CONFIG_SND_SOC_SOF_OF=m
CONFIG_SND_SOC_SOF_OF_DEV=m
CONFIG_SND_SOC_SOF_COMPRESS=y
CONFIG_SND_SOC_SOF=m
CONFIG_SND_SOC_SOF_IPC3=y
CONFIG_SND_SOC_SOF_IMX_TOPLEVEL=y
CONFIG_SND_SOC_SOF_IMX_COMMON=m
CONFIG_SND_SOC_SOF_IMX8=m
CONFIG_SND_SOC_SOF_IMX8M=m
CONFIG_SND_SOC_SOF_IMX8ULP=m
# CONFIG_SND_SOC_SOF_MTK_TOPLEVEL is not set
CONFIG_SND_SOC_SOF_XTENSA=m
# CONFIG_SND_SOC_XILINX_I2S is not set
# CONFIG_SND_SOC_XILINX_AUDIO_FORMATTER is not set
# CONFIG_SND_SOC_XILINX_SPDIF is not set
# CONFIG_SND_SOC_XTFPGA_I2S is not set
CONFIG_SND_SOC_I2C_AND_SPI=y
CONFIG_SND_SOC_WM_HUBS=m
# CONFIG_SND_SOC_AC97_CODEC is not set
# CONFIG_SND_SOC_ADAU1372_I2C is not set
# CONFIG_SND_SOC_ADAU1372_SPI is not set
# CONFIG_SND_SOC_ADAU1701 is not set
# CONFIG_SND_SOC_ADAU1761_I2C is not set
# CONFIG_SND_SOC_ADAU1761_SPI is not set
# CONFIG_SND_SOC_ADAU7002 is not set
# CONFIG_SND_SOC_ADAU7118_HW is not set
# CONFIG_SND_SOC_ADAU7118_I2C is not set
# CONFIG_SND_SOC_AK4104 is not set
# CONFIG_SND_SOC_AK4118 is not set
# CONFIG_SND_SOC_AK4375 is not set
CONFIG_SND_SOC_AK4458=m
# CONFIG_SND_SOC_AK4554 is not set
CONFIG_SND_SOC_AK4613=m
# CONFIG_SND_SOC_AK4642 is not set
# CONFIG_SND_SOC_AK5386 is not set
CONFIG_SND_SOC_AK5558=m
# CONFIG_SND_SOC_ALC5623 is not set
# CONFIG_SND_SOC_AW8738 is not set
# CONFIG_SND_SOC_BD28623 is not set
CONFIG_SND_SOC_BT_SCO=y
CONFIG_SND_SOC_CROS_EC_CODEC=m
# CONFIG_SND_SOC_CS35L32 is not set
# CONFIG_SND_SOC_CS35L33 is not set
# CONFIG_SND_SOC_CS35L34 is not set
# CONFIG_SND_SOC_CS35L35 is not set
# CONFIG_SND_SOC_CS35L36 is not set
# CONFIG_SND_SOC_CS35L41_SPI is not set
# CONFIG_SND_SOC_CS35L41_I2C is not set
# CONFIG_SND_SOC_CS35L45_SPI is not set
# CONFIG_SND_SOC_CS35L45_I2C is not set
# CONFIG_SND_SOC_CS42L42 is not set
# CONFIG_SND_SOC_CS42L51_I2C is not set
# CONFIG_SND_SOC_CS42L52 is not set
# CONFIG_SND_SOC_CS42L56 is not set
# CONFIG_SND_SOC_CS42L73 is not set
# CONFIG_SND_SOC_CS42L83 is not set
# CONFIG_SND_SOC_CS4234 is not set
# CONFIG_SND_SOC_CS4265 is not set
# CONFIG_SND_SOC_CS4270 is not set
# CONFIG_SND_SOC_CS4271_I2C is not set
# CONFIG_SND_SOC_CS4271_SPI is not set
CONFIG_SND_SOC_CS42XX8=y
CONFIG_SND_SOC_CS42XX8_I2C=y
# CONFIG_SND_SOC_CS43130 is not set
# CONFIG_SND_SOC_CS4341 is not set
# CONFIG_SND_SOC_CS4349 is not set
# CONFIG_SND_SOC_CS53L30 is not set
# CONFIG_SND_SOC_CX2072X is not set
# CONFIG_SND_SOC_DA7213 is not set
CONFIG_SND_SOC_DMIC=m
CONFIG_SND_SOC_HDMI_CODEC=y
CONFIG_SND_SOC_ES7134=m
CONFIG_SND_SOC_ES7241=m
# CONFIG_SND_SOC_ES8316 is not set
# CONFIG_SND_SOC_ES8326 is not set
# CONFIG_SND_SOC_ES8328_I2C is not set
# CONFIG_SND_SOC_ES8328_SPI is not set
CONFIG_SND_SOC_GTM601=m
# CONFIG_SND_SOC_HDA is not set
# CONFIG_SND_SOC_ICS43432 is not set
# CONFIG_SND_SOC_INNO_RK3036 is not set
# CONFIG_SND_SOC_MAX98088 is not set
CONFIG_SND_SOC_MAX98357A=m
# CONFIG_SND_SOC_MAX98504 is not set
# CONFIG_SND_SOC_MAX9867 is not set
CONFIG_SND_SOC_MAX98927=m
# CONFIG_SND_SOC_MAX98520 is not set
# CONFIG_SND_SOC_MAX98373_I2C is not set
# CONFIG_SND_SOC_MAX98373_SDW is not set
# CONFIG_SND_SOC_MAX98390 is not set
# CONFIG_SND_SOC_MAX98396 is not set
# CONFIG_SND_SOC_MAX9860 is not set
CONFIG_SND_SOC_MSM8916_WCD_ANALOG=m
CONFIG_SND_SOC_MSM8916_WCD_DIGITAL=m
# CONFIG_SND_SOC_PCM1681 is not set
# CONFIG_SND_SOC_PCM1789_I2C is not set
# CONFIG_SND_SOC_PCM179X_I2C is not set
# CONFIG_SND_SOC_PCM179X_SPI is not set
CONFIG_SND_SOC_PCM186X=m
CONFIG_SND_SOC_PCM186X_I2C=m
# CONFIG_SND_SOC_PCM186X_SPI is not set
# CONFIG_SND_SOC_PCM3060_I2C is not set
# CONFIG_SND_SOC_PCM3060_SPI is not set
CONFIG_SND_SOC_PCM3168A=m
CONFIG_SND_SOC_PCM3168A_I2C=m
# CONFIG_SND_SOC_PCM3168A_SPI is not set
# CONFIG_SND_SOC_PCM5102A is not set
CONFIG_SND_SOC_PCM512x=m
CONFIG_SND_SOC_PCM512x_I2C=m
# CONFIG_SND_SOC_PCM512x_SPI is not set
# CONFIG_SND_SOC_RK3328 is not set
# CONFIG_SND_SOC_RK817 is not set
CONFIG_SND_SOC_RL6231=m
# CONFIG_SND_SOC_RT1308_SDW is not set
# CONFIG_SND_SOC_RT1316_SDW is not set
# CONFIG_SND_SOC_RT1318_SDW is not set
# CONFIG_SND_SOC_RT5616 is not set
# CONFIG_SND_SOC_RT5631 is not set
# CONFIG_SND_SOC_RT5640 is not set
CONFIG_SND_SOC_RT5659=m
# CONFIG_SND_SOC_RT5682_SDW is not set
# CONFIG_SND_SOC_RT700_SDW is not set
# CONFIG_SND_SOC_RT711_SDW is not set
# CONFIG_SND_SOC_RT711_SDCA_SDW is not set
# CONFIG_SND_SOC_RT715_SDW is not set
# CONFIG_SND_SOC_RT715_SDCA_SDW is not set
# CONFIG_SND_SOC_RT9120 is not set
CONFIG_SND_SOC_SGTL5000=m
CONFIG_SND_SOC_SIMPLE_AMPLIFIER=m
CONFIG_SND_SOC_SIMPLE_MUX=m
CONFIG_SND_SOC_SPDIF=m
# CONFIG_SND_SOC_SRC4XXX_I2C is not set
# CONFIG_SND_SOC_SSM2305 is not set
# CONFIG_SND_SOC_SSM2518 is not set
# CONFIG_SND_SOC_SSM2602_SPI is not set
# CONFIG_SND_SOC_SSM2602_I2C is not set
# CONFIG_SND_SOC_SSM4567 is not set
# CONFIG_SND_SOC_STA32X is not set
# CONFIG_SND_SOC_STA350 is not set
# CONFIG_SND_SOC_STI_SAS is not set
# CONFIG_SND_SOC_TAS2552 is not set
# CONFIG_SND_SOC_TAS2562 is not set
# CONFIG_SND_SOC_TAS2764 is not set
# CONFIG_SND_SOC_TAS2770 is not set
# CONFIG_SND_SOC_TAS2780 is not set
# CONFIG_SND_SOC_TAS5086 is not set
CONFIG_SND_SOC_TAS571X=m
# CONFIG_SND_SOC_TAS5720 is not set
# CONFIG_SND_SOC_TAS5805M is not set
# CONFIG_SND_SOC_TAS6424 is not set
# CONFIG_SND_SOC_TDA7419 is not set
# CONFIG_SND_SOC_TFA9879 is not set
# CONFIG_SND_SOC_TFA989X is not set
# CONFIG_SND_SOC_TLV320ADC3XXX is not set
# CONFIG_SND_SOC_TLV320AIC23_I2C is not set
# CONFIG_SND_SOC_TLV320AIC23_SPI is not set
CONFIG_SND_SOC_TLV320AIC31XX=m
# CONFIG_SND_SOC_TLV320AIC32X4_I2C is not set
# CONFIG_SND_SOC_TLV320AIC32X4_SPI is not set
# CONFIG_SND_SOC_TLV320AIC3X_I2C is not set
# CONFIG_SND_SOC_TLV320AIC3X_SPI is not set
# CONFIG_SND_SOC_TLV320ADCX140 is not set
# CONFIG_SND_SOC_TS3A227E is not set
# CONFIG_SND_SOC_TSCS42XX is not set
# CONFIG_SND_SOC_TSCS454 is not set
# CONFIG_SND_SOC_UDA1334 is not set
# CONFIG_SND_SOC_WCD9335 is not set
CONFIG_SND_SOC_WCD_MBHC=m
CONFIG_SND_SOC_WCD934X=m
# CONFIG_SND_SOC_WCD938X_SDW is not set
# CONFIG_SND_SOC_WM8510 is not set
# CONFIG_SND_SOC_WM8523 is not set
CONFIG_SND_SOC_WM8524=y
# CONFIG_SND_SOC_WM8580 is not set
# CONFIG_SND_SOC_WM8711 is not set
# CONFIG_SND_SOC_WM8728 is not set
# CONFIG_SND_SOC_WM8731_I2C is not set
# CONFIG_SND_SOC_WM8731_SPI is not set
# CONFIG_SND_SOC_WM8737 is not set
# CONFIG_SND_SOC_WM8741 is not set
# CONFIG_SND_SOC_WM8750 is not set
# CONFIG_SND_SOC_WM8753 is not set
# CONFIG_SND_SOC_WM8770 is not set
# CONFIG_SND_SOC_WM8776 is not set
# CONFIG_SND_SOC_WM8782 is not set
# CONFIG_SND_SOC_WM8804_I2C is not set
# CONFIG_SND_SOC_WM8804_SPI is not set
# CONFIG_SND_SOC_WM8903 is not set
CONFIG_SND_SOC_WM8904=m
# CONFIG_SND_SOC_WM8940 is not set
CONFIG_SND_SOC_WM8960=m
CONFIG_SND_SOC_WM8962=m
# CONFIG_SND_SOC_WM8974 is not set
# CONFIG_SND_SOC_WM8978 is not set
# CONFIG_SND_SOC_WM8985 is not set
CONFIG_SND_SOC_WM8994=m
CONFIG_SND_SOC_WSA881X=m
# CONFIG_SND_SOC_WSA883X is not set
# CONFIG_SND_SOC_ZL38060 is not set
CONFIG_SND_SOC_RPMSG_WM8960=m
CONFIG_SND_SOC_RPMSG_WM8960_I2C=m
CONFIG_SND_SOC_RPMSG_AK4497=m
# CONFIG_SND_SOC_MAX9759 is not set
# CONFIG_SND_SOC_MT6351 is not set
# CONFIG_SND_SOC_MT6358 is not set
# CONFIG_SND_SOC_MT6660 is not set
# CONFIG_SND_SOC_NAU8315 is not set
# CONFIG_SND_SOC_NAU8540 is not set
# CONFIG_SND_SOC_NAU8810 is not set
# CONFIG_SND_SOC_NAU8821 is not set
# CONFIG_SND_SOC_NAU8822 is not set
# CONFIG_SND_SOC_NAU8824 is not set
CONFIG_SND_SOC_TPA6130A2=m
CONFIG_SND_SOC_LPASS_MACRO_COMMON=m
CONFIG_SND_SOC_LPASS_WSA_MACRO=m
CONFIG_SND_SOC_LPASS_VA_MACRO=m
# CONFIG_SND_SOC_LPASS_RX_MACRO is not set
# CONFIG_SND_SOC_LPASS_TX_MACRO is not set
CONFIG_SND_SIMPLE_CARD_UTILS=y
CONFIG_SND_SIMPLE_CARD=y
CONFIG_SND_AUDIO_GRAPH_CARD=y
# CONFIG_SND_AUDIO_GRAPH_CARD2 is not set
# CONFIG_SND_TEST_COMPONENT is not set
# CONFIG_SND_XEN_FRONTEND is not set
# CONFIG_SND_VIRTIO is not set
CONFIG_SOUNDWIRE=m
# SoundWire Devices
# CONFIG_SOUNDWIRE_INTEL is not set
CONFIG_SOUNDWIRE_QCOM=m


And these are the relevant portions of my device tree

dummy_dai: dummy-dai {
compatible = "linux,snd-soc-dummy";
#sound-dai-cells = <0>;
status = "okay";
};

sound-header {
compatible = "simple-audio-card";
status = "okay";
simple-audio-card,name = "40-pin Header";
simple-audio-card,format = "i2s";
simple-audio-card,cpu {
sound-dai = <&sai1>;
};
simple-audio-card,codec {
#sound-dai-cells = <0>;
sound-dai = <&dummy_dai>;
};
};


soc@0 {
compatible = "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
ranges = <0x0 0x0 0x0 0x3e000000>;
dma-ranges = <0x40000000 0x0 0x40000000 0xc0000000>;
nvmem-cells = <&imx8mq_uid>;
nvmem-cell-names = "soc_unique_id";

caam_sm: caam-sm@100000 {
compatible = "fsl,imx6q-caam-sm";
reg = <0x100000 0x8000>;
};

bus@30000000 { /* AIPS1 */
compatible = "fsl,aips-bus", "simple-bus";
reg = <0x30000000 0x400000>;
#address-cells = <1>;
#size-cells = <1>;
ranges = <0x30000000 0x30000000 0x400000>;

sai1: sai@30010000 {
#sound-dai-cells = <0>;
compatible = "fsl,imx8mq-sai",
"fsl,imx6sx-sai";
reg = <0x30010000 0x10000>;
interrupts = <GIC_SPI 95 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_SAI1_IPG>,
<&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_SAI1_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>, <&clk IMX8MQ_CLK_DUMMY>;
clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3";
dmas = <&sdma2 8 1 0>, <&sdma2 9 1 0>;
dma-names = "rx", "tx";
fsl,dataline = <0 0xff 0xff>;
status = "disabled";
};


&sai1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
status = "okay";
#sound-dai-cells = <0>;
assigned-clocks =
<&clk IMX8MQ_CLK_SAI1>;
assigned-clock-parents = <&clk IMX8MQ_AUDIO_PLL1_OUT>;
assigned-clock-rates = <45158400>;
clocks = <&clk IMX8MQ_CLK_SAI1_IPG>, <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_SAI1_ROOT>, <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_DUMMY>, <&clk IMX8MQ_AUDIO_PLL1_OUT>,
<&clk IMX8MQ_AUDIO_PLL2_OUT>;
clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3", "pll8k", "pll11k";
};

 

0 项奖励
回复
0 回复数