aplay: pcm_write:2057: write error: Input/output error in wm8960 on imx8mp board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

aplay: pcm_write:2057: write error: Input/output error in wm8960 on imx8mp board

682件の閲覧回数
Satyaprakash
Contributor II

Hii,

i'm able to load wm8960 modules and able to detect soundcard also!!

root@phyboard-pollux-imx8mp-2:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: Dummy [Dummy], device 0: Dummy PCM [Dummy PCM]
  Subdevices: 8/8
  Subdevice #0: subdevice #0
  Subdevice #1: subdevice #1
  Subdevice #2: subdevice #2
  Subdevice #3: subdevice #3
  Subdevice #4: subdevice #4
  Subdevice #5: subdevice #5
  Subdevice #6: subdevice #6
  Subdevice #7: subdevice #7
card 1: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 []
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 1: wm8960audio [wm8960-audio], device 1: HiFi-ASRC-FE (*) []
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 2: audiohdmi [audio-hdmi], device 0: imx8 hdmi i2s-hifi-0 []
  Subdevices: 1/1
  Subdevice #0: subdevice #0

but when i'm playing any .wav files i'm getting this error!!

root@phyboard-pollux-imx8mp-2:~# aplay -D hw:1,0 file_example_WAV_5MG.wav 
Playing WAVE 'file_example_WAV_5MG.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
aplay: pcm_write:2057: write error: Input/output error

IMX8MPLUS 

0 件の賞賛
返信
0 返答(返信)