android6.0 insmod xx.ko, exec format error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android6.0 insmod xx.ko, exec format error

6,410件の閲覧回数
jiejia
Contributor III

Hi,

   I have a board reference to imx6q-sabresd using android_M6.0.1_2.0.0_source.tar.gz.

   I am trying to port device drivers on this board. 

   makefile:

obj-m := sema.o
KDIR := /work/myandroid/kernel_imx/
PWD := $(shell pwd)
all:
   make -C $(KDIR) ARCH=arm CROSS_COMPILE=arm-linux-androideabi- M=$(PWD) modules
clean:
   $(MAKE) -C $(KDIR) M=$(PWD) clean

 

when insmod sema.ko:

root@sabresd_6dq:/data/local/tmp # insmod sema.ko
insmod: failed to load sema.ko: Exec format error

ラベル(4)
0 件の賞賛
返信
1 返信

3,482件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jia,

    The question is on how to compile linux kernel module and write Makefile, Actually, it is not within our support range. Only give you some advice, help you correct your Makefile, see below, please!

---------------------------------------------Pay attention to correct path of your compiler----------------------------

obj-m := sema.o

sema-objs := sema.o
KDIR := /work/myandroid/kernel_imx/
PWD := $(shell pwd)

ARCH=arm

CROSS_COMPILE=arm-eabi-

CC=$(CROSS_COMPILE)gcc

LD=$(CROSS_COMPILE)ld
all:
   make -C $(KDIR) ARCH=$(ARCH) CROSS_COMPILE=$(CROSS_COMPILE) M=$(PWD) modules
clean:
   $(MAKE) -C $(KDIR) M=$(PWD) clean

--------------------------------------------------------------------------------------------------------------------------------------------

Try it , please!

Regards,

Weidong

0 件の賞賛
返信