android image creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

android image creation

1,371 Views
ikerMarinelaren
Contributor II

Hello,

I am creating my own Android Gingerbread imagen.

I am having a problem when building because when I arrive to the installation of the Mms package the compilation get stuck. I attach the error log.

Anobody knows how can I solve this error?

At first it is supossed that the compiation can't go on because these package are missing. I have tried introducing them but after some time continuing addind, I left it.

Anybody knows how I could configure the compiations files which file must changed, to select which apps I want to install? anybody knows why are these packages missing? Is a general mistake or it is just mine?

Than you very much.

Iker

Tags (1)
0 Kudos
Reply
0 Replies