android hangs in open_devnull_stdio() ( inside init)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android hangs in open_devnull_stdio() ( inside init)

ソリューションへジャンプ
3,487件の閲覧回数
VAISAKH
Contributor II

Dear all,

I have a imx6q based hardware ) .I am trying to port  android on it. I am using  freescale r13.3  android .

With NFS its works fine..

But booting from SD cards fails.After digging through init code I found it hangs in side

open_devnull_stdio().. function at  dup2(fd,1);

Please see bootargs below,

bootargs=console=ttymxc0 , 115200 init=/init rw video=mxcfb0  fbmem=5M vmalloc=400M root=/dev/mmcblk0p4 androidboot.console=ttymxc0 ..

( Using UART1 for debugging )

please help me

Thanks in advance

ラベル(2)
0 件の賞賛
返信
1 解決策
2,932件の閲覧回数
imxcommunitysco
Senior Contributor II

Hi Vaisakh,

In reviewing your kernel boot arguments, I don't know if you have provided the complete set, but I would suggest removing the 'root=/dev/mmcblk0p4' option.  This is not necessary to explicitly define the root file system since the root file system is a composite of the RAM disk and mounted file systems.

If the above suggestion does not work, it would also be helpful to attach the output of the console when the kernel boots.  This would provide the entire kernel command line and potential insight into what might be happening.

On a side note, we are moving away from supporting R13.3 release for i.MX 6 since the supported release is the R13.4 GA release.

Thanks,

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,932件の閲覧回数
RichardZhao
Contributor I

Could you prove full log and memory size? And you can also try to decrease vmalloc=xxx.

0 件の賞賛
返信
2,932件の閲覧回数
VAISAKH
Contributor II

Hello,

Thanks for the reply.I have tried  with  the vmalloc = 128 and 64 M but hanged at the same place .)

Please see my logs attached with this post

Memory is 2GB ....

With thanks

Vaisakh N

0 件の賞賛
返信
2,933件の閲覧回数
imxcommunitysco
Senior Contributor II

Hi Vaisakh,

In reviewing your kernel boot arguments, I don't know if you have provided the complete set, but I would suggest removing the 'root=/dev/mmcblk0p4' option.  This is not necessary to explicitly define the root file system since the root file system is a composite of the RAM disk and mounted file systems.

If the above suggestion does not work, it would also be helpful to attach the output of the console when the kernel boots.  This would provide the entire kernel command line and potential insight into what might be happening.

On a side note, we are moving away from supporting R13.3 release for i.MX 6 since the supported release is the R13.4 GA release.

Thanks,

0 件の賞賛
返信
2,932件の閲覧回数
VAISAKH
Contributor II

Anybody,Please help?

0 件の賞賛
返信