Hello sir,
I am working in the IMX6 solo lite custom board based on the I.MX 6 SOLOLITE EVK.
we are booting our board from SD1 card (4 bit). we changed the 8 bit SD1 to 4 bit SD1.
we are flashing the prebuild Android U-boot, uImage, Recovery, File system the SD card as per Android USER GUIDE for I.MX 6 SOLOLITE EVK.
But boot is hang on the after "Freeing init memory: 208K".
I attached my debug log and u-boot environment variables. Please find it.
Kindly give me any suggestion to solve this problem.
Original Attachment has been moved to: custom_board_log.txt.zip
Original Attachment has been moved to: Env_Variable.txt.zip
已解决! 转到解答。
Please try this:
For u-boot:
- u-boot-2009.08/include/mx6sl_evk.h
remove the "#define CONFIG_MMC_8BIT_PORTS 0x1"
- u-boot-2009.08/board/freescale/mx6sl_evk.c
remove the
"MX6SL_PAD_SD1_DAT4__USDHC1_DAT4,
MX6SL_PAD_SD1_DAT5__USDHC1_DAT5,
MX6SL_PAD_SD1_DAT6__USDHC1_DAT6,
MX6SL_PAD_SD1_DAT7__USDHC1_DAT7,"
For kernel:
- linux/arch/arm/mach-mx6/board-mx6sl_evk.c (comment out the 8bit support)
static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {
.cd_gpio = MX6_BRD_SD1_CD,
.wp_gpio = MX6_BRD_SD1_WP,
// .support_8bit = 1,
.support_18v = 1,
.keep_power_at_suspend = 1,
.delay_line = 0,
.platform_pad_change = plt_sd_pad_change,
};
- linux/arch/arm/mach-mx6/board-mx6sl_common.h (comment out the DAT4-8)
| /* SD1 */ | 
MX6SL_PAD_SD1_CLK__USDHC1_CLK_50MHZ,
MX6SL_PAD_SD1_CMD__USDHC1_CMD_50MHZ,
MX6SL_PAD_SD1_DAT0__USDHC1_DAT0_50MHZ,
MX6SL_PAD_SD1_DAT1__USDHC1_DAT1_50MHZ,
MX6SL_PAD_SD1_DAT2__USDHC1_DAT2_50MHZ,
MX6SL_PAD_SD1_DAT3__USDHC1_DAT3_50MHZ,
// MX6SL_PAD_SD1_DAT4__USDHC1_DAT4_50MHZ,
// MX6SL_PAD_SD1_DAT5__USDHC1_DAT5_50MHZ,
// MX6SL_PAD_SD1_DAT6__USDHC1_DAT6_50MHZ,
// MX6SL_PAD_SD1_DAT7__USDHC1_DAT7_50MHZ,
I am not sure if it is stop because of looking for the network. So please try to connect the board with network or add ip=none in bootargs.
As there is some different between your board and the solo lite EVK, have you try to build your own uImage and then replace the prebuild one?
Hi jimmychan,
Thanks for your Reply . I am a new beginner for ANDROID development.
In my custom board, there is no Ethernet.
I thought that it was searching for the file system from ip.
I tried to adding the ip=none in bootargs.
I flashed the file system in /dev/sdb5 partition of the SD card.
If i try to build my own image where can i change for the ip =none in my android building environment.
Thanks,
Vinothraj
i changed the 'ip=none' in the BOARD_KERNEL_CMDLINE in <myandroid>/device/fsl/evk_6sl/BoardConfig.mk.
But there is no improvement in the Boot log.
I flashed the prebuilt system.img file in /dev/sdb5 .
then i can not find the "init" executable file in my filesystem ( /dev/sdb5 ).i am booting my custom board by sd1 slot.
My custom board is designed for 4 bit data line sd1 card. IMX6 SL EVK is designed for 8 bit data line sd1 card.
So can you give the information for change the 8 bit data line to 4 bit data line sd1 card in u-boot and kernel source code.
Please try this:
For u-boot:
- u-boot-2009.08/include/mx6sl_evk.h
remove the "#define CONFIG_MMC_8BIT_PORTS 0x1"
- u-boot-2009.08/board/freescale/mx6sl_evk.c
remove the
"MX6SL_PAD_SD1_DAT4__USDHC1_DAT4,
MX6SL_PAD_SD1_DAT5__USDHC1_DAT5,
MX6SL_PAD_SD1_DAT6__USDHC1_DAT6,
MX6SL_PAD_SD1_DAT7__USDHC1_DAT7,"
For kernel:
- linux/arch/arm/mach-mx6/board-mx6sl_evk.c (comment out the 8bit support)
static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {
.cd_gpio = MX6_BRD_SD1_CD,
.wp_gpio = MX6_BRD_SD1_WP,
// .support_8bit = 1,
.support_18v = 1,
.keep_power_at_suspend = 1,
.delay_line = 0,
.platform_pad_change = plt_sd_pad_change,
};
- linux/arch/arm/mach-mx6/board-mx6sl_common.h (comment out the DAT4-8)
| /* SD1 */ | 
MX6SL_PAD_SD1_CLK__USDHC1_CLK_50MHZ,
MX6SL_PAD_SD1_CMD__USDHC1_CMD_50MHZ,
MX6SL_PAD_SD1_DAT0__USDHC1_DAT0_50MHZ,
MX6SL_PAD_SD1_DAT1__USDHC1_DAT1_50MHZ,
MX6SL_PAD_SD1_DAT2__USDHC1_DAT2_50MHZ,
MX6SL_PAD_SD1_DAT3__USDHC1_DAT3_50MHZ,
// MX6SL_PAD_SD1_DAT4__USDHC1_DAT4_50MHZ,
// MX6SL_PAD_SD1_DAT5__USDHC1_DAT5_50MHZ,
// MX6SL_PAD_SD1_DAT6__USDHC1_DAT6_50MHZ,
// MX6SL_PAD_SD1_DAT7__USDHC1_DAT7_50MHZ,
Thanks for sharing information.
I changed according to your reply. I got new log from booting my board.
like
"
mmcblk1: mmc1:aaaa SU08G 7.40 GiB
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on
mmcblk1: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
"
i attached my new log. Please find it.
I have same problem can you please help me out I bring up the hdmi for me. In my customized board we dont have any change with respect to sdcard & more over the card which is prepared with the MFG tool was not booting..
U-Boot 2009.08-dirty (Oct 31 2014 - 12:21:25)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 180
Temperature: 35 C, calibration data 0x5734d669
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
*** Warning - bad CRC or MMC, using default environment
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot: 0
kernel @ 10808000 (4047004)
ramdisk @ 11800000 (183192)
kernel cmdline:
use boot.img command line:
console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale androidboot.serialno=0a0fa1d4d8191854
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Initializing cgroup subsys cpuset
Initializing cgroup subsys cpu
Linux version 3.0.35-05524-g8513494-dirty (sainath@sainath-Veriton-Series) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #68 SMP PREEMPT Mon Nov 17 10:30:47 IST 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @c1125000 s5760 r8192 d14720 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 208384
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale androidboot.serialno=0a0fa1d4d8191854
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 379MB 187MB 256MB = 822MB total
Memory: 823468k/823468k available, 225108k reserved, 442368K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc003f000 ( 220 kB)
.text : 0xc003f000 - 0xc077d970 (7419 kB)
.data : 0xc077e000 - 0xc07ed140 ( 445 kB)
.bss : 0xc07ed164 - 0xc091bb70 (1211 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:496
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Initializing cgroup subsys cpuacct
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
local enable
CPU1: Booted secondary processor
local enable
CPU2: Booted secondary processor
local enable
CPU3: Booted secondary processor
local enable
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
DEBUG NOTICE/n
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
DEBUG NOTICE/n
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
DEBUG NOTICE/n
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
DEBUG NOTICE/n
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
DEBUG NOTICE/n
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
DEBUG NOTICE/n
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
Uart successful....
Init completed ....
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
IMX usb wakeup probe
bio: create slab <bio-0> at 0
DEBUG NOTICE/n
print_constraints: SPKVDD: 4200 mV
DEBUG NOTICE/n
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
add wake up source irq 75
mc_pfuze 1-0008: recv failed!:-5,d4
mc_pfuze: probe of 1-0008 failed with error -1
MMC start......................./n
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
max17135 2-0048: PMIC MAX17135 for eInk display
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 176K
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = d9880000 suspend_iram_base=d991c000
PM driver module loaded
IMX usb wakeup probe
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
ashmem: initialized
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 744
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
------------[ cut here ]------------
WARNING: at mm/page_alloc.c:2121 __alloc_pages_nodemask+0x18c/0x710()
Modules linked in:
[<c004bd70>] (unwind_backtrace+0x0/0xf8) from [<c0079570>] (warn_slowpath_common+0x4c/0x64)
[<c0079570>] (warn_slowpath_common+0x4c/0x64) from [<c00795a4>] (warn_slowpath_null+0x1c/0x24)
[<c00795a4>] (warn_slowpath_null+0x1c/0x24) from [<c00cffc4>] (__alloc_pages_nodemask+0x18c/0x710)
[<c00cffc4>] (__alloc_pages_nodemask+0x18c/0x710) from [<c004ecd0>] (__dma_alloc+0xa0/0x2fc)
[<c004ecd0>] (__dma_alloc+0xa0/0x2fc) from [<c004efa4>] (dma_alloc_writecombine+0x24/0x2c)
[<c004efa4>] (dma_alloc_writecombine+0x24/0x2c) from [<c0266eac>] (mxcfb_set_par+0x170/0x6ac)
[<c0266eac>] (mxcfb_set_par+0x170/0x6ac) from [<c0258050>] (fb_set_var+0x124/0x290)
[<c0258050>] (fb_set_var+0x124/0x290) from [<c02668f8>] (mxcfb_register+0x268/0x3ec)
[<c02668f8>] (mxcfb_register+0x268/0x3ec) from [<c02692f0>] (mxcfb_probe+0x51c/0xa80)
[<c02692f0>] (mxcfb_probe+0x51c/0xa80) from [<c028a4a4>] (platform_drv_probe+0x18/0x1c)
[<c028a4a4>] (platform_drv_probe+0x18/0x1c) from [<c02892d4>] (driver_probe_device+0x90/0x1ac)
[<c02892d4>] (driver_probe_device+0x90/0x1ac) from [<c028947c>] (__driver_attach+0x8c/0x90)
[<c028947c>] (__driver_attach+0x8c/0x90) from [<c0288518>] (bus_for_each_dev+0x5c/0x88)
[<c0288518>] (bus_for_each_dev+0x5c/0x88) from [<c0288cc0>] (bus_add_driver+0x174/0x234)
[<c0288cc0>] (bus_add_driver+0x174/0x234) from [<c0289928>] (driver_register+0x78/0x13c)
[<c0289928>] (driver_register+0x78/0x13c) from [<c003f640>] (do_one_initcall+0xfc/0x164)
[<c003f640>] (do_one_initcall+0xfc/0x164) from [<c00089cc>] (kernel_init+0xc4/0x16c)
[<c00089cc>] (kernel_init+0xc4/0x16c) from [<c0045aa4>] (kernel_thread_exit+0x0/0x8)
---[ end trace 199f8b1c5287134b ]---
mxc_sdc_fb mxc_sdc_fb.0: Unable to allocate framebuffer memory
detected fb_set_par error, error code: -12
mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
mxc_sdc_fb mxc_sdc_fb.2: Can't get fb option for mxcfb2!
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
m25p80 spi0.0: unrecognized JEDEC id ffffff
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
PPTP driver version 0.8.5
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1
elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -22
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
ov5642_read_reg:write reg error:reg=300a
ov5642_probe:cannot find camera
ov5640_read_reg:write reg error:reg=300a
ov5640_probe:cannot find camera
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
mag3110 2-000e: check mag3110 chip ID
input: mag3110 as /devices/virtual/input/input2
mag3110 2-000e: mag3110 is probed
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
input: mma845x as /devices/virtual/input/input3
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
revserved_memory_account:viv_gpu registerd
Thermal calibration data is 0x5734d669
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12
wm8962 0-001a: Failed to get supply 'DCVDD': -19
wm8962 0-001a: Failed to request supplies: -19
wm8962 0-001a: asoc: failed to probe CODEC wm8962.0-001a: -19
asoc: failed to instantiate card wm8962-audio: -19
imx_3stack asoc driver
ALSA device list:
No soundcards found.
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (12869 buckets, 51476 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
IPv4 over IPv4 tunneling driver
GRE over IPv4 demultiplexor driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 10
ip6_tables: (C) 2000-2006 Netfilter Core Team
IPv6 over IPv4 tunneling driver
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 SEM08G 7.28 GiB
mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB
mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB
rescan partition
mmcblk0: unknown partition table
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
rescan partition
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
mmcblk0boot1: unknown partition table
Bluetooth: RFCOMM ver 1.11
rescan partition
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
mmcblk0boot0: unknown partition table
L2TP core driver, V2.0
PPPoL2TP kernel driver, V2.0
L2TP IP encapsulation support (L2TPv3)
L2TP netlink interface
L2TP ethernet pseudowire support (L2TPv3)
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
Freeing init memory: 220K
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
android_usb: already disabled
mtp_bind_config
root@android:/ # input: eCompass as /devices/virtual/input/input4
Division by zero in kernel.
[<c004bd70>] (unwind_backtrace+0x0/0xf8) from [<c023a02c>] (__do_div64+0xf0/0x100)
Division by zero in kernel.
[<c004bd70>] (unwind_backtrace+0x0/0xf8) from [<c023a02c>] (__do_div64+0xf0/0x100)
init: untracked pid 2143 exited
Division by zero in kernel.
[<c004bd70>] (unwind_backtrace+0x0/0xf8) from [<c023a02c>] (__do_div64+0xf0/0x100)
Division by zero in kernel.
[<c004bd70>] (unwind_backtrace+0x0/0xf8) from [<c023a02c>] (__do_div64+0xf0/0x100)
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
init: untracked pid 2334 exited
warning: `zygote' uses 32-bit capabilities (legacy support in use)
init: untracked pid 2422 exited
init: untracked pid 2413 exited
init: untracked pid 2434 exited
init: untracked pid 2439 exited
init: untracked pid 2455 exited
init: untracked pid 2459 exited
init: untracked pid 2475 exited
init: untracked pid 2479 exited
root@android:/ #
root@android:/ #
root@android:/ #
root@android:/ # init: untracked pid 2494 exited
root@android:/ # init: untracked pid 2499 exited
root@android:/ #
root@android:/ #
root@android:/ # ls -l
drwxr-xr-x root root 1970-01-01 00:00 acct
drwxrwx--- system cache 2014-11-17 13:37 cache
dr-x------ root root 1970-01-01 00:00 config
lrwxrwxrwx root root 1970-01-01 00:00 d -> /sys/kernel/debug
drwxrwx--x system system 1970-01-01 00:00 data
-rw-r--r-- root root 116 1970-01-01 00:00 default.prop
drwxr-xr-x root root 1970-01-01 00:00 dev
drwxr-xr-x root root 1970-01-01 00:00 device
lrwxrwxrwx root root 1970-01-01 00:00 etc -> /system/etc
lrwxrwxrwx root root 1970-01-01 00:00 extsd -> /mnt/extsd
-rw-r----- root root 863 1970-01-01 00:00 fstab.freescale
-rwxr-x--- root root 109356 1970-01-01 00:00 init
-rwxr-x--- root root 5006 1970-01-01 00:00 init.freescale.rc
-rwxr-x--- root root 1930 1970-01-01 00:00 init.freescale.usb.rc
-rwxr-x--- root root 2487 1970-01-01 00:00 init.goldfish.rc
-rwxr-x--- root root 23640 1970-01-01 00:00 init.rc
-rwxr-x--- root root 1795 1970-01-01 00:00 init.trace.rc
-rwxr-x--- root root 3947 1970-01-01 00:00 init.usb.rc
drwxrwxr-x root system 1970-01-01 00:00 mnt
dr-xr-xr-x root root 1970-01-01 00:00 proc
drwx------ root root 2014-11-13 09:15 root
drwxr-x--- root root 1970-01-01 00:00 sbin
lrwxrwxrwx root root 1970-01-01 00:00 sdcard -> /storage/emulated/legacy
d---r-x--- root sdcard_r 1970-01-01 00:00 storage
drwxr-xr-x root root 1970-01-01 00:00 sys
drwxr-xr-x root root 1970-01-01 00:00 system
lrwxrwxrwx root root 1970-01-01 00:00 udisk -> /mnt/udisk
-rw-r--r-- root root 2880 1970-01-01 00:00 ueventd.freescale.rc
-rw-r--r-- root root 272 1970-01-01 00:00 ueventd.goldfish.rc
-rw-r--r-- root root 4024 1970-01-01 00:00 ueventd.rc
lrwxrwxrwx root root 1970-01-01 00:00 vendor -> /system/vendor
root@android:/ # init: untracked pid 2519 exited
init: untracked pid 2527 exited