Hi,
I am trying to boot android jelly bean on imx6 sabrelite board but the problem is can not able to get desktop environment. Its struck over android splash screen and below is the error displayed. Please help me how to fix this issue.
warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 20573687338 (2014-01-07 13:14:31.619795003 UTC)
eth0: Freescale FEC PHY driver [Micrel KSZ9021 Gigabit PHY] (mii_bus:phy_addr=1:06, irq=284)
ADDRCONF(NETDEV_UP): eth0: link is not ready
acc_open
acc_release
PHY: 1:06 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
binder: release 2680:2692 transaction 5952 in, still active
binder: send failed reply for transaction 5952 to 2782:2782
binder: release 2680:2914 transaction 5955 in, still active
binder: send failed reply for transaction 5955 to 2809:2863
binder: release 2680:3013 transaction 5904 out, still active
binder: send failed reply for transaction 6012 to 2998:2998
binder: send failed reply for transaction 6023 to 2915:2962
binder: 2915:2962 transaction failed 29189, size 240-0
binder: 2998:2998 transaction failed 29189, size 2788-4
request_suspend_state: wakeup (0->0) at 30898374005 (2014-01-07 13:14:41.944479003 UTC)
alarm_release: clear alarm, pending 0
binder: release 2884:2972 transaction 4582 out, still active
alarm_release: clear alarm, pending 0
init: untracked pid 2400 exited
binder: release 2405:2405 transaction 5904 in, still active
binder: send failed reply for transaction 5904, target dead
binder: release 2782:2943 transaction 4617 out, still active
init: untracked pid 2927 exited
init: untracked pid 2884 exited
init: untracked pid 3017 exited
init: untracked pid 2782 exited
init: untracked pid 2809 exited
init: untracked pid 2864 exited
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
binder: release 2946:2958 transaction 4582 in, still active
binder: send failed reply for transaction 4582, target dead
binder: release 2946:2977 transaction 4617 in, still active
binder: send failed reply for transaction 4617, target dead
init: untracked pid 2946 exited
init: untracked pid 2915 exited
init: untracked pid 2680 exited
request_suspend_state: wakeup (0->0) at 35482847340 (2014-01-07 13:14:46.528955005 UTC)
init: untracked pid 3015 exited
acc_open
acc_release
init: untracked pid 2405 exited
binder: release 3358:3507 transaction 9596 out, still active
binder: release 3517:3531 transaction 9596 in, still active
binder: send failed reply for transaction 9596, target dead
binder: release 3517:3555 transaction 9752 in, still active
binder: send failed reply for transaction 9752 to 3455:3547
binder: release 3258:3269 transaction 10337 in, still active
binder: send failed reply for transaction 10337 to 3481:3481
binder: 3481:3481 transaction failed 29189, size 208-0
binder: 3481:3481 transaction failed 29189, size 4324-4
alarm_release: clear alarm, pending 0
alarm_release: clear alarm, pending 0
request_suspend_state: wakeup (0->0) at 43142007674 (2014-01-07 13:14:54.188115006 UTC)
init: untracked pid 3038 exited
init: untracked pid 3037 exited
init: untracked pid 3502 exited
init: untracked pid 3432 exited
init: untracked pid 3417 exited
Thanks & Regards,
sasidhar
已解决! 转到解答。
Hi Sasidhar,
This explains a lot. You're running software for a 2GiB board on a machine with only 1GiB of DDR.
Please use our latest U-Boot package from http://boundarydevices.com/u-boot-2013-10-release/ to re-program things using u-boot.nitrogen6q to fix that.
After fixing this, I suspect things will start working.
I got one issue regarding booting of android - 5.0.2 lollipop in sabresd-imx6q board.
init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufac'
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'
init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'
android_usb: already disabled
read descriptors
read strings
mtp_bind_config
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
This binder: 147:147 transaction failed 29189, size 0-0 message keep on occur in my serial terminal but in sabresd board dispaly i didn't get anything...
help me to solve this one thanks in advance
Hi Eric,
Thanks for your suggestions, Now i can able to boot android. But the problem is adb is not detecting the imx6 sabrelite board. And the output of adb is as follows :
$ adb devices
List of devices attached
0123456789ABCDEF offline
I went through the link https://community.freescale.com/thread/256677 and followed the steps
For Linux PC:
android-sdk-linux_86/tools/android update adb
| # ANDROID 3RD PARTY USB VENDOR ID LIST -- DO NOT EDIT. # USE 'android update adb' TO GENERATE. # 1 USB VENDOR ID PER LINE. 0x15a2 |
| SUBSYSTEM=="usb", SYSFS{idVendor}=="15a2", MODE="0666" |
chmod a+r /etc/udev/rules.d/imx-android.rules
i followed the above steps but still iam facing the same issue, Please guide me to fix this issue
Thanks & Regards,
Sasidhar.
Hi Sasidhar,
You should see a prompt on your display to authorize your PC to run ADB. The "offline" message seems to indicate "unauthorized".
There's also a way to place a file in the /data partition, but I can't recall off-hand where the file is or where to get the data to place in the file.
Hi Eric,
I had enabled "USB DEBUGGING" in developer options. When i connect IMX6 board to PC i can see a prompt on display "usb Debugging connected", but still i am getting unauthorized output for adb in PC.
$ adb devices
List of devices attached
0123456789ABCDEF unauthorized
Thanks & Regards,
Sasidhar.
Hi Sasidhar,
As an alternative to using the on-screen prompt for authorization, you can also place your public key into /data/misc/adb/adb_keys as described here:
http://stackoverflow.com/questions/15746917/adb-over-network-without-previous-usb-pairing
Essentially, on your PC:
~/$ cat $HOME/.android/adbkey.pub
Then paste the key into /data/misc/adb/adb_keys on the Android machine.
Hi Sasidhar,
Have you tried running adb server as root? I typically use this command-line to start ADB on my PC:
~/$ sudo `which adb` devices
This is mainly to save on edits to the files in /etc/udev/.
Hello Sasidhar,
This type of error normally occurs if the filesystems (esp system) didn't mount properly, and might indicate a problem when creating your SD card or SATA image.
Are you using our (Boundary Devices) Android?
We added code to allow booting to either SD card, so you'll need to ensure that a kernel command-line parameter points at your boot device.
See http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata for details and this section of the boot script for an example:
HI Eric,
Thanks for your suggestion. I am using imx6-jb-sdcard-20130628.img.gz downloaded from the link http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata and i am flashing it onto the sdcard using the command zcat /home/sasi/android_jb/imx6-jb-sdcard-20130628.img.gz | sudo dd of=/dev/sdb. still i'm facing the same issue (binder issue). The android_log.txt file has been attached for your reference. Waiting for your valuable suggestions.
Thanks & Regards,
Sasidhar
Hi Sasidhar,
Using the .img file should configure the filesystem properly, and will include our boot script.
The log you uploaded seems to cut off the end of some long lines, so I can't see the entire kernel command line:
>> Kernel command line: enable_wait_mode=off console=ttymxc1,115200 vmalloc=400M consoleblank=0 video=mxcfb0:dev=hdmi,bpp=32,1280x720M@60,if=RGB24 3
This does appear to be generated using the stock boot script though:
If you put the SD card in your PC, do you see all of the partitions? Does your system auto-mount /system?
Also, can you run "mount" from the shell when trying to boot Android?
What I'm getting at here is that the problem is most likely the SD card image, and specifically the /system partition (P5).
I can see it mount though:
>> EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)
Finally, can you run this command and capture the output for a minute or so?
# logcat V:* &
This will produce a lot of output, and will likely repeat as Android attempts to re-start, but 60 seconds or so should give an idea of what is crashing.
HI Eric,
Thanks for your suggestions, My system is auto-mount, when i put SD card in my PC i can able to see all the partitions. And even i can able to run mount from the shell when Android is booting. when i run
# logcat V:* &
Each time i reboot IMX6 sabrelite board, i am getting different errors like
> Process com.android.launcher (pid 4815) has died.
> W/ActivityManager( 3816): Process com.android.phone has crashed too many times: killing!
I searched for NFS boot i got this below link
http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-1-booting-over-nfs/
but it is mentioned as android_kernel boot but not entire rootfs. Is there any chance to boot android rootfs through NFS.
The logcat ouput file has been attached for your reference. Please help me out in this issue.
Hello Sasidhar,
I'm not sure why I didn't see the attachment previously. Perhaps there's a delay on the Community site while the scanner runs.
Can you forward the output from "print" at the U-Boot prompt and "netcfg" from the Android shell?
I'm suspicious about this bit from the boot loader:
U-Boot 2013.04-00316-g1903727 (Jul 23 2013 - 11:01:29) CPU: Freescale i.MX6Q rev1.2 at 792 MHz Reset cause: POR Board: SABRE Lite DRAM: 2 GiB
We don't sell 2GiB versions of SABRE Lite.
Are you sure that you have a 2GiB board?
Can you upload a photo?
Hi Eric,
I am using IMX6 sabrelite board with DDR 1GB only. And Below mentioned details are the output from "print" at the U-Boot prompt and "netcfg" from the Android shell. I had attached images of IMX6 Sabrelite board which i am using for your reference.
U-Boot > print
baudrate=115200
bootcmd=for dtype in sata mmc ; do for disk in 0 1 ; do ${dtype} dev ${disk} ;for fs in fat ext2 ; do ${fs}load ${dtype} ${disk}:1 10008000 /6x_bootscript&& source 10008000 ; done ; done ; done; setenv stdout serial,vga ; echo ; echo 6x_bootscript not found ; echo ; echo serial console at 115200, 8N1 ; echo ; echo details at http://boundarydevices.com/6q_bootscript ; usb start; setenv stdin serial,usbkbd
bootdelay=1
clearenv=if sf probe || sf probe || sf probe 1 ; then sf erase 0xc0000 0x2000 && echo restored environment to factory default ; fi
console=ttymxc1
ethact=FEC
ethaddr=00:19:b8:01:1d:41
ethprime=FEC
loadaddr=0x12000000
loadsplash=if sf probe ; then sf read ${splashimage} c2000 ${splashsize} ; fi
upgradeu=for dtype in sata mmc ; do for disk in 0 1 ; do ${dtype} dev ${disk} ;for fs in fat ext2 ; do ${fs}load ${dtype} ${disk}:1 10008000 /6x_upgrade && source 10008000 ; done ; done ; done
root@android:/ # netcfg
lo UP 127.0.0.1/8 0x00000049 00:00:00:00:00:00
can0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
eth0 UP 192.168.1.32/24 0x00001043 00:19:b8:01:1d:41
tunl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
sit0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
ip6tnl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
root@android:/ # init: untracked pid 2873 exited
request_suspend_state: wakeup (0->0) at 73434213011 (2014-01-11 06:45:39.070027002 UTC)
Thanks & Regards,
Sasidhar.
Hi Sasidhar,
This explains a lot. You're running software for a 2GiB board on a machine with only 1GiB of DDR.
Please use our latest U-Boot package from http://boundarydevices.com/u-boot-2013-10-release/ to re-program things using u-boot.nitrogen6q to fix that.
After fixing this, I suspect things will start working.