android booting error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android booting error

4,445件の閲覧回数
asif1206
Contributor I

Hello all

 

We are  using verdin development board 1.1. we are using android 11.0.0.2.4.0 from nxp

 

we are getting the following error will loading android.


U-Boot SPL 2020.04-g88700f6 (Apr 01 2021 - 10:18:20 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.2(release):android-11.0.0_1.0.0-rc3-1-gd56b636
NOTICE: BL31: Built : 10:18:34, Apr 1 2021


U-Boot 2020.04-g88700f6 (Apr 01 2021 - 10:18:20 +0000)

CPU: i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 32C
Reset cause: POR
No MMC card found
MISSING TORADEX CONFIG BLOCK
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
Fail to setup video link
In: serial
Out: serial
Err: serial
Model: Toradex Verdin iMX8M Mini Quad 2GB Wi-Fi / BT IT V1.1A, Serial# 06827748
Carrier: Toradex Verdin Development Board V1.1A, Serial# 10807589

BuildInfo:
- ATF d56b636
- U-Boot 2020.04-g88700f6

flash target is MMC:0
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 2  1  0
avb_slot_verify.c:482: ERROR: dtbo_a: Hash of data does not match digest in descriptor.
Writing A/B metadata to disk.
verify FAIL, state: UNLOCK
boot 'boot_a' still
Kernel load addr 0x40480000 size 28991 KiB
kernel @ 40480000 (29686272)
ramdisk @ 44680000 (9778471)
fdt @ 44480000 (47522)
Device is unlocked, press power key to skip warning logo...
no video device found!
can't show unlock warning.
## Flattened Device Tree blob at 44480000
Booting using the fdt blob at 0x44480000
Using Device Tree in place at 0000000044480000, end 000000004448e9a1

Starting kernel ...

[ 0.000000][ T0] asif 29-12-2021 setup.c Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000][ T0] Linux version 5.10.52-dirty (root@hp-g1) (Android (7284624, based on r416183b) clang version 12.0.5 (https://android.googlesource.com/toolchain/llvm-project c935d99d7cf2016289302412d708641d52d2f7ee), LLD 12.0.5 (/buildbot/src/android/llvm-toolchain/out/llvm-project/lld c935d99d7cf2016289302412d708641d52d2f7ee)) #20 SMP PREEMPT Sun Jan 16 17:11:03 IST 2022
[ 0.000000][ T0] asif 29-12-2021 setup.c Machine model: Toradex Verdin iMX8M Mini WB on Dahlia Board 15-1-2022
[ 0.000000][ T0] Stack Depot is disabled
[ 0.000000][ T0] earlycon: asif 30-12-2021 file earlycon.c function earlycon_print_info
[ 0.000000][ T0] earlycon: ec_imx6q0 at MMIO 0x0000000030860000 (options '115200')
[ 0.000000][ T0] printk: bootconsole [ec_imx6q0] enabled
[ 0.000000][ T0] efi: UEFI not found.
[ 0.000000][ T0] kvm [0]: Reserved 14 MiB at 0xbec00000
[ 0.000000][ T0] Zone ranges:
[ 0.000000][ T0] DMA32 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000][ T0] Normal empty
[ 0.000000][ T0] Movable zone start for each node
[ 0.000000][ T0] Early memory node ranges
[ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000][ T0] node 0: [mem 0x00000000b8000000-0x00000000b83fffff]
[ 0.000000][ T0] node 0: [mem 0x00000000b8400000-0x00000000bfffffff]
[ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000][ T0] cma: Reserved 800 MiB at 0x0000000086000000
[ 0.000000][ T0] psci: probing for conduit method from DT.
[ 0.000000][ T0] psci: PSCIv1.1 detected in firmware.
[ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs
[ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000][ T0] psci: SMC Calling Convention v1.1
[ 0.000000][ T0] percpu: Embedded 33 pages/cpu s95896 r8192 d31080 u135168
[ 0.000000][ T0] Detected VIPT I-cache on CPU0
[ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[ 0.000000][ T0] CPU features: detected: ARM erratum 845719
[ 0.000000][ T0] CPU features: detected: GIC system register CPU interface
[ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000][ T0] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure cgroup.memory=nokmem console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 init=/init androidboot.console=ttymxc0 androidboot.hardware=nxp firmware_class.path=/vendor/firmware loop.max_part=7 transparent_hugepage=never androidboot.lcd_density=240 androidboot.primary_display=imx-drm androidboot.wificountrycode=CN moal.mod_para=wifi_mod_para_sd8987.conf cma=800M@0x400M-0xb80M androidboot.vendor.sysrq=1 buildvariant=userdebug androidboot.soc_type=imx8mm androidboot.boot_device_root=mmcblk0 androidboot.boottime=1BLL:0,1BLE:8272,KL:0,KD:0,AVB:4202,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.verifiedbootstate=orange androidboot.flash.locked=0 androidboot.slot_suffix=_a androidboot.vbmeta.device=PARTUUID=058088d3-bb9d-441e-8a89-f2c1caec637e androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=unlocked androidboot.vbmeta.h
[ 0.000000][ T0] cgroup: Disabling pressure control group feature
[ 0.000000][ T0] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000][ T0] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[ 0.000000][ T0] Memory: 1178468K/2097152K available (16000K kernel code, 1918K rwdata, 9936K rodata, 1024K init, 1119K bss, 99484K reserved, 819200K cma-reserved)
[ 0.000000][ T0] random: get_random_u64 called from kmem_cache_open+0x2c/0x2f4 with crng_init=0
[ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000][ T0] rcu: RCU event tracing is enabled.
[ 0.000000][ T0] rcu: RCU dyntick-idle grace-period acceleration is enabled.
[ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[ 0.000000][ T0] Trampoline variant of Tasks RCU enabled.
[ 0.000000][ T0] Tracing variant of Tasks RCU enabled.
[ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000][ T0] GICv3: 128 SPIs implemented
[ 0.000000][ T0] GICv3: 0 Extended SPIs implemented
[ 0.000000][ T0] GICv3: Distributor has no Range Selector support
[ 0.000000][ T0] GICv3: 16 PPIs implemented
[ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000][ T0] ITS: No ITS available, not enabling LPIs
[ 0.000000][ T0] rcu: Offload RCU callbacks from CPUs: (none).
[ 0.000000][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000004][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.009390][ T0] asif 10-1-2022 inside serial8250_isa_init_ports
[ 0.015055][ T0] asif 10-1-2022 B inside for port0
[ 0.020127][ T0] asif 10-1-2022 8250_port.c serial8250_init_port
[ 0.026604][ T0] asif 10-1-2022 8250_port.c serial8250_set_defaultfs
[ 0.033339][ T0] asif 16-1-2022 inside set_io_from_upio
[ 0.038851][ T0] asif 10-1-2022 set_io_from_upio G default
[ 0.044804][ T0] asif 10-1-2022 set_io_from_upio G2 up->cur_iotype (null) p->handle_irq ?#Õ^†
[ 0.053901][ T0] asif 10-1-2022 B inside for port1
[ 0.058976][ T0] asif 10-1-2022 8250_port.c serial8250_init_port
[ 0.065453][ T0] asif 10-1-2022 8250_port.c serial8250_set_defaultfs
[ 0.072190][ T0] asif 16-1-2022 inside set_io_from_upio
[ 0.077702][ T0] asif 10-1-2022 set_io_from_upio G default
[ 0.083653][ T0] asif 10-1-2022 set_io_from_upio G2 up->cur_iotype (null) p->handle_irq ?#Õ^†
[ 0.092752][ T0] asif 10-1-2022 B inside for port2
[ 0.097828][ T0] asif 10-1-2022 8250_port.c serial8250_init_port
[ 0.104303][ T0] asif 10-1-2022 8250_port.c serial8250_set_defaultfs
[ 0.111040][ T0] asif 16-1-2022 inside set_io_from_upio
[ 0.116552][ T0] asif 10-1-2022 set_io_from_upio G default
[ 0.122503][ T0] asif 10-1-2022 set_io_from_upio G2 up->cur_iotype (null) p->handle_irq ?#Õ^†
[ 0.131603][ T0] asif 10-1-2022 B inside for port3
[ 0.136678][ T0] asif 10-1-2022 8250_port.c serial8250_init_port
[ 0.143155][ T0] asif 10-1-2022 8250_port.c serial8250_set_defaultfs
[ 0.149888][ T0] asif 16-1-2022 inside set_io_from_upio
[ 0.155402][ T0] asif 10-1-2022 set_io_from_upio G default
[ 0.161353][ T0] asif 10-1-2022 set_io_from_upio G2 up->cur_iotype (null) p->handle_irq ?#Õ^†
[ 0.170476][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.181480][ T0] pid_max: default: 32768 minimum: 301
[ 0.186955][ T0] LSM: Security Framework initializing
[ 0.192198][ T0] SELinux: Initializing.
[ 0.196494][ T0] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.204500][ T0] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.214047][ T1] asif 15-1-2022 inside kernel_init_freeable
[ 0.219027][ T1] asif 15-1-2022 wait_for_completion
[ 0.224267][ T1] asif 15-1-2022 set_memds
[ 0.229488][ T1] rcu: Hierarchical SRCU implementation.
[ 0.234907][ T1] EFI services will not be available.
[ 0.239645][ T1] smp: asif 29-12-2021 smp.c Bringing up secondary CPUs ...
[ 0.247157][ T0] Detected VIPT I-cache on CPU1
[ 0.247185][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.247230][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.247802][ T0] Detected VIPT I-cache on CPU2
[ 0.247821][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.247847][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.248406][ T0] Detected VIPT I-cache on CPU3
[ 0.248424][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.248452][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.248529][ T1] smp: Brought up 1 node, 4 CPUs
[ 0.310210][ T1] SMP: Total of 4 processors activated.
[ 0.315620][ T1] CPU features: detected: 32-bit EL0 Support
[ 0.321506][ T1] CPU features: detected: CRC32 instructions
[ 0.327351][ T1] CPU features: detected: 32-bit EL1 Support
[ 0.333219][ T1] CPU features: detected: Protected KVM
[ 0.338698][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.360341][ T1] CPU: All CPU(s) started at EL2
[ 0.362312][ T14] alternatives: patching kernel code
[ 0.377309][ T1] Registered cp15_barrier emulation handler
[ 0.380250][ T1] Registered setend emulation handler
[ 0.385484][ T1] KASLR disabled due to lack of seed
[ 0.390789][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.401160][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.442377][ T1] pinctrl core: initialized pinctrl subsystem asif 29-12-2021 core.c
[ 0.447667][ T1] pinctrl core: asif 30-12-2021 core.c before pinctrl-devices
[ 0.455116][ T1] pinctrl core: asif 30-12-2021 core.c before pinctrl-maps
[ 0.462290][ T1] pinctrl core: asif 30-12-2021 core.c before pinctrl-handles
[ 0.470806][ T1] NET: Registered protocol family 16 asif 29-12-2021 socket.c
[ 0.479905][ T1] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.485261][ T1] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.493772][ T1] audit: initializing netlink subsys (disabled)
[ 0.499983][ T36] audit: type=2000 audit(0.324:1): state=initialized audit_enabled=0 res=1
[ 0.500520][ T1] thermal_sys: Registered thermal governor 'step_wise'
[ 0.508314][ T1] thermal_sys: Registered thermal governor 'user_space'
[ 0.515044][ T1] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.522097][ T1] cpuidle: using governor menu
[ 0.534169][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.541383][ T1] ASID allocator initialised with 65536 entries
[ 0.547550][ T1] Serial: AMBA PL011 UART driver
[ 0.552293][ T1] imx rpmsg driver is registered.
[ 0.596357][ T1] iommu: Default domain type: Translated
[ 0.599712][ T1] SCSI subsystem initialized
[ 0.603750][ T1] usbcore: registered new interface driver usbfs asif 29-12-2021 driver.c
[ 0.612007][ T1] usbcore: registered new interface driver hub asif 29-12-2021 driver.c
[ 0.620221][ T1] usbcore: registered new device driver usb
[ 0.626121][ T1] mc: Linux media interface: v0.10
[ 0.630975][ T1] videodev: Linux video capture interface: v2.00
[ 0.637259][ T1] EDAC MC: Ver: 3.0.0
[ 0.642060][ T1] Advanced Linux Sound Architecture Driver Initialized.
[ 0.648324][ T1] Bluetooth: Core ver 2.22
[ 0.652167][ T1] NET: Registered protocol family 31 asif 29-12-2021 socket.c
[ 0.659654][ T1] Bluetooth: HCI device and connection manager initialized
[ 0.666747][ T1] Bluetooth: HCI socket layer initialized
[ 0.672346][ T1] Bluetooth: L2CAP socket layer initialized
[ 0.678127][ T1] Bluetooth: SCO socket layer initialized
[ 0.683891][ T1] nfc: nfc_init: NFC Core ver 0.1
[ 0.688661][ T1] NET: Registered protocol family 39 asif 29-12-2021 socket.c
[ 0.696635][ T1] clocksource: Switched to clocksource arch_sys_counter
[ 0.783961][ T1] VFS: Disk quotas dquot_6.6.0
[ 0.785804][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.794083][ T1] NET: Registered protocol family 2 asif 29-12-2021 socket.c
[ 0.800912][ T1] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.810043][ T1] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.818307][ T1] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.827015][ T1] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.835158][ T1] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.842310][ T1] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.849672][ T1] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.857655][ T1] NET: Registered protocol family 1 asif 29-12-2021 socket.c
[ 0.864952][ T1] NET: Registered protocol family 44 asif 29-12-2021 socket.c
[ 0.872467][ T1] PCI: CLS 0 bytes, default 64
[ 0.877326][ T1] Trying to unpack rootfs image as initramfs...
[ 1.290006][ T1] Freeing initrd memory: 9548K
[ 1.316772][ T1] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.323038][ T1] kvm [1]: IPA Size Limit: 40 bits
[ 1.339141][ T1] kvm [1]: GICv3: no GICV resource entry
[ 1.341797][ T1] kvm [1]: disabling GICv2 emulation
[ 1.346968][ T1] kvm [1]: GIC system register CPU interface enabled
[ 1.353623][ T1] kvm [1]: vgic interrupt IRQ9
[ 1.359320][ T1] kvm [1]: Protected nVHE mode initialized successfully
[ 1.374135][ T1] Initialise system trusted keyrings
[ 1.376821][ T1] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[ 1.395105][ T1] fuse: init (API version 7.32)
[ 1.434027][ T1] Key type asymmetric registered
[ 1.436015][ T1] Asymmetric key parser 'x509' registered
[ 1.441694][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 241)
[ 1.449750][ T1] io scheduler mq-deadline registered
[ 1.454987][ T1] io scheduler kyber registered
[ 1.459869][ T1] io scheduler bfq registered
[ 1.468188][ T1] asif 10-1-2022 Before serial8250_isa_init_ports
[ 1.471644][ T1] asif 10-1-2022 inside serial8250_isa_init_ports
[ 1.477929][ T1] asif 10-1-2022 inside serial8250_isa_init_ports if return
[ 1.485108][ T1] asif 30-12-2021 a Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 1.493862][ T1] asif 16-1-2022 serial_core.c uart_configure_port port_iobase (null) port_mapbase (null) port_membase (null) return
[ 1.494083][ T1] asif 16-1-2022 serial_core.c uart_configure_port port_iobase (null) port_mapbase (null) port_membase (null) return
[ 1.506083][ T1] asif 16-1-2022 serial_core.c uart_configure_port port_iobase (null) port_mapbase (null) port_membase (null) return
[ 1.518260][ T1] asif 16-1-2022 serial_core.c uart_configure_port port_iobase (null) port_mapbase (null) port_membase (null) return
[ 1.538184][ T1] brd: module loaded
[ 1.561679][ T1] loop: module loaded
[ 1.564625][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
[ 1.571259][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <[email protected]>. All Rights Reserved.
[ 1.582841][ T1] libphy: Fixed MDIO Bus: probed
[ 1.586397][ T1] tun: Universal TUN/TAP device driver, 1.6
[ 1.592225][ T1] CAN device driver interface
[ 1.596714][ T1] PPP generic driver version 2.4.2
[ 1.601770][ T1] PPP BSD Compression module registered
[ 1.607130][ T1] PPP Deflate Compression module registered
[ 1.612920][ T1] PPP MPPE Compression module registered
[ 1.618416][ T1] NET: Registered protocol family 24 asif 29-12-2021 socket.c
[ 1.625941][ T1] PPTP driver version 0.8.5
[ 1.630581][ T1] usbcore: registered new interface driver rtl8150 asif 29-12-2021 driver.c
[ 1.638949][ T1] usbcore: registered new interface driver r8152 asif 29-12-2021 driver.c
[ 1.647322][ T1] usbcore: registered new interface driver cdc_ether asif 29-12-2021 driver.c
[ 1.656069][ T1] usbcore: registered new interface driver cdc_eem asif 29-12-2021 driver.c
[ 1.664667][ T1] usbcore: registered new interface driver cdc_ncm asif 29-12-2021 driver.c
[ 1.673220][ T1] usbcore: registered new interface driver aqc111 asif 29-12-2021 driver.c
[ 1.682567][ T1] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.688943][ T1] ehci-pci: EHCI PCI platform driver
[ 1.694139][ T1] ehci-platform: EHCI generic platform driver
[ 1.700705][ T1] usbcore: registered new interface driver cdc_acm asif 29-12-2021 driver.c
[ 1.708634][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.717678][ T1] usbcore: registered new interface driver uas asif 29-12-2021 driver.c
[ 1.725655][ T1] usbcore: registered new interface driver usb-storage asif 29-12-2021 driver.c
[ 1.734927][ T1] dummy_hcd dummy_hcd.0: USB Host+Gadget Emulator, driver 02 May 2005
[ 1.742589][ T1] dummy_hcd dummy_hcd.0: Dummy host controller
[ 1.748620][ T1] dummy_hcd dummy_hcd.0: new USB bus registered, assigned bus number 1
[ 1.756931][ T1] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 1.765772][ T1] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.773728][ T1] usb usb1: Product: Dummy host controller
[ 1.779414][ T1] usb usb1: Manufacturer: Linux 5.10.52-dirty dummy_hcd
[ 1.786242][ T1] usb usb1: SerialNumber: dummy_hcd.0
[ 1.791764][ T1] hub 1-0:1.0: USB hub found
[ 1.795983][ T1] hub 1-0:1.0: 1 port detected
[ 1.801376][ T1] usbcore: registered new interface driver xpad asif 29-12-2021 driver.c
[ 1.809125][ T1] usbcore: registered new interface driver uvcvideo asif 29-12-2021 driver.c
[ 1.817567][ T1] USB Video Class driver (1.1.1)
[ 1.822391][ T1] gspca_main: v2.14.0 registered
[ 1.827622][ T1] device-mapper: uevent: version 1.0.3
[ 1.832758][ T1] device-mapper: ioctl: 4.44.0-ioctl (2021-02-01) initialised: [email protected]
[ 1.842259][ T1] Bluetooth: HCI UART driver ver 2.3
[ 1.846887][ T1] Bluetooth: HCI UART protocol H4 registered
[ 1.852797][ T1] Bluetooth: HCI UART protocol LL registered
[ 1.858684][ T1] Bluetooth: HCI UART protocol Broadcom registered
[ 1.865007][ T1] Bluetooth: HCI UART protocol QCA registered
[ 1.871762][ T1] sdhci: Secure Digital Host Controller Interface driver
[ 1.877856][ T1] sdhci: Copyright(c) Pierre Ossman
[ 1.882926][ T1] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.889654][ T1] hid: raw HID events driver (C) Jiri Kosina
[ 1.896389][ T1] usbcore: registered new interface driver usbhid asif 29-12-2021 driver.c
[ 1.903669][ T1] usbhid: USB HID core driver
[ 1.908575][ T1] ashmem: initialized
[ 1.912455][ T1] gnss: GNSS driver registered with major 234
[ 1.918719][ T1] usbcore: registered new interface driver snd-usb-audio asif 29-12-2021 driver.c
[ 1.927495][ T1] GACT probability NOT on
[ 1.931330][ T1] Mirror/redirect action on
[ 1.935699][ T1] netem: version 1.3
[ 1.939529][ T1] u32 classifier
[ 1.942864][ T1] input device check on
[ 1.947237][ T1] Actions configured
[ 1.952401][ T1] xt_time: kernel timezone is -0000
[ 1.956632][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 1.963074][ T1] gre: GRE over IPv4 demultiplexor driver
[ 1.968241][ T1] ip_gre: GRE over IPv4 tunneling driver
[ 1.974728][ T1] IPv4 over IPsec tunneling driver
[ 1.979391][ T1] Initializing XFRM netlink socket
[ 1.983759][ T1] IPsec XFRM device driver
[ 1.988640][ T1] NET: Registered protocol family 10 asif 29-12-2021 socket.c
[ 1.998997][ T1] Segment Routing with IPv6
[ 2.000756][ T1] mip6: Mobile IPv6
[ 2.005311][ T1] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.011932][ T1] ip6_gre: GRE over IPv6 tunneling driver
[ 2.016931][ T1] NET: Registered protocol family 17 asif 29-12-2021 socket.c
[ 2.024071][ T1] NET: Registered protocol family 15 asif 29-12-2021 socket.c
[ 2.031676][ T1] can: controller area network core
[ 2.036718][ T1] NET: Registered protocol family 29 asif 29-12-2021 socket.c
[ 2.044095][ T1] can: raw protocol
[ 2.047805][ T1] can: broadcast manager protocol
[ 2.052742][ T1] can: netlink gateway - max_hops=1
[ 2.058177][ T1] Bluetooth: RFCOMM TTY layer initialized
[ 2.063363][ T1] Bluetooth: RFCOMM socket layer initialized
[ 2.069260][ T1] Bluetooth: RFCOMM ver 1.11
[ 2.073685][ T1] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.080322][ T1] Bluetooth: HIDP socket layer initialized
[ 2.086065][ T1] l2tp_core: L2TP core driver, V2.0
[ 2.091089][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 2.096594][ T1] tipc: Activated (version 2.0.0)
[ 2.101913][ T1] NET: Registered protocol family 30 asif 29-12-2021 socket.c
[ 2.109567][ T1] tipc: Started in single node mode
[ 2.123485][ T1] NET: Registered protocol family 36 asif 29-12-2021 socket.c
[ 2.128533][ T1] NET: Registered protocol family 40 asif 29-12-2021 socket.c
[ 2.136451][ T1] registered taskstats version 1
[ 2.140559][ T1] Loading compiled-in X.509 certificates
[ 2.146043][ T1] page_owner is disabled
[ 2.150301][ T1] Key type ._fscrypt registered
[ 2.154849][ T1] Key type .fscrypt registered
[ 2.159486][ T1] Key type fscrypt-provisioning registered
[ 2.169051][ T1] ALSA device list:
[ 2.169869][ T1] No soundcards found.
[ 2.173995][ T1] asif 15-1-2022 before console_on_rootfs
[ 2.179748][ T1] asif 15-1-2022 file --> (efault)
[ 2.184681][ T1] Warning: unable to open an initial console.asif 12-1-2022
[ 2.191929][ T1] asif 15-1-2022 After console_on_rootfs
[ 2.200336][ T1] Freeing unused kernel memory: 1024K
[ 2.245036][ T1] Run /init as init process
[ 2.283110][ T1] init: init first stage started!
[ 2.288745][ T1] init: Loading module /lib/modules/soc-imx8m.ko with args ""
[ 2.298183][ T1] SoC: i.MX8MM revision 1.0
[ 2.299958][ T1] init: Loaded kernel module /lib/modules/soc-imx8m.ko
[ 2.306709][ T1] init: Loading module /lib/modules/mxc-clk.ko with args ""
[ 2.316324][ T1] init: Loaded kernel module /lib/modules/mxc-clk.ko
[ 2.320461][ T1] init: Loading module /lib/modules/clk-imx8mm.ko with args ""
[ 2.352916][ T1] init: Loaded kernel module /lib/modules/clk-imx8mm.ko
[ 2.357139][ T1] init: Loading module /lib/modules/imx8m_pm_domains.ko with args ""
[ 2.367717][ T1] init: Loaded kernel module /lib/modules/imx8m_pm_domains.ko
[ 2.372476][ T1] init: Loading module /lib/modules/timer-imx-sysctr.ko with args ""
[ 2.383957][ T1] Bus freq driver module loaded
[ 2.388911][ T1] imx8mm-pinctrl 30330000.pinctrl:
[ 2.388911][ T1] asif-->inside file pinctrl-imx.c function int imx_pinctrl_problE asif 31-12-2021 a
[ 2.401115][ T1] imx8mm-pinctrl 30330000.pinctrl:
[ 2.401115][ T1] asif-->inside file pinctrl-imx.c function static int imx_pinctrl_problE asif 31-12-2021 b
[ 2.416305][ T1] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver asif 28-12-2021 b
[ 2.425769][ T1] pinctrl core: asif-->31-12-2021 inside file pinctrl/core.c function static void pinctrl_init_device debugf start
[ 2.437448][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c before if 1 --> 30330000.pinctrl , 2--> 30330000.pinctrl
[ 2.449759][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c else 1 --> 30330000.pinctrl
[ 2.459823][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c before debugfs_create_dir 1 --> 30330000.pinctrl, 
[ 2.472051][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debugfs_create_dir 2 --> 
[ 2.482574][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 1
[ 2.492469][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 2
[ 2.502365][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 3
[ 2.512308][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 4
[ 2.522130][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 5
[ 2.532025][ T1] pinctrl core: asif-->03-01-2022 inside file pinctrl/core.c after debufs_create_file 6
[ 2.541909][ T1] pinctrl core: asif-->31-12-2021 inside file pinctrl/core.c function static void pinctrl_init_device debugf end
[ 2.557432][ T1] printk: console [ttymxc0] enabled
[ 2.557432][ T1] printk: console [ttymxc0] enabled
[ 2.564762][ T1] printk: bootconsole [ec_imx6q0] disabled
[ 2.564762][ T1] printk: bootconsole [ec_imx6q0] disabled
[ 2.576617][ T1]
[ 2.576617][ T1] asif 15-1-2022--> serial_core.c uart_report_port port->iotype 2
[ 2.588745][ T1] asif 15-1-2022 serial_core.c UPIO_MEM,UPIO_MEM16,32,32BE,AU,TSI
[ 2.596415][ T1]
[ 2.596415][ T1] asif 15-1-2022========
[ 2.596415][ T1] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 45, base_baud = 1500000) is a IMX
[ 2.596415][ T1] ========
[ 2.615645][ T1]
[ 2.615645][ T1] asif 15-1-2022--> serial_core.c uart_report_port port->iotype 2
[ 2.625585][ T1] asif 15-1-2022 serial_core.c UPIO_MEM,UPIO_MEM16,32,32BE,AU,TSI
[ 2.633255][ T1]
[ 2.633255][ T1] asif 15-1-2022========
[ 2.633255][ T1] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 46, base_baud = 1500000) is a IMX
[ 2.633255][ T1] ========
[ 2.662796][ T1] gpio-129 (CTRL_SLEEP_MOCI#): hogged as output/high
[ 2.686885][ T125] mmc0: CQHCI version 5.10
[ 2.725104][ T125] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.736933][ T1] i2c i2c-0: IMX I2C adapter registered
[ 2.742915][ T1] i2c i2c-2: IMX I2C adapter registered
[ 2.749392][ T1] i2c i2c-3: IMX I2C adapter registered
[ 2.766592][ T1] mxs-dma 33000000.dma-controller: initialized
[ 2.776219][ T1] imx mu driver is registered.
[ 2.781359][ T1] ion_alloc: module is from the staging directory, the quality is unknown, you have been warned.
[ 2.794658][ T1] ion_sys_heap: module is from the staging directory, the quality is unknown, you have been warned.
[ 2.807938][ T1] ion_cma_heap: module is from the staging directory, the quality is unknown, you have been warned.
[ 2.820057][ T1] ion_unmapped_heap: module is from the staging directory, the quality is unknown, you have been warned.
[ 2.832173][ T1] Invalid reserved mem info
[ 2.837704][ T33] mmc0: Command Queue Engine enabled
[ 2.842919][ T33] mmc0: new HS400 MMC card at address 0001
[ 2.849588][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: failed to find trusty node. Use normal mode.
[ 2.850487][ T33] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 2.860585][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/soc@0:bus@30000000/30370000.snvs/30370000.snvs:snvs-powerkey/input/input7
[ 2.866140][ T33] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 2.870376][ T7] input: gpio-keys as /devices/platform/gpio-keys/input/input8
[ 2.871449][ T7] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 2 mkt segment 2 supported-hw 0x4 0x4
[ 2.873094][ T7] mmc2: CQHCI version 5.10
[ 2.907392][ T33] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 2.907454][ T7] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 2.914154][ T33] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (238:0)
[ 2.934010][ T1] imx-drm soc@0:bus@32c00000:display-subsystem: no available port
[ 2.945110][ T33] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14
[ 2.969201][ T1] __power_supply_register: Expected proper parent device for 'battery'
[ 2.976397][ T125] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 2.977721][ T1] __power_supply_register: Expected proper parent device for 'usb'
[ 2.982951][ T125] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[ 3.003101][ T32] imx-sdma 302c0000.dma-controller: firmware found.
[ 3.009705][ T32] imx-sdma 302c0000.dma-controller: loaded firmware 4.6
[ 3.013269][ T125] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 3.022958][ T125] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 3.025164][ T33] imx-sdma 302b0000.dma-controller: firmware found.
[ 3.031974][ T125] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.046384][ T125] usb usb2: Product: EHCI Host Controller
[ 3.052006][ T125] usb usb2: Manufacturer: Linux 5.10.52-dirty ehci_hcd
[ 3.058835][ T125] usb usb2: SerialNumber: ci_hdrc.1
[ 3.064815][ T33] imx-sdma 30bd0000.dma-controller: firmware found.
[ 3.065124][ C0] random: fast init done
[ 3.075417][ T125] hub 2-0:1.0: USB hub found
[ 3.080006][ T125] hub 2-0:1.0: 1 port detected
[ 3.087160][ T135] mmc2: new ultra high speed SDR104 SDIO card at address 0001
[ 3.110841][ T1] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.121054][ T143] random: sh: uninitialized urandom read (40 bytes read)
[ 3.130535][ T143] random: sh: uninitialized urandom read (40 bytes read)
[ 3.137669][ T143] random: sh: uninitialized urandom read (4 bytes read)
[ 3.155596][ T1] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.345046][ T32] usb 2-1: new high-speed USB device number 2 using ci_hdrc
[ 3.506940][ T32] usb 2-1: New USB device found, idVendor=0424, idProduct=2744, bcdDevice= 2.21
[ 3.515842][ T32] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 3.523696][ T32] usb 2-1: Product: USB2744
[ 3.528063][ T32] usb 2-1: Manufacturer: Microchip Tech
[ 3.534087][ T32] hub 2-1:1.0: USB hub found
[ 3.538687][ T32] hub 2-1:1.0: 4 ports detected
[ 3.829041][ T32] usb 2-1.1: new low-speed USB device number 3 using ci_hdrc
[ 3.949811][ T32] usb 2-1.1: New USB device found, idVendor=04ca, idProduct=0061, bcdDevice= 1.00
[ 3.958884][ T32] usb 2-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 3.966903][ T32] usb 2-1.1: Product: USB Optical Mouse
[ 3.972323][ T32] usb 2-1.1: Manufacturer: PixArt
[ 3.979934][ T32] input: PixArt USB Optical Mouse as /devices/platform/soc@0/soc@0:bus@32c00000/32e50000.usb/ci_hdrc.1/usb2/2-1/2-1.1/2-1.1:1.0/0003:04CA:0061.0001/input/input9
[ 3.996023][ T32] hid-generic 0003:04CA:0061.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.1-1.1/input0
[ 4.089058][ T32] usb 2-1.4: new high-speed USB device number 4 using ci_hdrc
[ 4.207316][ T32] usb 2-1.4: New USB device found, idVendor=0424, idProduct=2740, bcdDevice= 2.00
[ 4.216389][ T32] usb 2-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.224407][ T32] usb 2-1.4: Product: Hub Controller
[ 4.229565][ T32] usb 2-1.4: Manufacturer: Microchip Tech
[ 13.326336][ T1] init: Wait for partitions returned after 10009ms
[ 13.332801][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout: metadata
[ 13.347140][ T1] init: Failed to mount required partitions early ...
[ 13.355035][ T1] init: InitFatalReboot: signal 6
[ 13.365224][ T1] init: #00 pc 00000000000afd40 /system/bin/init
[ 13.371552][ T1] init: #01 pc 000000000004cd90 /system/bin/init
[ 13.377851][ T1] init: #02 pc 0000000000013ab0 /system/lib64/libbase.so
[ 13.384839][ T1] init: #03 pc 0000000000013090 /system/lib64/libbase.so
[ 13.391828][ T1] init: #04 pc 0000000000075b1c /system/bin/init
[ 13.398119][ T1] init: #05 pc 000000000002e0ec /system/bin/init
[ 13.404449][ T1] asif 16-1-2022 kvm_main.c kvm: exiting hardware virtualization
[ 13.414506][ T1] ci_hdrc ci_hdrc.1: remove, state 1
[ 13.419684][ T1] usb usb2: asif 16-1-2022 hub.c USB disconnect, device number 1
[ 13.427364][ T1] usb 2-1: asif 16-1-2022 hub.c USB disconnect, device number 2
[ 13.434944][ T1] usb 2-1.1: asif 16-1-2022 hub.c USB disconnect, device number 3
[ 13.477905][ T1] usb 2-1.4: asif 16-1-2022 hub.c USB disconnect, device number 4
[ 13.489073][ T1] ci_hdrc ci_hdrc.1: USB bus 2 deregistered
[ 13.521094][ T1] reboot: Restarting system with command 'bootloader'
ÿ
U-Boot SPL 2020.04-g88700f6 (Apr 01 2021 - 10:18:20 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.2(release):android-11.0.0_1.0.0-rc3-1-gd56b636
NOTICE: BL31: Built : 10:18:34, Apr 1 2021


U-Boot 2020.04-g88700f6 (Apr 01 2021 - 10:18:20 +0000)

CPU: i.MX8MMQ rev1.0 1600 MHz (running at 1200 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 37C
Reset cause: POR
No MMC card found
MISSING TORADEX CONFIG BLOCK
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
Fail to setup video link
In: serial
Out: serial
Err: serial
Model: Toradex Verdin iMX8M Mini Quad 2GB Wi-Fi / BT IT V1.1A, Serial# 06827748
Carrier: Toradex Verdin Development Board V1.1A, Serial# 10807589

BuildInfo:
- ATF d56b636
- U-Boot 2020.04-g88700f6

flash target is MMC:0
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 2  0
u-boot=>
u-boot=>
u-boot=>
u-boot=>
u-boot=>
u-boot=>

 

 

ラベル(2)
0 件の賞賛
返信
1 返信

4,420件の閲覧回数
art
NXP Employee
NXP Employee

The most likely cause of the issue is wrong boot media partitioning. Check it
according to the i.MX Android User's Guide document for your version of Android.

Best Regards,
Artur

0 件の賞賛
返信