android_O8.1.0_1.3.0_8M_tools use builded imx-android-oreo uboot can not success?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android_O8.1.0_1.3.0_8M_tools use builded imx-android-oreo uboot can not success?

ソリューションへジャンプ
1,322件の閲覧回数
传策薛
Contributor V

Hi community:

   I download the nxp Android8 repo source,

   and use the branch "imx-android-oreo "

   and "source build/envsetup.sh ","lunch evk_8mq-userdebug","make -j4"

  

   after build complete, I copy the "out/target/product/evk_8mq/u-boot-imx8mq.imx"  as  "mfgtools/Profiles/Linux/OS Firmware/firmware/imx-boot-imx8mqevk-sd.bin-flash_evk"

   finally, I burning to the imx8mq-evk board, but error at "Jumping to OS image":

      pastedImage_5.png

     

   

   should i change something?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,116件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

You can find in the below web-page:

Android OS for i.MX Applications Processors|NXP 

You only need to download the 

O8.1.0_1.3.0_8MQ_GA_DOCS file.

In the zip file, you can find all the Android information related to our BSP.

Hope this can help you.

Best Regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,116件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello, 

I apologize for the delay,

Are you following our Android user's guide? ln, the user's guide you can find step by step how to build and deploy the image on the board.

Best Regards,

Diego.

0 件の賞賛
返信
1,116件の閲覧回数
传策薛
Contributor V

what is the name of the user guides?

0 件の賞賛
返信
1,117件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

You can find in the below web-page:

Android OS for i.MX Applications Processors|NXP 

You only need to download the 

O8.1.0_1.3.0_8MQ_GA_DOCS file.

In the zip file, you can find all the Android information related to our BSP.

Hope this can help you.

Best Regards,

Diego.

0 件の賞賛
返信