android 9, recovery, apply update from ADB for IMX8MM, adb devices got error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

android 9, recovery, apply update from ADB for IMX8MM, adb devices got error

1,887 Views
ChandlerHH
Contributor I

Hi  all,

 

1, I tested the android recovery feature on android 9 for iMX8MM,  but failed to run "apply update from ADB", when selected it and pressed "key-power", it showed texts on screen as followed:

'Supported API:3

Stopping adbd...

E: Failed to open driver control: No such file or directory

E: Failed to open driver control: No such file or directory

 

Now send the package you want to apply

to the devices with "adb sideload <filename>"...'

2, the logcat of android:

' [ 57.263767] init: processing action (sys.usb.ffs.ready=1) from (/init.recovery.freescale.rc:21)
[ 57.273213] init: Command 'write /config/usb_gadget/g1/UDC ci_hdrc.0' action=sys.usb.ffs.ready=1 (/init.recovery.freescale.rc:24) took 0ms and failed: Unable to write to file '/config/usb_gadget/g1/UDC': Unable to write file contents: No such device '

failed_to_open_drive.jpgrecovery_menu.png

it looks like that the UDC configuration has error?

I found out some topics of the android recovery in community, but none of them matches my question.

could anyone have some suggestions, many thanks!

0 Kudos
Reply
0 Replies