android-12.2.0.0 has no display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

android-12.2.0.0 has no display

跳至解决方案
991 次查看
AIdeveloper
Contributor II

Hi After I update to android-12.2.0.0 by uuu, login from uart is ok, but no display from mipi-dsi output.
At the bootup, the monitor display NXP, but monitor report NO HDMI cable instered after bootup.

I get android-12.2.0.0 image from file:
https://cache.nxp.com/secured/bsps/android-12.0.0_2.0.0_image_8mmevk.tar.gz?__gda__=1659932087_041e8...)

The uuu scipts is below and no error is reported.
sudo ./uuu_imx_android_flash.sh -f imx8mm -a -e -t sd -d mipi-panel -c 28

Could somebody can help?
Thanks!

0 项奖励
回复
1 解答
981 次查看
AIdeveloper
Contributor II

 

Fixed:

sudo ./uuu_imx_android_flash.sh -f imx8mm -a -t sd -d mipi-panel -c 28 -e

-->>

sudo ./uuu_imx_android_flash.sh -f imx8mm -a -t sd -d m4 -c 28 -e

# -d ddr4: also ok

在原帖中查看解决方案

1 回复
982 次查看
AIdeveloper
Contributor II

 

Fixed:

sudo ./uuu_imx_android_flash.sh -f imx8mm -a -t sd -d mipi-panel -c 28 -e

-->>

sudo ./uuu_imx_android_flash.sh -f imx8mm -a -t sd -d m4 -c 28 -e

# -d ddr4: also ok