android 11 installation issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android 11 installation issue

988 次查看
embedded_Dev
Contributor III

Hello @all,

I am trying to install android11 source in my ubuntu 16.04 PC. I am facing the following error

----------------------------------------------

Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0
Setting WORKSPACE to /home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0
Setting android_builddir to /home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build
tar: /home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis: Cannot open: No such file or directory
tar: Error is not recoverable: exiting now
fatal: can't open patch '/home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis/patch/0001-imx8_helpers-enable-a-UART-on-crash.patch': No such file or directory
fatal: can't open patch '/home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis/patch/0002-imx8m-_bl31_setup-remove-RDC-limitation-on-UART-port.patch': No such file or directory
fatal: can't open patch '/home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis/patch/0001-plat-imx8mm-use-uart3-as-console.patch': No such file or directory
fatal: can't open patch '/home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis/patch/0001-Parsing-the-devicetree-name.patch': No such file or directory
fatal: can't open patch '/home/prasanth/Projects/android11/imx-android-11.0.0_1.0.0/android_build/device/nxp/imx8m/phyboard_polis/patch/0001-iMX8-soc.mk-only-remove-dtbs-in-clean.patch': No such file or directory
Android source is ready for the build

-----------------------------------------------------------------------------------

I tried to install the same source from  other ubuntu 16.04 PC  but i am facing issue in my PC. I have installed all the dependencies but still i am facing the same issues

Please let me know if any

Thanks & Regards

Shamiullah

标签 (1)
0 项奖励
回复
1 回复

975 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello embedded_Dev,

 

Please try to use the latest android11.0.0_2.2.0 and ubuntu 18.04 or even better the 20.04.

 

Regards

0 项奖励
回复