adding kernel paches to imx7d picopi yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adding kernel paches to imx7d picopi yocto

1,569 次查看
maash
Contributor II

Hi.

I'm using the picopi with yocto and trying to add some kernel patches to my package. I've watched several tutorials, read the yocto project tutorials, but I'm still a bit baffled what goes wrong.

So I've got meta-avs-demos -project from NXP codeaurora. It compiles OK out of box.

However I cannot seem to be able to patch the kernel and then do the full build.

I've followed these instructions to get the kernel sources, add the pathes and make successful build:

TipsAndTricks/Patching the source for a recipe - Yocto Project 

And that amounts to basically:

devtool modify linux-imx

cd workspace/sources/linux-imx/

checkout tn-imx_4.1.15_2.0.0_ga

git pull

git am /path/to/paches

bitbake linux-imx

This builds OK.

However if I try then make the whole package bitbake avs-image, this fails:

BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx7d-pico"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.1.15-2.1.0"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"

....

ERROR: Task do_unpack in /home/build/workspace/sources/poky/meta/recipes-kernel/perf/perf.bb depends upon non-existent task do_patch in /home/build/workspace/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb
ERROR: Command execution failed: 1

I've tried adding the stuff to layer (which is why I would like get this working in the first place), however it also fails.

标记 (2)
1 回复

1,327 次查看
maash
Contributor II

Ok, I got it working. I had to change recipe to use newer head of the kernel. Dunno why the workarea linux as one the layers didn't work. Perhaps some other layer used different kernel version or something.