add wifi firmware in yocto image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

add wifi firmware in yocto image

2,063 Views
dharmeshkanzari
Contributor II

hello there,

i want to add wifi firmware in yocto image.

in this user guide, they have basic image. 

WaRP7-User-Guide/Yocto_Project.adoc at master · WaRP7/WaRP7-User-Guide · GitHub 

now i want to add wifi firmware.

0 Kudos
Reply
2 Replies

1,589 Views
daiane_angolini
NXP Employee
NXP Employee

the Yocto meta-freescale source code install by default the wifi firmware into any image (but core-image-minimal).

What image are you using?

0 Kudos
Reply

1,589 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dharmesh

this board is designed and supported by third party

WaRP7 - The Next Generation IoT and Wearable De... | element14 | Design Center 

so one can post it on vendor support or meta-fsl-arm mailing list, so that someone familiar

with it could try to assist you.
Feedback and Support | element14 

meta-freescale Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply