adb reboot cannot reboot system.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adb reboot cannot reboot system.

2,246 次查看
kangjianwei
Contributor I

We change the PF3000 Power On mode from auto mode to pressing power key to power on mode.  we find that the command 'adb reboot' cannot to restart system. Before no change mode, the reboot is ok.

the log as:

:/ # reboot
snvs_rtc_set_alarm set
sysrq: rtc_set_alarm done
sysrq: SysRq : Emergency Remount R/O
EXT4-fs (mmcblk2p4): re-mounted. Opts: (null)
EXT4-fs (mmcblk2p10): re-mounted. Opts: (null)
Emergency Remount complete
ci_hdrc ci_hdrc.1: remove, state 4
usb usb1: USB disconnect, device number 1
ci_hdrc ci_hdrc.1: USB bus 1 deregistered
android_work: sent uevent USB_STATE=DISCONNECTED
reboot: Restarting system with command ''
Unable to restart system

Now the power on mode is ok, we can press button to power on, and set "PWRONRSTEN = 1", press Button key > 4S, the system can power off.

why we change the power mode cause the reboot issue?

thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,996 次查看
kangjianwei
Contributor I

please close the question.

we find that the WDT pin hardware is missed.  now the reset feature is ok.

0 项奖励
回复

1,996 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which board are you using?

which bsp are you using?

0 项奖励
回复