adb devices not detecting device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adb devices not detecting device

5,458 次查看
srinivas_jakkul
Contributor I

Hi,

I have installed Windows 10 on Virtualbox on a MAC host.

Installed android platform-tools and tools and updated the environment variables.

After this, I have connected the Indigo2 device (imx8mn nano) to the system

Then connected USB device to Windows machine from the menu (Devices  -> USB -> Jupiter USB device) as shown in the IMG-5037.jpg

Then opened the Device Manager in the Windows (Virtual system). Scan for new hardwarde as shown in IMG-5038.jpg

Here the device is shown. But adb devices is not recognizing the device

After this, I have tried to update the  driver using using ADB device driver and also WinUsb Device Driver as shown in IMG-5040.

In both cases, I am getting error as "This device cannot start (Code 10) Error.

Any help is appreciated as I am using this for first time on a fresh installation of Windows 10

Let me know if any other information is needed. I am able to connect to serial console to that same Windows machine for console logs

/Srini

标签 (1)
0 项奖励
回复
1 回复

5,258 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Srinivas,

   Probably, you need to install android ADB driver to windows 10. try it , please!

   you refer to the link to download and install adb driver.

https://community.nxp.com/docs/DOC-342719 

Have a nice day!

BR,

weidong

0 项奖励
回复