about yocto build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about yocto build error

2,158件の閲覧回数
kevinli
Contributor II

HI,   All:

   编译yocto项目到最后出现生成sdcard出错,请问这可能什么原因导致的?

ERROR: core-image-minimal-1.0-r0 do_image_sdcard: Function failed: do_image_sdcard (log file is located at /media/kevin/disk2/imx-yocto-bsp/build/tmp/work/imx6qdlsabresd-fslc-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.27325)

   谢谢!

具体log:

VirtualBox:/media/kevin/disk2/imx-yocto-bsp/build$ bitbake core-image-minimal
WARNING: You have included the meta-gnome layer, but 'x11' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-gnome README for details on enabling meta-gnome support.
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:00
Loaded 3484 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-fslc-linux-gnueabi"
MACHINE = "imx6qdlsabresd"
DISTRO = "fslc-framebuffer"
DISTRO_VERSION = "2.5"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe
meta-multimedia = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp
meta-sdk = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:01
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: core-image-minimal-1.0-r0 do_image_sdcard: Function failed: do_image_sdcard (log file is located at /media/kevin/disk2/imx-yocto-bsp/build/tmp/work/imx6qdlsabresd-fslc-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.27325)
ERROR: Logfile of failure stored in: /media/kevin/disk2/imx-yocto-bsp/build/tmp/work/imx6qdlsabresd-fslc-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.27325
Log data follows:
| DEBUG: Executing python function set_image_size
| DEBUG: 8158.800000 = 6276 * 1.300000
| DEBUG: 8192.000000 = max(8158.800000, 8192)[8192.000000] + 1
| DEBUG: 8192.000000 = int(8192.000000)
| DEBUG: 8192 = aligned(8192)
| DEBUG: returning 8192
| DEBUG: Python function set_image_size finished
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg/opkg_0.3.6.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.43.8.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-kernel/dtc/dtc_1.4.5.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/python/python-native_2.7.15.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.30.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-extended/pigz/pigz_2.4.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/kmod-native_git.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dnf/dnf_2.7.5.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mtools/mtools_4.0.18.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-connectivity/openssl/openssl_1.0.2p.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/swig/swig_3.0.12.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mklibs/mklibs-native_0.1.43.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/prelink/prelink_git.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-extended/bc/bc_1.06.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-core/update-rc.d/update-rc.d_0.7.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-support/lzop/lzop_1.03.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-runtime_7.3.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/meta-freescale/recipes-kernel/linux/linux-fslc-imx_4.9-1.0.x.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/createrepo-c/createrepo-c_git.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/rpm/rpm_4.14.1.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.27.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-extended/parted/parted_3.2.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.3.6.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dosfstools/dosfstools_4.1.bb:do_populate_sysroot', 'virtual:native:/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/bison/bison_3.0.4.bb:do_populate_sysroot', '/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-cross_7.3.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['opkg-native', 'e2fsprogs-native', 'dtc-native', 'python-native', 'binutils-cross-arm', 'pigz-native', 'ldconfig-native', 'kmod-native', 'dnf-native', 'mtools-native', 'openssl-native', 'swig-native', 'mklibs-native', 'prelink-native', 'depmodwrapper-cross', 'bc-native', 'update-rc.d-native', 'qemuwrapper-cross', 'lzop-native', 'gcc-runtime', 'makedevs-native', 'linux-fslc-imx', 'createrepo-c-native', 'rpm-native', 'glibc', 'parted-native', 'quilt-native', 'pseudo-native', 'opkg-utils-native', 'dosfstools-native', 'bison-native', 'gcc-cross-arm', 'autoconf-native', 'pkgconfig-native', 'libsolv-native', 'libarchive-native', 'libtool-native', 'gnu-config-native', 'automake-native', 'util-linux-native', 'texinfo-dummy-native', 'gettext-minimal-native', 'attr-native', 'flex-native', 'zlib-native', 'python3-native', 'gtk-doc-native', 'xz-native', 'elfutils-native', 'binutils-native', 'qemu-native', 'shadow-native', 'linux-libc-headers', 'libgcc', 'libxml2-native', 'sqlite3-native', 'glib-2.0-native', 'file-native', 'expat-native', 'ninja-native', 'cmake-native', 'curl-native', 'popt-native', 'bzip2-native', 'db-native', 'dbus-native', 'nss-native', 'ncurses-native', 'readline-native', 'gdbm-native', 'python3-iniparse-native', 'libdnf-native', 'libcomps-native', 'librepo-native', 'libpcre-native', 'lzo-native', 'libmpc-native', 'mpfr-native', 'gmp-native', 'm4-native', 'pixman-native', 'alsa-lib-native', 'libffi-native', 're2c-native', 'autoconf-archive-native', 'nspr-native', 'python3-six-native', 'libcheck-native', 'gobject-introspection-native', 'gpgme-native', 'util-macros-native', 'libpng-native', 'python3-setuptools-native', 'libassuan-native', 'libgpg-error-native', 'unzip-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_image_sdcard
| 0+0 records in
| 0+0 records out
| 0 bytes copied, 9.4333e-05 s, 0.0 kB/s
| Model: (file)
| Disk /media/kevin/disk2/imx-yocto-bsp/build/tmp/work/imx6qdlsabresd-fslc-linux-gnueabi/core-image-minimal/1.0-r0/deploy-core-image-minimal-image-complete/core-image-minimal-imx6qdlsabresd-20200420030605.rootfs.sdcard: 25.2MB
| Sector size (logical/physical): 512B/512B
| Partition Table: msdos
| Disk Flags:
|
| Number Start End Size Type File system Flags
| 1 4194kB 12.6MB 8389kB primary lba
| 2 12.6MB 21.0MB 8389kB primary
|
| 110+0 records in
| 110+0 records out
| 56320 bytes (56 kB, 55 KiB) copied, 0.000238358 s, 236 MB/s
| 418+1 records in
| 418+1 records out
| 428680 bytes (429 kB, 419 KiB) copied, 0.000759174 s, 565 MB/s
| mkfs.fat: warning - lowercase labels might not work properly with DOS or Windows
| mkfs.fat 4.1 (2017-01-24)
| Disk full
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_image_sdcard (log file is located at /media/kevin/disk2/imx-yocto-bsp/build/tmp/work/imx6qdlsabresd-fslc-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.27325)
ERROR: Task (/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_sdcard) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2150 tasks of which 2149 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory

Summary: 1 task failed:
/media/kevin/disk2/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_sdcard
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ラベル(5)
0 件の賞賛
返信
1 返信

1,935件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi kevinli ,

Please verify that your host machine has enough space for compilation process of yocto project. 

Would you please confirm the ubuntu version you are using?  Would you also please confirm which BSP version you are using and the steps which you have performed? 

Regards,

Radhiika Somaiya.

0 件の賞賛
返信