about ddr configuration in imx7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about ddr configuration in imx7

948 Views
flabyjacob
Contributor III

hello,

we got to know that DDR controller is initialized by DCD table from board.cfg file,we went through .cfg file to know about clock configuration of DDR, but we could not find any such configuration,

please help us to know how ddr clock for imx7 is configured..? or if it is configured by boot code from the internal boot ROM how we will get to know at which frequency ddr is running at..?

kindly help me.

Any assistance with this issue would be much appreciated.

i.MX Processorsimx 7d

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

876 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Default memory frequency, shown in Table 6-28 (Clock root setting by ROM) of the

i.MX 7Dual Reference Manual, Rev. 1, 01/2018 is used by U-boot for Linux boot.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply