about  I.MX6 linux kernel4.1 - rt18  used GPU question?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about  I.MX6 linux kernel4.1 - rt18  used GPU question?

879件の閲覧回数
lvxiong
Contributor I

The SDK I used was imx-4.1-krogoth, compiled with DISTRO = fsl-imx-wayland MACHINE = imx6qsabresd source fsl-setup-release.sh-b build, compiled with bitbake fsl-image-gui.

But Linux kernel I want to add patch-4.1.15-rt18.patch on  the bsp linux4.1 kernel.  Will the GPU still work ok? Is GPU SDK specified only in version 4.1?

ラベル(5)
0 件の賞賛
返信
1 返信

793件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi James

I believe GPU will still work ok in your case.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信