about Chip on/off control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about Chip on/off control

ソリューションへジャンプ
1,870件の閲覧回数
goto11
Contributor III

Hello,Community

Which register should I control to turn on the PMIC_ON_REQ pin when the SNVS power supply is first turned on?

Please tell me how to distinguish the following two states with software.
・ SNVS power supply turned on first
・ Start with ONOFF pin

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,745件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  i.MX PMIC_ON_REQ is  asserted after VDD_SNVS_IN (SNVS power supply is first turned on).

When VDD_SNVS_IN is present the ONOFF controls PMIC_ON_REQ.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,746件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  i.MX PMIC_ON_REQ is  asserted after VDD_SNVS_IN (SNVS power supply is first turned on).

When VDD_SNVS_IN is present the ONOFF controls PMIC_ON_REQ.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信